AD4170 no-OS Example Project

See projects/ad4170 (doxygen) for the Doxygen documentation.

Contents

Supported Evaluation Boards

Overview

The AD4170-4 is a low noise, low power, 24-bit sigma-delta ADC with a programmable gain amplifier, an integrated 2.5 V reference and a 16 entry channel sequencer selecting from 4 differential or 8 single-ended analog inputs. The digital filter can be configured as sinc5+average, sinc5, sinc3 or FIR, with output data rates from 1.6 SPS up to 500 kSPS.

This project also covers the pin and register compatible family members:

  • AD4171-4 and AD4172-2, which differ in the available analog input count.

  • AD4190-4 and AD4195-4, which drop the DAC and limit the sinc5 filter configuration.

  • AD4171-8, which exposes 8 differential or 16 single-ended analog inputs.

The device variant driven by the project is selected through the AD4170_DEV_ID macro in common_data.h, which defaults to ID_AD4171_8.

Refer to the AD4170-4 data sheet for detailed information regarding operation of the IC.

Applications

  • Precision instrumentation

  • Weigh scales and strain gauges

  • Temperature measurement (RTD, thermocouple, thermistor)

  • Process control

Hardware Specifications

Power Supply Requirements

The evaluation board is powered from the SDP-K1 through the Arduino headers, so no external supply is required for the default configuration.

Pin Description

The evaluation boards are Arduino form factor shields, so they mate directly with the Arduino headers of the SDP-K1. The following table lists the signals used by this project.

Arduino

SDP-K1 pin

Description

D10

PA15

SPI Chip Select (GPIO)

D11

PA7

SPI1 Master Out Slave In

D12

PB4

SPI1 Master In Slave Out

D13

PB3

SPI1 Clock

The ADC samples SDI on the SCLK rising edge with SCLK idling high, so the SPI controller is configured for mode 3 at 11.25 MHz.

The example polls the RDYB bit of the DATA_STATUS register instead of monitoring the DIG_AUX1 output, so no data ready interrupt line needs to be wired. Consequently the ad4170_read24s() and ad4170_continuous_read() fast paths, which require a DIG_AUX1 GPIO configured as RDY, are not exercised here.

No-OS Build Setup

Please see: https://wiki.analog.com/resources/no-os/build

No-OS Supported Examples

The initialization data used in the examples is taken out from: Project Common Data Path

The macros used in Common Data are defined in platform specific files found in: Project Platform Configuration Path

IIO example (default)

This project is an IIOD demo for the AD4170 family evaluation boards. The project launches an IIOD server on the board so that the user may connect to it via an IIO client. Using IIO-Oscilloscope, the user can configure the ADC and view the measured data on a plot.

If you are not familiar with ADI IIO Application, please take a look at: IIO No-OS

If you are not familiar with ADI IIO-Oscilloscope Client, please take a look at: IIO Oscilloscope

The No-OS IIO Application together with the No-OS IIO AD4170 driver take care of all the back-end logic needed to setup the IIO server.

The ADC is brought up with sequencer channels 0 to 7 mapped to the AIN0-AIN1 up to the AIN14-AIN15 differential pairs, using the internal 2.5 V reference, a gain of 1 and the sinc5+average filter. Sequencer channels 8 to 15 have both multiplexer inputs left AD4170_OPEN, since the AD4171-8 has no further analog inputs to pair; map them in common_data.c to measure anything on them. One IIO channel is exposed for each of the 16 sequencer channels regardless of the Channel_En register contents, so that the channels the ADC converts can be picked from the IIO client at buffer enable or at raw read time. Channels are named voltage0 to voltage15 after their sequencer channel, not after the multiplexer inputs they convert. Each channel provides the raw, scale and sampling_frequency attributes.

The output data rate is a property of the setup a channel is mapped to, and the 16 sequencer channels share only 8 setups, so writing sampling_frequency retunes every channel mapped to the same setup. Map a channel to a setup of its own in common_data.c to rate it independently.

This example initializes the IIO device and calls the IIO app as shown in: IIO Example

To build the IIO example:

make EXAMPLE=iio_example

No-OS Supported Platforms

STM32 Platform

Used hardware

Build Command

# to delete current build
make reset
# to build the project for STM32 platform
make PLATFORM=stm32 HARDWARE=sdp-k1.ioc EXAMPLE=iio_example
# to flash the code
make run