ADIN1140 no-OS Project

See projects/adin1140 (doxygen) for the Doxygen documentation.

Supported Evaluation Boards

Overview

The ADIN1140 is a low-power, single-port 10BASE-T1S MAC/PHY designed for multi-drop industrial Ethernet over a single twisted pair (SPE). It complies with the IEEE 802.3cg-2019 standard and implements the Physical Layer Collision Avoidance (PLCA) reconciliation sublayer, allowing multiple nodes to share a mixing segment without classic CSMA/CD overhead. The integrated MAC is accessed through a 4-wire SPI link using the OPEN Alliance TC6 (OA-TC6) chunked protocol, which makes the ADIN1140 a good fit for host MCUs that lack an on-chip Ethernet MAC.

This project provides bare-metal and FreeRTOS-based examples that exercise the no-OS ADIN1140 driver in two modes:

  • Raw Ethernet frame transmit/receive (driver-level smoke test)

  • TCP/UDP throughput measurement with lwIP + lwiperf

Hardware Specifications

Power Supply Requirements

The EVAL-ADIN1140 evaluation board operates with a 3.3 V supply, sourced from the host MCU board through the SPI/IO header or 6-30 V sourced from the P4 connector. The board's VDDIO domain is selected to match the host (typically 3.3 V); confirm jumper selection on the eval board before powering up.

Supported Examples

The initialization data used in the examples is taken out from the Project Common Data Path.

The macros used in Common Data are defined in platform specific files found in the Project Platform Configuration Path.

The project uses the CMake build system. The example to build is selected by pointing PROJECT_DEFCONFIG at one of the project's .conf defconfig files:

  • frame_rx_tx.conf

  • iperf_lwip_example.conf

  • iperf_lwip_freertos.conf

The target board is selected with a CMake preset (max32690fthr or nucleo-h563zi). See the Build Command sections under each supported platform below for the full invocation.

frame_rx_tx example

The frame_rx_tx example is a bare-metal driver-level smoke test. It brings up the ADIN1140 over SPI/OA-TC6, enables promiscuous mode and the broadcast filter, and then in a 200 ms loop:

  • prints the link state and the on-chip TX/RX frame counters (ADIN1140_TX_FRAME_CNT_REG / ADIN1140_RX_FRAME_CNT_REG);

  • transmits a broadcast Ethernet frame containing the ASCII payload "Hello ADIN1140!" via adin1140_write_fifo();

  • drains any received frame with adin1140_read_fifo() and prints source/destination MAC addresses and the first bytes of the payload.

The test source MAC is CA:2F:B7:10:23:63. The example does not use lwIP and so does not require a host IP/network configuration; it only needs another node on the same 10BASE-T1S mixing segment to observe or respond to the broadcast frames.

In order to build the frame_rx_tx example, pass its defconfig to CMake:

-DPROJECT_DEFCONFIG=adin1140/frame_rx_tx.conf

iperf_lwip_example

The iperf_lwip_example runs the lwIP stack on top of the ADIN1140 netif glue (no_os_lwip_init + adin1140_lwip_ops) and starts the default lwiperf TCP server on the standard iperf port. It is the canonical bare-metal Ethernet-over-SPE throughput test.

The example wires the ADIN1140 INT pin to a GPIO interrupt on the host MCU. The ISR sets a global irq_triggered flag; the main loop calls no_os_lwip_step() and clears the flag only when the MAC-PHY has signalled work, so SPI traffic is driven by the hardware rather than by polling.

Default network parameters are baked into the project CFLAGS:

  • IP address: 192.168.97.40

  • Netmask: 255.255.0.0

  • Gateway: 192.168.97.1

The host running iperf must be on the same subnet (for example a static 192.168.97.x IP on the host's network interface). Once the board prints iperf server started. Network is ready for iperf testing., run:

iperf -c 192.168.97.40 -i 1

on the host. Throughput reports are printed both on the host (by iperf) and on the board's UART through the lwiperf_report callback.

In order to build the iperf_lwip_example, pass its defconfig to CMake:

-DPROJECT_DEFCONFIG="adin1140/iperf_lwip_example.conf"

iperf_lwip_freertos example

The iperf_lwip_freertos example is the FreeRTOS counterpart of iperf_lwip_example. It creates a single net_task that owns no_os_lwip_init, the GPIO-IRQ setup and the lwiperf server.

The ADIN1140 INT pin is configured for level-low triggering; the ISR masks the pin at the GPIO controller and uses xTaskNotifyFromISR() to wake the network task. The task blocks on ulTaskNotifyTake(), calls no_os_lwip_step(), then re-enables the GPIO IRQ. This is the recommended pattern for combining the ADIN1140 with FreeRTOS-based applications, since it avoids the busy-wait loop used by the bare-metal version while still being driven entirely by the MAC-PHY's INT signal.

The example uses the same default IP / netmask / gateway as iperf_lwip_example. It pulls the FreeRTOS configuration from projects/adin1140/src/FreeRTOSConfig.h.

In order to build the iperf_lwip_freertos example, pass its defconfig to CMake:

-DPROJECT_DEFCONFIG=adin1140/iperf_lwip_freertos.conf

No-OS Supported Platforms

Maxim Platform

Hardware Used

Connections

Common control signals (UART log + ADIN1140 SPI + INT) are wired as follows. SPI uses no-OS chip-select index 1, mode 0.

MAX32690FTHR (TARGET=max32690)

SPI is on instance 0, clocked at 25 MHz; the ADIN1140 INT line is routed to GPIO P0.8 (GPIO0_IRQn).

Signal

MAX32690FTHR Pin

EVAL-ADIN1140 Pin

GND

GND

GND

3V3

3V3

VDDIO / 3V3

SPI SCLK

SPI0 SCK

SCLK

SPI SS (CS)

SPI0 SS1

/CS

SPI MOSI

SPI0 MOSI

MOSI

SPI MISO

SPI0 MISO

MISO

ADIN1140 INT

P0.8

/INT

UART TX (log)

UART0 TX

--

UART RX (log)

UART0 RX

--

Build Command

The MAXIM_LIBRARIES environment variable must point at the MaximSDK Libraries directory (see the Maxim CMake build guide for the full toolchain setup and prerequisites).

The build is a two-step CMake flow: configure with a board preset and a project defconfig, then build the adin1140 target. Run the commands from the no-OS repository root.

# Configure for the MAX32690FTHR, iperf_lwip_example
cmake --preset max32690fthr -B build \
      -DPROJECT_DEFCONFIG=adin1140/iperf_lwip_example.conf --fresh

# Build the project
cmake --build build --target adin1140

# Flash the board
cmake --build build --target flash

To build a different example, point PROJECT_DEFCONFIG at another .conf file (for example adin1140/frame_rx_tx.conf or adin1140/iperf_lwip_freertos.conf). The resulting adin1140.elf, adin1140.hex and adin1140.bin are placed in the build directory.

STM32 Platform

Hardware Used

  • EVAL-ADIN1140

  • NUCLEO-H563ZI (STM32H563ZIT6 host MCU)

  • A USB-C cable (powers the Nucleo and provides the ST-LINK debug probe plus the Virtual COM Port used for the UART log)

Prerequisites

The STM32 build regenerates the low-level HAL/CubeMX sources from the project's .ioc file (nucleo-h563zi.ioc) as part of the CMake configure step, so both STM32CubeMX and STM32CubeIDE must be installed on the build host:

  • STM32CubeMX — code generator, invoked to produce the HAL sources from the .ioc.

  • STM32CubeIDE — provides the bundled arm-none-eabi toolchain and the flash/debug tools (ST-LINK GDB server / STM32_Programmer_CLI).

The build locates them through two environment variables. Set them if the tools are not in a default install location (point them at the executables, or on Windows at the install directories):

export STM32CUBEMX=</path/to/stm32cubemx>
export STM32CUBEIDE=</path/to/stm32cubeide>
# Windows (PowerShell):
#   $env:STM32CUBEMX = "C:\ST\STM32CubeMX\STM32CubeMX.exe"
#   $env:STM32CUBEIDE = "C:\ST\STM32CubeIDE"

See the STM32 CMake build guide for the full toolchain setup and prerequisites.

Connections

The ADIN1140 is driven from SPI1 (no-OS chip-select handled as a software GPIO on port D, mode 0, 13 MHz) and its INT line is routed to PD15 (EXTI15). The UART log is on USART3, which on the NUCLEO-H563ZI is wired to the on-board ST-LINK Virtual COM Port and appears as a serial device on the host over the same USB-C connection (115200 8N1) — no external USB-UART adapter is needed.

Signal

NUCLEO-H563ZI Pin

EVAL-ADIN1140 Pin

GND

GND

GND

3V3

3V3

VDDIO / 3V3

SPI SCLK

PA5 (SPI1 SCK)

SCK

SPI SS (CS)

PD14 (GPIO SW-CS)

D6

SPI MOSI

PB5 (SPI1 MOSI)

MO

SPI MISO

PG9 (SPI1 MISO)

MI

ADIN1140 INT

PD15 (EXTI15)

D13

Build Command

The build uses the CMake preset flow. Configure with the nucleo-h563zi preset and a project defconfig, then build (and optionally flash) the adin1140 target. Run the commands from the no-OS repository root.

# Configure for the NUCLEO-H563ZI, iperf_lwip_freertos example
cmake --preset nucleo-h563zi -B build-adin1140 \
      -DPROJECT_DEFCONFIG=adin1140/"iperf_lwip_freertos.conf" --fresh

# Build the project
cmake --build build-adin1140 --target adin1140

Currently, the STM32H563 cannot be programmed using the no-OS build system, so an alternative such as STM32CubeProgrammer can be used. The build artifacts can be found in build-adin1140/build/.

To build a different example, point PROJECT_DEFCONFIG at another .conf file (adin1140/frame_rx_tx.conf, adin1140/iperf_lwip_example.conf or adin1140/iperf_lwip_freertos.conf). The resulting adin1140.elf, adin1140.hex and adin1140.bin are placed in the build directory.

Testing with iperf

Both iperf_lwip_example and iperf_lwip_freertos bring up an lwiperf TCP server on the board (default IP 192.168.97.40, port 5001). To measure throughput:

  1. Connect the EVAL-ADIN1140 to the 10BASE-T1S segment shared with the host (directly, or through a 10BASE-T1S ↔ standard-Ethernet media converter).

  2. Give the host interface a static address on the same subnet, e.g. 192.168.97.50/16.

  3. Open the ST-LINK Virtual COM Port (115200 8N1) to watch the board log. Wait until it reports that the iperf server is up.

  4. Run the iperf client on the host against the board (the board is the server):

    iperf -c 192.168.97.40 -p 5001 -i 1 -t 15
    

Throughput is reported once per second by the host iperf client and, via the lwiperf_report callback, on the board's UART. The iperf_lwip_freertos example additionally prints a periodic driver statistics line (RX/TX bandwidth and frame/error counters from oa_tc6_get_stats / adin1140_get_stats) on the same UART, which is useful for confirming there are no CRC/alignment errors or buffer drops during the transfer.