MAX22017 no-OS Driver
See drivers/dac/max22017 (doxygen) for the Doxygen documentation.
Supported Devices
MAX22017
Overview
The MAX22017 is a two-channel industrial-grade configurable analog output device that can be changed on-the-fly in software to voltage or current output mode. The MAX22017 offers one 16-bit DAC per output channel. The MAX22017 can operate from an internal or external reference.
MAX22017 Device Configuration
Driver Initialization
In order to be able to use the device, you will have to provide the support for the communication protocol (SPI) as well as an external GPIO for the RSTB pin.
The first API to be called is max22017_init. Make sure that it returns 0, which means that the driver was intialized correctly.
GPIO Controller Configuration
Both devices have an internal GPIO controller, only difference is that MAX22017 supports 6 GPIOs meanwhile MAX22018 only supports 4 GPIOs. In the driver files the max22017_gpio_ops can be found and used when declaring a no-OS GPIO initializaon parameter, therefor all the platform specific operation are called from the no-OS GPIO API as a standalone platform.
Channel Configuration
Channel data can be set/get with the max22017_set_data and max22017_get_data.
Channel slew-rate configuration can also be set using max22017_slew_rate
Channel gain and offset can be calibrated with max22017_offset_calib and max22017_gain_calib.
Channel operation mode can also be configured using max22017_op_mode as well as other channel specific configurations that can be changed using max22017_config
Soft Reset
MAX22017 can be soft reseted by using max22017_soft_reset.
MAX22017 Driver Initialization Example
struct max22017_desc *max22017;
struct no_os_spi_init_param spi_ip = {
.device_id = 0,
.extra = &max22017_spi_extra,
.max_speed_hz = 100000,
.platform_ops = &max_spi_ops,
.chip_select = 0,
};
struct no_os_gpio_init_param max22017_rstb_ip = {
.port = 1,
.pull = NO_OS_PULL_NONE,
.number = 6,
.platform_ops = &max_gpio_ops,
.extra = &max22017_gpio_extra,
};
struct max22017_init_param max22017_ip = {
.chip_id = ID_MAX22017,
.comm_param = &max22017_spi_ip,
.crc_en = false,
.ext_dac_ref = false,
.rstb_param = &max22017_rstb_ip,
};
ret = max22017_init(&max22017, &max22017_ip);
if (ret)
goto error;
MAX22017 no-OS IIO Support
The MAX22017 IIO driver comes on top of the MAX22017 driver and offers support for interfacing IIO clients through IIO lib.
MAX22017 IIO Device Configuration
Device Attributes
Channel Attributes
MAX22017 has a total of 2 channel attributes:
raw - the output data to be transmitted to the channel's DACoffset - offset value used for channel's offset calibration
Debug Attributes
The device has a total of 37 debug attributes.
ow_detect - Open Wire detection statusow_detect_available - List of possible options for Open Wire detectiontimeout - Timeout value of the devicetimeout_available - List of possible values for the timeouttimeout_cfg - Timeout Configurationtimeout_cfg_available - List of possible options for the timeout configurationtimeout_en - Timeout enable/disabletimeout_en_available - List of possible options for timeout statusthermal_shutdown - Thermal Shutdown statusthermal_shutdown_available - List of possible options for the thermal shutdown statusovercurrent_shutdown - Overcurrent Shutdown statusovercurrent_shutdown_available - List of possible options for the overcurrrent shutdown statuscurrent_limit - Current Limit valuecurrent_limit_available - List of possible values for current limitdac_ref - DAC reference statusdac_ref_available - List of possible options for the DAC reference statusinterrupts - Interrupts Word valueinterrupts_enable - Interrups Enable Word valueld_ctrl - Load DAC ctrl configurationld_ctrl_available - List of possible options for Load DAC ctrl configurationgain - gain value used for channel's gain calibrationslew_rate - enable/disable slew rateslew_rate_available - list of possible options for slew rate statusrange - Channel's AO slew rate rangerange_available - List of possible ranges depending on the applicationstep_size - Step size of the slew ratestep_size_available - list of possible values for the step sizeupdate_rate - Update rate valuof the Channel's AOupdate_rate_available - List of possible update ratesoperation_mode - Operation mode of the channeloperation_mode_available - List of possible operation modespolarity - Polarity of the channelpolarity_available - List of possible polaritiescm_sense - Common mode sense restistor valuecm_sense_available - List of possible values for the common mode resistorldac - Load DAC statusldac - List of possible options for Load DAC status
Device Channels
MAX22017 has a total of 2 channels.
max22017 IIO Driver Initialization Example
int ret;
struct max22017_iio_desc *max22017_iio_desc;
struct max22017_iio_desc_init_param max22017_iio_ip = {
.max22017_init_param = &max22017_ip,
};
struct iio_app_desc *app;
struct iio_app_init_param app_init_param = { 0 };
ret = max22017_iio_init(&max22017_iio_desc, &max22017_iio_ip);
if (ret)
goto error;
struct iio_app_device iio_devices[] = {
{
.name = "max22017",
.dev = max22017_iio_desc,
.dev_descriptor = max22017_iio_desc->iio_dev,
},
};
app_init_param.devices = iio_devices;
app_init_param.nb_devices = NO_OS_ARRAY_SIZE(iio_devices);
app_init_param.uart_init_params = max22017_uart_ip;
ret = iio_app_init(&app, app_init_param);
if (ret)
goto app_error;
return iio_app_run(app);