adrv902x no-OS Example Project

See projects/adrv902x (doxygen) for the Doxygen documentation.

Supported Parts

Supported Carriers

Overview

This guide is a source of information for system engineers and software developers using the Analog Devices, Inc., ADRV902x family of software defined radio transceivers. This family consists of the ADRV9026 integrated quad RF transceiver and the ADRV9029 integrated quad RF transceiver with digital predistortion (DPD) and crest factor reduction (CFR) capability.

The ADRV9025/ADRV9026/ADRV9029 devices feature four transmitters, four receivers, and dual observation receivers covering a frequency range of 75 MHz to 6 GHz. They integrate JESD204B and JESD204C interfaces for high-speed digital data transfer and ARM Cortex-M3 based firmware (Madura API) for device control.

Driver Layout

The Madura API is located in the no-OS driver directory under:

no-OS/drivers/rf-transceiver/madura/
├── adrv9025.c
├── adrv9025_conv.c
├── adrv9025.h
├── common
│   ├── adi_common.h
│   ├── adi_common_macros.h
│   ├── adi_common_types.h
│   ├── adi_common_user.h
│   ├── adi_error
│   └── adi_logging
├── devices
│   └── adrv9025
└── platforms
    ├── adi_platform.h
    └── adi_platform_types.h

Selecting the JESD Use Case

The JESD use case is selected automatically from the bitstream at configure time - there is normally nothing to edit by hand. scripts/xsa_profile.sh reads the hardware handoff (system.hwh) inside the .xsa and reports which firmware profile the design needs:

  • LINK_MODE 2 in the handoff selects JESD204C, otherwise JESD204B;

  • an axi_adrv9026_rx_os_jesd_rx core means ORx is present;

  • the main-Rx adc_tpl_core NUM_CHANNELS gives the Rx converter count.

CMakeLists.txt uses that result to put exactly one firmware profile directory on the include path and to derive the build-time settings, so #include "ActiveUseCase_profile.h" always resolves to the profile that matches the loaded bitstream:

JESD link mode (from XSA)

ORx

Firmware profile directory

Compile settings

JESD204B

absent

JESD204B_no_ORx

204B

JESD204B

present

JESD204B_ORx

204B

JESD204C

present

JESD204C_ORx

JESD204C_PROFILE

The main-Rx converter count is passed as -DADRV9025_RX_JESD_CONVS_PER_DEVICE=<n> and the 204C profile also defines JESD204C_PROFILE; app_config.h picks up both, so those axes need no manual editing. If the XSA asks for a profile whose directory is missing, the configure step stops with an error telling you which one to generate.

Adding or Updating a Use Case

You only need these steps to introduce a new profile directory or refresh an existing one from Madura TES:

  1. From the Madura TES GUI, generate the resources folder that contains the files listed below:

    • Firmware files (ADRV9025_FW.bin and ADRV9025_DPDCORE_FW.bin),

    • Stream binary (e.g., stream_image_6E3E00EFB74FE7D465FA88A171B81B8F.bin),

    • ActiveUseCase.profile and ActiveUtilInit.profile.

  2. no-OS cannot read files at runtime, so the .bin files are committed as C arrays. These are shared across all profiles and live at the root of src/common/firmware/. Regenerate them only when the firmware or stream image itself changes:

    xxd -i ADRV9025_FW.bin > ADRV9025_FW.h
    

    Copy the generated unsigned char array into the corresponding header file in the project structure (ADRV9025_FW.h, ADRV9025_DPDCORE_FW.h or ADRV9025_stream_image.h).

  3. Convert the .profile JSON into the header the firmware expects with profile_to_header.py, writing it into the profile directory that xsa_profile.sh selects for the target bitstream:

    scripts/profile_to_header.py ActiveUseCase.profile \
        src/common/firmware/JESD204C_ORx/ActiveUseCase_profile.h
    

    profile_to_header.py is whitespace-exact - round-tripping an unchanged .profile reproduces the committed header byte-for-byte, so it doubles as a parity check against the Linux firmware/*.profile the same bitstream is validated against. (The older json2cstring.sh only adds the C-string wrapper for a file literally named ActiveUseCase.profile; prefer the Python script for the per-profile headers.) ActiveUtilInit_profile.h is shared and lives at the firmware root.

  4. Build the project. The profile is selected from the XSA; no source edit is required.

No-OS Supported Examples

The demo applications highlight the functionality of the adrv902x evaluation board. Three example variants are provided in the project:

Basic Example

The basic example (variant basic_example) simply initializes the components on the evaluation board and enables a JESD link. TX will transmit a DDS waveform with the default parameters set by the DAC driver. The output looks like the one below:

adrv9025-phy Rev 0, API version: 7.0.0.14 found
tx_adxcvr: OK (9830400 kHz)
rx_adxcvr: OK (9830400 kHz)
adrv9025-phy Rev 176, Firmware 7.0.0.11 API version: 7.0.0.14 Stream version: 9.4.0.1 successfully initialized via jesd204-fsm
tx_jesd status:
    Link is enabled
    Measured Link Clock: 245.760 MHz
    Reported Link Clock: 245.760 MHz
    Measured Device Clock: 245.760 MHz
    Reported Device Clock: 245.760 MHz
    Desired Device Clock: 245.760 MHz
    Lane rate: 9830.400 MHz
    Lane rate / 40: 245.760 MHz
    LMFC rate: 7.680 MHz
    SYNC~: deasserted
    Link status: DATA
    SYSREF captured: Yes
    SYSREF alignment error: No
rx_jesd status:
    Link is enabled
    Measured Link Clock: 245.760 MHz
    Reported Link Clock: 245.760 MHz
    Measured Device Clock: 122.881 MHz
    Reported Device Clock: 122.880 MHz
    Desired Device Clock: 122.880 MHz
    Lane rate: 9830.400 MHz
    Lane rate / 40: 245.760 MHz
    LMFC rate: 3.840 MHz
    Link status: DATA
    SYSREF captured: Yes
    SYSREF alignment error: No
Bye

By default axi_jesd204_rx_status_read() prints link-level information only. To also print the per-lane details (CGS/ILAS state, lane errors and the decoded link parameters for every RX/ORx lane), build with the JESD204_DUMP_LANE_STATUS define. It must be set on the no-os target, because the JESD204 driver is compiled into the library rather than the application:

target_compile_definitions(no-os PUBLIC JESD204_DUMP_LANE_STATUS)

This applies to all three example variants (and to any project that calls the status read). TX has no per-lane status; ORx uses the RX driver and is covered by the same define.

DMA Example

The DMA example (variant dma_example) sends a sine wave on TX channels using DMA from a lookup table. If you physically loopback a TX channel to an RX channel via an electrical wire, you may run the DMA example and read the received data at RX from its particular memory address.

After the output from the basic example, the application will eventually print something like this:

DMA_EXAMPLE Tx: address=0x1dc900 samples=8192 channels=8 bits=32
DMA_EXAMPLE Rx: address=0x1e4900 samples=65536 channels=8 bits=16

This means that the memory address where the data at RX is stored is 0x1e4900. There are a total of 65536 samples, 16-bit wide across 8 channels, which is equivalent to 8192, 16-bit samples per channel. The location of the transmitted data is also given (0x1dc900).

At this point you may use a Tcl script to retrieve data from memory and store it into .csv files for processing:

# ZCU102 (ZynqMP APU)
xsct tools/scripts/platform/xilinx/capture.tcl ZYNQ_PSU 0x1e4900 65536 8 16

# VCU118 (MicroBlaze) - pass MICROBLAZE as the processor type instead
xsct tools/scripts/platform/xilinx/capture.tcl MICROBLAZE 0x1e4900 65536 8 16

You can find more information about the data here.

The data in the .csv files generated can be visualised using the plot.py script in the no-OS repository. The following command will display the data on all 8 channels:

python tools/scripts/platform/xilinx/plot.py 8

IIO Example

The IIO example (variant iio_example) launches a IIOD server on the board so that the user may connect to it via an IIO client. Using iio-oscilloscope, the user can configure the DAC and view the ADC data on a plot.

If you are not familiar with ADI IIO Application, please take a look at: IIO No-OS

If you are not familiar with ADI IIO-Oscilloscope Client, please take a look at: IIO Oscilloscope

To run the IIOD demo, connect to the board via UART with the following settings:

Baud Rate: 115200bps
Data: 8 bit
Parity: None
Stop bits: 1 bit
Flow Control: none

After the link bring-up messages, the application will eventually print:

Running IIOD server...
If successful, you may connect an IIO client application by:
1. Disconnecting the serial terminal you use to view this message.
2. Connecting the IIO client application using the serial backend configured as shown:
    Baudrate: 115200
    Data size: 8 bits
    Parity: none
    Stop bits: 1
    Flow control: none

This message implies a IIOD server is being run and you may connect to it using a serial-backend enabled iio-oscilloscope with the settings indicated at the serial terminal.

No-OS Supported Platforms

Xilinx

Used Hardware

Connections

Connect the adrv902x evaluation board to the correct FMC connector on the ZCU102 carrier board before programming it. Connect a USB cable to the carrier board USB-UART port and the host PC for serial console access at 115200 baud, 8N1.

Build Command

The Xilinx platform uses the CMake/Ninja build system via the no_os_build.py helper script. Available variants: basic_example, dma_example, iio_example. Available boards: zcu102, vcu118.

The ZCU102 runs on the ZynqMP APU (Cortex-A53); the VCU118 runs on a MicroBlaze soft-core. The build selects the toolchain and any core-specific workarounds from the XSA automatically, so the only difference is the --board argument and its matching hardware handoff.

A Xilinx XSA hardware description file is required. The HDL design name is adrv9026; the hardware name is composed as adrv9026_<board> (e.g. adrv9026_zcu102 or adrv9026_vcu118).

For toolchain setup and prerequisites, see the Xilinx CMake build guide.

# Source the Vitis toolchain environment
source ~/.xilinx/2025.1/Vitis/settings64.sh
# PowerShell (Windows) equivalent:
#   & "$env:USERPROFILE\.xilinx\2025.1\Vitis\settings64.bat"

cd no-OS

# Build the basic example for ZCU102
python tools/scripts/no_os_build.py build \
    --project adrv902x --variant basic_example --board zcu102 \
    --hardware /path/to/adrv9026_zcu102/system_top.xsa

# Build and flash via JTAG
python tools/scripts/no_os_build.py build \
    --project adrv902x --variant basic_example --board zcu102 \
    --hardware /path/to/adrv9026_zcu102/system_top.xsa \
    --probe openocd --flash

# Build the DMA example for ZCU102
python tools/scripts/no_os_build.py build \
    --project adrv902x --variant dma_example --board zcu102 \
    --hardware /path/to/adrv9026_zcu102/system_top.xsa

# Build the IIO example for ZCU102
python tools/scripts/no_os_build.py build \
    --project adrv902x --variant iio_example --board zcu102 \
    --hardware /path/to/adrv9026_zcu102/system_top.xsa

# Build (and flash) an example for VCU118 - only --board and --hardware
# change; the same command shape works for every variant
python tools/scripts/no_os_build.py build \
    --project adrv902x --variant basic_example --board vcu118 \
    --hardware /path/to/adrv9026_vcu118/system_top.xsa