AD9739A no-OS Driver
See drivers/dac/ad9739a (doxygen) for the Doxygen documentation.
Supported Devices
Overview
The AD9739A is a 14-bit RF digital-to-analog converter (DAC), capable of creating wideband signals from DC to 3 GHz. Featuring an update rate up to 2.5 GSPS, this device is ideal for broadband communications, military jamming, instrumentation, and radar systems. It features low-voltage differential signaling (LVDS) for enhanced data and signal quality, advanced clock management with delay lock loops (DLL) for optimized timing, crucial for high-speed data transfer, and minimizes signal distortion. Its dynamic performance is highlighted by Spurious-Free Dynamic Range (SFDR) and Intermodulation Distortion (IMD). Integration is streamlined by flexible initialization via SPI configurations for reliable operation in complex systems.
Applications
Broadband communications systems
DOCSIS CMTS systems
Military jammers
Instrumentation, automatic test equipment
Radar, avionics
Operation Modes
The AD9739A supports the following operation modes:
Normal Baseband Mode: Standard DAC output mode for baseband signal generation.
Mix Mode: Enables the DAC to operate in mix-mode for direct RF synthesis applications.
Sleep Mode: Reduces power consumption by placing the DAC in a low-power state.
Device Configuration
The ad9739a_setup function initializes the AD9739A device by first
allocating memory using no_os_malloc, then establishing SPI
communication through no_os_spi_init, and confirming the device ID via
ad9739a_read. It proceeds to configure various registers using
ad9739a_write and performs a device reset with ad9739a_reset. To ensure
the MU controller and LVDS receiver are properly locked and operational,
the function repeatedly writes to specific registers and checks their
status, incorporating delay_fdata_cycles for timing control.
Additionally, it sets the DAC's full-scale current using
ad9739a_dac_fs_current, displays a success message, and returns the
initialized device structure.
Initialization and Cleanup
The initialization and cleanup functions prepare the device for
operation and ensure proper resource management. The ad9739a_setup()
function initializes the AD9739A DAC by configuring its SPI interface,
verifying the device ID, setting up the MU controller, configuring the
LVDS receiver, and establishing the full-scale output current. After the
device has served its purpose, the ad9739a_remove() function is used
to deallocate resources by removing the SPI descriptor and freeing
allocated memory. Together, these functions ensure that the device is
correctly integrated into a system during initialization and safely
removed when no longer needed.
Register Communication Functions
For basic register access, the driver provides functions that facilitate
SPI-based communication with the AD9739A DAC registers. The
ad9739a_write() function constructs and sends SPI commands needed to
update register values, while the ad9739a_read() function retrieves
register values using similarly structured SPI transactions. These two
functions abstract the low-level details of SPI communication to provide
a simple and effective API for register read and write operations.
Reset and Power Management
Robust operation of the device requires efficient management of its
reset and power states. The ad9739a_reset() function performs a
software reset by writing commands that restore default settings,
thereby clearing the device's reset state. Complementing this, the
ad9739a_power_down() function is used to manage the device's power
configuration by either applying a new power setting or retrieving the
current power status when invalid configurations are provided. These
functions allow high-level control over device resets and power
sequences in a streamlined, consistent manner.
Mode and Output Current Configuration
For fine-tuning the DAC's operational behavior, the driver includes
functions that adjust both the operational mode and the full-scale
output current. The ad9739a_operation_mode() function selects among different
operational modes—such as normal baseband mode or mixed mode—by
configuring the device's mode register, and it also supports reading the
current mode setting. In addition, the ad9739a_dac_fs_current()
function configures or retrieves the DAC's full-scale output current.
Together, these functions provide the flexibility needed to tailor the
device's performance to diverse application requirements.
Timing and Delay Control
Precise timing control is critical for synchronizing DAC operations, and
the driver addresses this need with a dedicated function. The
delay_fdata_cycles() function introduces a delay based on a
specified number of DAC cycles, effectively translating cycle counts
into controlled timing delays. This functionality is essential for
ensuring proper synchronization across the device's operations.
Driver Initialization Example
#include <stdlib.h>
#include <stdio.h>
#include "ad9739a.h"
#include "no_os_spi.h"
#include "no_os_alloc.h"
int main(void)
{
struct ad9739a_dev *device;
int32_t status;
struct ad9739a_init_param init_param = {
.spi_init = {
.device_id = 0,
.max_speed_hz = 10000000,
.chip_select = 0,
.mode = NO_OS_SPI_MODE_0,
.platform_ops = &xil_spi_ops,
.extra = &xil_spi_param,
},
.common_mode_voltage_dacclk_p = 0xF,
.common_mode_voltage_dacclk_n = 0xF,
.full_scale_current = 20.0,
};
status = ad9739a_setup(&device, init_param);
if (status < 0) {
printf("AD9739A initialization failed.\n");
goto error;
}
printf("AD9739A initialization successful.\n");
error:
ad9739a_remove(device);
return status;
}