XSA to Device Tree

The adidt.xsa subpackage converts Vivado .xsa archives into Linux Device Tree sources for ADI JESD204 FSM-framework designs.

Overview

The pipeline performs five stages:

  1. SDT generation – invokes lopper (sdtgen) as a subprocess to produce a base System Device Tree from the .xsa.

  2. XSA parsing – extracts the Vivado hardware handoff (.hwh XML) from the .xsa ZIP and detects ADI AXI IPs (JESD204 controllers, clock generators, converters).

  3. Node building – each board builder constructs a BoardModel (see Board Model) from the XSA topology and config, then renders it to DTS node strings via Jinja2 templates. The BoardModel is editable before rendering — callers can modify clock dividers, JESD parameters, or GPIO mappings programmatically.

  4. DTS merging – inserts the rendered nodes into the base DTS, producing both a standalone overlay (.dtso) and a fully merged (.dts).

  5. HTML visualization – generates a self-contained interactive report with D3.js topology, clock tree, and JESD204 parameter panels.

  6. Clock graph – parses clocks / clock-names / clock-output-names properties from the merged DTS and writes directed clock-distribution graphs in Graphviz DOT and D2 formats (SVG rendered automatically when dot / d2 are available on PATH).

Pipeline diagram

XSA to device tree pipeline XSA to device tree pipeline

Base DTS and Overlay Structure

The pipeline produces two output files: a merged DTS (.dts) and a standalone overlay (.dtso). Understanding what each contains — and what the base DTS from sdtgen provides — is important when debugging boot failures or integrating with custom HDL designs.

Base DTS (from sdtgen / lopper)

sdtgen generates a System Device Tree from the .hwh hardware handoff inside the .xsa archive. The base includes:

  • The root / node with board and FPGA part identifiers.

  • The amba_pl bus (simple-bus) containing every AXI IP in the Vivado block design — JESD204 controllers, DMA engines, SPI controllers, UART, Ethernet, GPIO, timer, interrupt controller, clock generators, transceivers, and memory controllers.

  • Each IP node has compatible = "xlnx,...", reg, interrupts, and Xilinx-specific properties (xlnx,ip-name, xlnx,num-lanes, etc.) derived from the HWH.

  • CPU and memory nodes (cpus, memory@...), chosen with stdout-path and bootargs, and aliases for serial/SPI/I2C.

  • Clock infrastructure: fixed-clock nodes and clk_bus_0 providing the AXI bus clock.

  • For MicroBlaze designs: the address-map property on the CPU node listing all accessible peripherals.

The base DTS nodes use Xilinx generic compatible strings (xlnx,axi-jesd204-rx-1.0, xlnx,axi-dmac-1.0, etc.) and lack ADI-driver-specific properties. The kernel can parse these nodes but ADI drivers will not probe without the correct adi,... compatible and configuration properties.

What the pipeline adds (overlay / merged nodes)

The NodeBuilder renders ADI-specific DTS content that either replaces or augments nodes from the base:

New nodes (inserted into the bus):

  • AXI clock generators — adi,axi-clkgen-2.00.a nodes with #clock-cells, clock-output-names, and bus clock references.

  • Fixed clocks — e.g. clkin_125 for external reference oscillators not described in the HWH.

New SPI device child nodes:

  • Clock chips — HMC7044 (adi,hmc7044), AD9523-1 (adi,ad9523-1), or AD9528 (adi,ad9528) with PLL, VCXO, channel dividers, and JESD204 sysref-provider configuration.

  • PLLs — ADF4382 (adi,adf4382) for converter device clocks.

  • Converters — AD9084 (adi,ad9084), AD9081 (adi,ad9081), AD9680, AD9144, ADRV9009, etc., with JESD204 link parameters, firmware names, lane mappings, and GPIO connections.

These appear inside &spi_bus { ... } overlay blocks that add children to the SPI controller nodes already present in the base.

Overlay property additions (&label { ... } blocks):

  • DMA engines — adds adi,axi-dmac-1.00.a compatible and #dma-cells to the existing DMA nodes.

  • ADXCVR transceivers — adds adi,axi-adxcvr-1.0 compatible, adi,sys-clk-select, adi,out-clk-select, clock references, and JESD204 input chain links.

  • JESD204 controllers — adds adi,axi-jesd204-rx-1.0 (or -tx-), adi,octets-per-frame, adi,frames-per-multiframe, and the full jesd204-device / jesd204-inputs FSM framework properties.

  • TPL cores — adds adi,axi-ad9081-rx-1.0 (or board-specific variant), DMA links, and converter associations.

  • HSCI — adds adi,axi-hsci-1.0.a and interface speed for high-speed converter interface blocks.

Board fixups (applied to the base before merging):

Some base DTS nodes require corrections that sdtgen cannot derive from the HWH alone. The board_fixups.py registry applies platform-specific patches — for example, VCU118 Ethernet PHY configuration and IIO device name normalization.

Assumptions about the base DTS

The pipeline expects the sdtgen-generated base to provide:

  1. An amba_pl (or amba) bus node as the top-level container.

  2. Labeled nodes for every AXI IP that the overlay will reference (axi_apollo_rx_dma, axi_apollo_rx_xcvr, etc.). The labels are derived from the Vivado block design instance names.

  3. A clk_bus_0 fixed-clock node providing the AXI bus clock frequency.

  4. Correct #address-cells and #size-cells on the bus (1 for MicroBlaze/VCU118, 2 for ZynqMP/ZCU102).

  5. For MicroBlaze: a cpus node, memory node with device_type, and chosen with bootargs = "earlycon" and stdout-path pointing to the UART. The SdtgenRunner applies fixups to ensure these are present.

If the XSA comes from an ADI HDL reference design, these assumptions hold automatically. Custom designs must follow the same naming conventions for the overlay labels to resolve.

Merged vs overlay output

  • The merged DTS (.dts) combines the base and overlay into a single file with #include "pl.dtsi" for the base, followed by the generated ADI nodes and &label { ... } augmentations. Compile it with cpp + dtc to produce a standalone DTB.

  • The overlay (.dtso) is a /plugin/; file that can be applied at runtime via dtoverlay on systems that support dynamic DT overlays. It contains the same ADI nodes but uses &amba_pl { ... } to target the bus node.

For MicroBlaze simpleImage targets, use the merged DTS — overlays require a base DTB that the bootloader applies the overlay to, which MicroBlaze’s direct-boot flow does not support.

Hardware Test Flow

The hardware tests consume a prepared kernel from the pinned DataX adi-linux target together with the DTB generated from the XSA pipeline. See Hardware CI for kernel preparation and explicit overrides.

Hardware testing workflow Hardware testing workflow

Example hardware invocation:

source /tools/Xilinx/2025.1/Vivado/settings64.sh
LG_ENV=/jenkins/lg_ad9081_zcu102.yaml ADI_XSA_BUILD_KERNEL=1 \
  pytest -q test/hw/ad9081/test_ad9081_xsa_hw_m4_l8.py

Installation

The XSA pipeline requires lopper (the Xilinx System Device Tree generator). Install the optional dependency group:

pip install "pyadi-dt[xsa]"

Usage

Start with the step-by-step tutorial before tuning profiles:

python examples/xsa/adrv9009_zcu102.py --xsa /path/to/design.xsa

or use the full-page tutorial at XSA Flow Tutorials and the adijif-focused guide XSA + adijif Tutorial.

Run the pipeline from the CLI:

adidtc xsa2dt -x design.xsa -c config.json -o out/

Select an explicit board profile (optional):

adidtc xsa2dt -x design.xsa -c config.json --profile ad9081_zcu102 -o out/

Generate manifest parity reports from a reference DTS root:

adidtc xsa2dt -x design.xsa -c config.json -o out/ \
  --reference-dts zynqmp-zcu102-rev10-ad9081-m8-l4.dts

Enable strict parity mode to fail generation when required roles are missing:

adidtc xsa2dt -x design.xsa -c config.json -o out/ \
  --reference-dts zynqmp-zcu102-rev10-ad9081-m8-l4.dts \
  --strict-parity

List available built-in profiles:

adidtc xsa-profiles

Show one profile and its defaults:

adidtc xsa-profile-show ad9081_zcu102

Built-in profiles

Profile availability and hardware qualification are separate. See Release hardware validation for the tested candidate, including ZU11EG generated-DTB boot and bounded runtime overlay validation.

Profile

Converter Family

Platform

JESD in Profile

Board Config Key

ad9081_zcu102

AD9081 MxFE

ZCU102

No (supply via cfg)

ad9081_board

ad9081_zc706

AD9081 MxFE

ZC706

No (supply via cfg)

ad9081_board

ad9081_vpk180

AD9081 MxFE

VPK180

Yes (JESD204C M8/L8)

ad9081_board

ad9082_zcu102

AD9082 MxFE

ZCU102

No (supply via cfg)

ad9081_board

ad9083_zcu102

AD9083 MxFE

ZCU102

No (supply via cfg)

ad9081_board

ad9084_vcu118

AD9084

VCU118

Yes

ad9084_board

ad9172_zcu102

AD9172 DAC

ZCU102

Yes

ad9172_board

adrv9009_zcu102

ADRV9009

ZCU102

No (supply via cfg)

adrv9009_board

adrv9009_zc706

ADRV9009

ZC706

No (supply via cfg)

adrv9009_board

adrv9009_zu11eg

Dual ADRV9009 SoM

ZU11EG / ADRV2CRR-FMC

No (supply via cfg)

adrv9009_board

adrv9025_zcu102

ADRV9025

ZCU102

No (supply via cfg)

adrv9009_board

adrv9008_zcu102

ADRV9008

ZCU102

No (supply via cfg)

adrv9009_board

adrv9008_zc706

ADRV9008

ZC706

No (supply via cfg)

adrv9009_board

adrv937x_zcu102

ADRV937x

ZCU102

No (supply via cfg)

adrv9009_board

adrv937x_zc706

ADRV937x

ZC706

No (supply via cfg)

adrv9009_board

adrv9002_zc706

ADRV9002

ZC706

No (supply via cfg)

—

adrv9003_zcu102

ADRV9003 (Navassa)

ZCU102

No (supply via cfg)

adrv9003_board

adrv9003_zc706

ADRV9003 (Navassa)

ZC706

No (supply via cfg)

adrv9003_board

fmcdaq2_zcu102

FMCDAQ2

ZCU102

No (supply via cfg)

fmcdaq2_board

fmcdaq2_zc706

FMCDAQ2

ZC706

No (supply via cfg)

fmcdaq2_board

fmcdaq3_zcu102

FMCDAQ3

ZCU102

Yes

fmcdaq3_board

fmcdaq3_zc706

FMCDAQ3

ZC706

Yes

fmcdaq3_board

fmcdaq3_vcu118

FMCDAQ3

VCU118 (MicroBlaze)

Yes

fmcdaq3_board

Profiles with “JESD in Profile = Yes” include default JESD framing parameters (F, K, M, L, Np, S) and can be used with cfg={} — no user config needed. Profiles with “No” require JESD parameters to be supplied via the cfg dict, typically from a pyadi-jif solver or manual configuration.

Profile discovery

Use the CLI to browse profiles without reading JSON files directly:

adidtc xsa-profiles                   # list all available profiles
adidtc xsa-profile-show ad9081_zcu102  # show defaults as JSON

The MCP server exposes the same data via list_xsa_profiles() and show_xsa_profile().

Profile selection

When profile is not given, the pipeline picks one in two steps:

  1. HDL design identity. Every bitstream built from ADI HDL initialises its system-ID ROM from projects/<project>/<carrier>[/<variant>]/mem_init_sys.txt, and that path is kept in the XSA. The parser exposes it as XsaTopology.hdl_project, hdl_carrier and hdl_variant. A profile whose design section names the same project, carrier and variant is selected. This tells apart designs whose netlists look alike (AD9081 and AD9082) and parts built from one project (dac_fmc_ebz).

  2. Converter family. Otherwise the profile named <converter_family>_<platform> is used, as before.

Declarative design profiles

Most HDL designs need no bespoke builder: their device tree is a fixed set of PL cores plus the devices on the PS SPI/I2C buses. A profile can describe those nodes directly in a design section, which DeclarativeBuilder renders in place of the family builders:

{
  "name": "ad9083_evb_zcu102",
  "defaults": {},
  "design": {
    "project": "ad9083_evb", "carrier": "zcu102", "variant": "",
    "reference": "arch/arm64/boot/dts/xilinx/zynqmp-zcu102-rev10-ad9083-fmc-ebz.dts",
    "pl": [
      {
        "instance": "axi_ad9083_rx_dma",
        "labels": ["rx_dma"],
        "node": "dma-controller",
        "reg": [[0, 65536]],
        "interrupt_flags": 4,
        "body": ["compatible = \"adi,axi-dmac-1.00.a\";", "#dma-cells = <1>;"]
      }
    ],
    "root": ["clocks {", "\t...", "};"],
    "overlays": [{"target": "&spi0", "body": ["status = \"okay\";", "..."]}],
    "notes": []
  }
}
pl

One entry per PL core. instance is the IP instance name in the XSA; the node’s unit address, reg (offsets and sizes relative to the instance’s base address) and interrupt number are taken from that instance when the tree is generated. If the XSA lacks a named instance, generation fails with ProfileError rather than describing hardware the bitstream does not contain. The stub sdtgen generated for the same instance is deleted.

root

Lines added to the root node (fixed clocks, regulators).

overlays

Blocks applied to nodes of the base tree, such as the PS SPI bus the converter sits on.

notes

What the seeder dropped, created or overrode; read these when reviewing a profile.

These profiles are seeded from the kernel reference tree of the matching release rather than written by hand:

python scripts/seed_declarative_profile.py \
    --inventory adidt/xsa/config/hdl_2026_r1_designs.json \
    --linux ~/dev/linux \
    --xsa-cache ~/.cache/adidt/kuiper/2026_r1_xsa \
    --only 'zynqmp-zcu102-rev10-ad9083*'

The seeder separates the design’s nodes from the carrier’s by source file, matches every PL node to the XSA instance at its address, and pulls in any carrier node the design refers to that the sdtgen base tree does not provide. Where the reference and the XSA disagree on an interrupt, the XSA wins and the difference is recorded in notes.

Boards that share a bitstream

Some boards differ only in the part fitted (the pulsar_adc ZedBoard design serves a dozen ADCs). No XSA can tell them apart, so the first reference tree seeded for a bitstream is its default profile and the others are selected by name:

adidtc xsa2dt -x system_top.xsa -c cfg.json --profile pulsar_adc_zed_ad4020
Designs without a released XSA

Passing --base-for <carrier>=<system-top.dts> also seeds designs the release ships no XSA for, borrowing an sdtgen base tree of another design on the same carrier. Their PL entries carry an address instead of an instance and are bound to an IP only when a tree is generated; such profiles are marked "validated": false.

See HDL 2026.1 design support for the state of every design in the release.

Reference DTS parity checking

When migrating from a hand-written DTS or validating against a known-good reference (e.g. the Kuiper release DTS), the pipeline can compare the generated output against a reference and report missing roles, links, and properties.

adidtc xsa2dt -x design.xsa -c config.json -o out/ \
  --reference-dts zynqmp-zcu102-rev10-ad9081-m8-l4.dts

This produces a _map.json and _coverage.json alongside the DTS output showing which driver requirements from the reference are present in the generated tree.

Add --strict-parity to fail the pipeline when required roles or properties are missing — useful in CI to prevent regressions:

adidtc xsa2dt -x design.xsa -c config.json -o out/ \
  --reference-dts ref.dts --strict-parity

The parity checker extracts a driver manifest from the reference DTS: required IIO device roles, phandle links (clocks, JESD204 inputs), and property values. It then verifies each requirement against the generated merged DTS. Any gaps appear in the coverage report and, with --strict-parity, raise a ParityError.

Or call the pipeline directly from Python:

from pathlib import Path
from adidt.xsa.pipeline import XsaPipeline
import json

cfg = json.loads(Path("config.json").read_text())
results = XsaPipeline().run(
    xsa_path=Path("design.xsa"),
    cfg=cfg,
    output_dir=Path("out/"),
)
print(results["merged"])       # Path to the merged .dts
print(results["report"])       # Path to the HTML visualization
print(results["clock_dot"])    # Path to the Graphviz clock-tree .dot
print(results["clock_d2"])     # Path to the D2 clock-tree .d2
# SVG paths are present only when the rendering tool is installed:
# results["clock_dot_svg"], results["clock_d2_svg"]

PetaLinux integration

The XSA pipeline can generate PetaLinux-ready system-user.dtsi files. See PetaLinux Integration for the full workflow, diagrams, and troubleshooting guide.

Quick example:

adidtc xsa2dt -x design.xsa -c cfg.json --format petalinux \
    --petalinux-project /path/to/myproject

Python API

Core classes and methods used in the XSA flow:

API

Purpose

XsaParser.parse(xsa_path: Path) -> XsaTopology

Extracts .hwh from the XSA and returns discovered JESD, clockgen, converter, connectivity, and part metadata.

NodeBuilder.build(topology: XsaTopology, cfg: dict) -> dict[str, list[str]]

Dispatches to board builders, each constructing a BoardModel and rendering it via BoardModelRenderer.

BoardModelRenderer.render(model: BoardModel) -> dict[str, list[str]]

Renders a BoardModel to DTS node strings using per-component Jinja2 templates. See Board Model.

DtsMerger.merge(base_dts: str, nodes: dict, output_dir: Path, name: str)

Produces <name>.dtso overlay + <name>.dts merged full tree.

HtmlVisualizer.generate(topology, cfg, merged_content, output_dir, name)

Writes self-contained HTML debug report with topology and clock links.

ClockGraphGenerator.generate(merged_dts, output_dir, name) -> dict[str, Path]

Parses clock properties from the merged DTS and writes .dot and .d2 clock-tree diagrams; renders SVG when dot / d2 are on PATH.

XsaPipeline.run(...) -> dict[str, Path]

Orchestrates all stages end-to-end and returns artifact paths.

XsaPipeline.run argument reference

Argument

Type

Description

xsa_path

Path

Vivado hardware handoff archive (must contain one .hwh).

cfg

dict

Runtime configuration (JESD, clock labels/channels, board overrides).

output_dir

Path

Output folder for base SDT, overlay/merged DTS, and report artifacts.

sdtgen_timeout

int

Timeout (seconds) for SDT generation subprocess.

profile

str | None

Optional explicit built-in/custom profile name.

reference_dts

Path | None

Optional DTS root for manifest-parity checks and coverage artifacts.

strict_parity

bool

If true, raises ParityError when required roles/links/properties are missing/mismatched.

emit_report

bool

When True (default), writes the <name>_report.html topology report and includes "report" in the result dict.

emit_clock_graphs

bool

When True (default), writes the Graphviz .dot and D2 .d2 clock-tree diagrams and attempts to render them to SVG when dot / d2 are on PATH.

lint

bool

When True, runs the structural DTS linter on the merged output and writes a diagnostics JSON file. Default False.

strict_lint

bool

When True, raises DtsLintError if the linter finds any errors. Implies lint=True. Default False.

output_format

str

"default" produces the standard overlay + merged DTS. "petalinux" additionally writes system-user.dtsi and device-tree.bbappend for drop-in use in a PetaLinux project. Default "default".

Tip

The cfg argument accepts either a plain dict or a PipelineConfig object. PipelineConfig.from_dict(d) provides typed access to JESD, clock, and board-specific settings with auto-detection of board config keys. See PipelineConfig in the API reference.

Using adijif (pyadi-jif) With the XSA Flow

The intended integration is:

  1. Use adijif to select/solve JESD and clock settings.

  2. Translate solved values into cfg keys expected by XsaPipeline.

  3. Run XsaPipeline with either explicit profile or auto-profile.

  4. Compile the generated merged DTS to DTB and deploy/test on hardware.

adijif integration workflow

adijif integration workflow adijif integration workflow

adijif-to-config mapping

adijif output

cfg key in XSA flow

RX JESD F, K, M, L, Np, S

cfg["jesd"]["rx"]

TX JESD F, K, M, L, Np, S

cfg["jesd"]["tx"]

RX device clock source choice

cfg["clock"]["rx_device_clk_label"] (for example clkgen/hmc7044)

TX device clock source choice

cfg["clock"]["tx_device_clk_label"]

HMC/clock output channel for RX

cfg["clock"]["hmc7044_rx_channel"]

HMC/clock output channel for TX

cfg["clock"]["hmc7044_tx_channel"]

Board wiring specifics (SPI/CS/GPIO/link IDs)

ad9081_board / adrv9009_board / fmcdaq2_board profile keys

Reference implementation

Use the ADRV9009 example for a complete adijif-driven flow:

  • examples/xsa/adrv9009_zcu102.py

For ADRV9025 ZCU102 XSA flows (Kuiper/local XSA), use:

  • examples/xsa/adrv9025_zcu102.py

The script demonstrates both quick-mode JESD extraction and optional solve() usage, then feeds those values directly into XsaPipeline.

You can also pass profile="ad9081_zcu102" (or another built-in profile) to XsaPipeline.run(). If no profile is passed, the pipeline will auto-select a matching profile when available (for example, ad9081_zcu102).

For AD9082 Kuiper projects, prefer explicit profile selection: profile="ad9082_zcu102". AD9081/AD9082 designs often share mxfe JESD instance names, so topology-only auto-inference is ambiguous.

For AD9083 Kuiper projects, prefer explicit profile selection: profile="ad9083_zcu102" for the same reason (shared mxfe naming).

For AD9081 ZC706 Kuiper projects, use: profile="ad9081_zc706".

For AD9172 Kuiper projects, use explicit profile selection: profile="ad9172_zcu102". XSA provides JESD/clock transport topology while SPI-attached DAC/clock chip details require board-specific overlays.

Auto-selection also covers FMCDAQ2 variants:

  • fmcdaq2_zcu102 (ZynqMP/ZCU102)

  • fmcdaq2_zc706 (Zynq-7000/ZC706)

FMCDAQ3 variants are available via explicit profiles:

  • fmcdaq3_zcu102 (ZynqMP / ZCU102)

  • fmcdaq3_zc706 (Zynq-7000 / ZC706)

  • fmcdaq3_vcu118 (MicroBlaze / VCU118)

Current FMCDAQ3 support focuses on JESD/clock transport defaults and artifact generation; board-specific SPI device overlay content remains to be extended. The VCU118 variant ships with a coordinator-based boot smoke test (test/hw/test_fmcdaq3_vcu118_hw.py) that drives the prebuilt Kuiper simpleImage.vcu118_fmcdaq3.strip over JTAG via BootFabric.

ADRV family profile variants include:

  • adrv9008_zcu102

  • adrv9008_zc706

  • adrv9002_zc706

  • adrv9003_zcu102

  • adrv9003_zc706

  • adrv9009_zc706

  • adrv9009_zcu102

  • adrv937x_zc706

  • adrv937x_zcu102

  • adrv9025_zcu102 (also selected from adrv9026-named JESD labels)

The adrv9009_zcu102 profile also supports the AD-FMCOMMS8-EBZ (FMComms8) dual-chip design. When the XSA topology is detected as FMComms8 layout (two ADRV9009 transceivers sharing one SPI bus), the pipeline generates a second PHY node (trx1_adrv9009) with independent HMC7044 channel assignments per chip:

  • trx0 (adrv9009-x2): uses HMC7044 channels 0/1 (dev/sysref) and 6 (FPGA sysref)

  • trx1 (adrv9009): uses HMC7044 channels 2/3 (dev/sysref) and 7 (FPGA sysref)

Hardware tests verify that both adrv9009-phy IIO devices appear in the IIO context.

For ADRV9008 Kuiper projects, prefer explicit profile selection: profile="adrv9008_zcu102". Many ADRV9008 XSAs use ADRV9009-style JESD/IP instance names, which makes converter-family auto-inference ambiguous.

AD9084 (Apollo) VCU118 MicroBlaze support

The pipeline supports AD9084 “apollo” dual-link designs on VCU118 (MicroBlaze). These designs feature four JESD204C links (RX A/B + TX A/B) with separate XCVR, DMA, and TPL cores per link. The board builder generates nodes for:

  • ADF4382 PLL (reference clock for AD9084 dev_clk)

  • HMC7044 clock distributor (JESD reference clocks, SYSREF)

  • HSCI high-speed connector interface

  • JESD204 overlay nodes with 4-clock config (s_axi_aclk, link_clk, device_clk, lane_clk) and per-link device clock from HMC7044 channels

  • AD9084 converter node with profile firmware, lane mappings, and HSCI

The built-in ad9084_vcu118 profile encodes the AD9084-EBZ board wiring for the HMC7044 + AD9084 + ADF4382 combination. When the pipeline sees an AD9084 design on VCU118 it now auto-applies those defaults unless the caller overrides them explicitly.

Configuration uses the ad9084_board key with JESD204 link IDs from dt-bindings/iio/adc/adi,ad9088.h:

cfg = {
    "jesd": {
        "rx": {"F": 6, "K": 32, "M": 4, "L": 8, "Np": 12, "S": 1},
        "tx": {"F": 6, "K": 32, "M": 4, "L": 8, "Np": 12, "S": 1},
    },
    "clock": {
        "rx_device_clk_label": "hmc7044",
        "rx_device_clk_index": 8,
        "tx_device_clk_label": "hmc7044",
        "tx_device_clk_index": 9,
        "rx_b_device_clk_index": 11,
        "tx_b_device_clk_index": 12,
    },
    "ad9084_board": {
        "converter_spi": "axi_spi_2",
        "converter_cs": 0,
        "clock_spi": "axi_spi",
        "hmc7044_cs": 1,
        "adf4382_cs": 0,
        "dev_clk_ref": "adf4382 0",
        "dev_clk_scales": "1 10",
        "firmware_name": "204C_M4_L8_NP16_1p25_4x4.bin",
        "reset_gpio": 62,
        "rx_a_link_id": 4,   # FRAMER_LINK_A0_RX
        "rx_b_link_id": 6,   # FRAMER_LINK_B0_RX
        "tx_a_link_id": 0,   # DEFRAMER_LINK_A0_TX
        "tx_b_link_id": 2,   # DEFRAMER_LINK_B0_TX
        "hsci_label": "axi_hsci_0",
        "hsci_auto_linkup": True,
        # ... lane mappings, HMC7044 channel config, etc.
    },
}

The sdtgen postprocessor applies MicroBlaze-specific fixups (CPU cluster rename, DDR4 memory node, earlycon bootargs) and the node builder uses platform-aware reg_addr()/reg_size() for 32-bit register format.

See test/ad9084/test_ad9084_xsa_hw_vcu118.py for a complete hardware test example that runs the full pipeline and verifies all IIO devices and JESD204C links.

If reference_dts=Path(...) is passed to XsaPipeline.run(), the pipeline also writes parity artifacts:

  • <name>.map.json – role and required-link parity summary

  • <name>.coverage.md – human-readable role/link/property coverage report (property checks are value-sensitive)

When strict_parity=True is used with reference_dts, the pipeline raises ParityError if any required manifest roles, links, or properties are missing in the generated DTS.

For properties, parity checks compare both property name and value from the reference DTS role node. Value comparison is whitespace-insensitive.

Configuration

The JSON config file supplies JESD204 link parameters and HMC7044 channel assignments. Example for an AD9081 RX+TX design:

{
  "jesd": {
    "rx": { "F": 4, "K": 32 },
    "tx": { "F": 4, "K": 32 }
  },
  "clkgen": {
    "label": "axi_clkgen_0"
  },
  "hmc": {
    "rx_channel": 12,
    "tx_channel": 13
  }
}

Board override keys

The profile/default config can carry board-specific keys to avoid hardcoding in the parser implementation.

ad9081_board keys:

  • clock_spi / clock_cs – SPI bus and chip-select for HMC7044

  • adc_spi / adc_cs – SPI bus and chip-select for AD9081

  • reset_gpio / sysref_req_gpio / rx1_enable_gpio / rx2_enable_gpio / tx1_enable_gpio / tx2_enable_gpio

  • hmc7044_channel_blocks – optional replacement list for HMC7044 channel subnodes (raw DTS snippet blocks)

adrv9009_board keys:

  • misc_clk_hz – fixed clock frequency for misc_clk_0

  • spi_bus / clk_cs / trx_cs – SPI and CS assignments

  • trx_reset_gpio / trx_sysref_req_gpio / trx_spi_max_frequency

  • ad9528_vcxo_freq

  • rx_link_id / rx_os_link_id / tx_link_id

  • tx_octets_per_frame / rx_os_octets_per_frame

  • trx_profile_props – optional replacement list for ADRV9009 PHY profile properties (raw DTS property lines)

  • ad9528_channel_blocks – optional replacement list for AD9528 channel subnodes (raw DTS snippet blocks)

adrv9003_board keys:

  • label / spi_cs / spi_max_frequency / reset_gpio

  • rx_link_id / tx_link_id

  • trx_profile_props – required TES-generated ADRV9003 PHY profile properties (raw DTS property lines). The built-in ADRV9003 board profiles intentionally provide no default profile because these properties are hardware and configuration specific.

fmcdaq2_board keys:

  • spi_bus / clock_cs / adc_cs / dac_cs – SPI bus and chip-select assignments (default mapping: AD9523 on CS0, AD9144 on CS1, AD9680 on CS2)

  • clock_vcxo_hz / clock_spi_max_frequency / adc_spi_max_frequency / dac_spi_max_frequency

  • adc_dma_label / dac_dma_label

  • adc_core_label / dac_core_label

  • adc_xcvr_label / dac_xcvr_label

  • adc_jesd_label / dac_jesd_label

  • adc_jesd_link_id / dac_jesd_link_id

  • adc_device_clk_idx / adc_sysref_clk_idx / adc_xcvr_ref_clk_idx / dac_device_clk_idx / dac_xcvr_ref_clk_idx

  • adc_sampling_frequency_hz

  • GPIO overrides: clk_sync_gpio, clk_status0_gpio, clk_status1_gpio, dac_txen_gpio, dac_reset_gpio, dac_irq_gpio, adc_powerdown_gpio, adc_fastdetect_a_gpio, adc_fastdetect_b_gpio

Hardware test note

The Kuiper kernel’s cf_axi_adc_core.c sets the IIO device name from pdev->dev.of_node->name, so the IIO name follows the DT node-name. Production Kuiper DTs spell the buffered ADC node axi-<chip>-rx-hpc; sdtgen-built XSAs spell the same node ad_ip_jesd204_tpl_<adc|dac>. Hardware tests therefore accept either set, e.g.:

  • FMCDAQ2: axi-ad9680-hpc / axi-ad9144-hpc or ad_ip_jesd204_tpl_adc / ad_ip_jesd204_tpl_dac

  • ADRV9009 ZC706: axi-adrv9009-rx-hpc / axi-adrv9009-rx-obs-hpc or both ADC frontends as ad_ip_jesd204_tpl_adc

ADRV9009 ZC706 in particular binds two IIO devices both named ad_ip_jesd204_tpl_adc — RX (@44a00000, via cf_axi_adc) and OBS (@44a08000, via ad_adc.c matching adi,axi-adrv9009-obs-1.0). ctx.find_device(name) returns whichever probed first. Tests that need the RX path (the one Talise radio_on actually streams) disambiguate by of_node reg address; test/hw/xsa/test_adrv9009_zc706_overlay.py::test_dma_loopback shows the pattern.

pyadi-iio looks up the buffered ADC by the production name (axi-adrv9009-rx-hpc). On the merged DTB that name is absent, so adi.adrv9009(uri=...) returns successfully but with _rxadc = None. Tests that drop down to pyadi-iio therefore need to gate on getattr(dev, "_rxadc", None) is not None and skip the high-level path when the merged-DTB names are in play.

Profile validation

Built-in and custom JSON profiles are validated when loaded:

  • Unknown keys under ad9081_board / adrv9009_board / adrv9003_board raise ProfileError (prevents silent typos).

  • Structured snippet fields such as hmc7044_channel_blocks, ad9528_channel_blocks, and trx_profile_props must be JSON lists.

merge_profile_defaults() deep-copies defaults during merge so mutating the effective runtime config does not mutate the source profile data.

Supported IP Cores

The XSA parser recognises the following ADI IP cores:

IP type (MODTYPE)

Role

axi_jesd204_rx, axi_jesd204_tx

JESD204 FSM controllers

axi_clkgen

PL clock generator

axi_ad9081, axi_ad9084, axi_ad9375

RF data converters

Parsed topology fields

XsaTopology carries:

Outputs

XsaPipeline.run() returns a dict with the following keys:

Key

Description

base_dir

Directory containing the sdtgen output

overlay

.dtso overlay (ADI nodes only)

merged

.dts with base SDT + ADI nodes merged

report

Self-contained HTML visualisation report

clock_dot

Graphviz DOT clock-tree diagram (always)

clock_d2

D2 clock-tree diagram (always)

clock_dot_svg

SVG rendered from DOT (when dot is on PATH)

clock_d2_svg

SVG rendered from D2 (when d2 is on PATH)

map

(Optional) manifest parity JSON report

coverage

(Optional) manifest parity Markdown summary

Clock Topology Graphs

XsaPipeline.run() automatically produces clock-tree diagrams derived from the merged DTS. Both output formats are written unconditionally; SVG renderings are produced alongside each when the corresponding tool is on PATH.

File

Tool for SVG

Notes

<name>_clocks.dot

dot (Graphviz)

Graphviz directed graph; render manually with dot -Tsvg -o clocks.svg <name>_clocks.dot

<name>_clocks.d2

d2

D2lang diagram; render manually with d2 <name>_clocks.d2 clocks.svg

Both formats use the same colour scheme:

Node type

Colour / shape

PS clocks (zynqmp_clk, ps7_clkc)

Orange, oval

Clock chips (hmc7044, ad9528, ad9523)

Dark blue, rectangle

GT transceivers (*xcvr*)

Purple, rectangle

JESD204 controllers (*jesd*)

Dark green, rectangle

PL clock generators (*clkgen*)

Teal, rectangle

Converters / PHY (trx*, ad9*, adrv*)

Dark red, rectangle

Edges are labelled with the clock-names value and the provider channel index (e.g. device_clk[9]). Edge styles distinguish signal-domain clocks from AXI bus clocks:

  • Solid coloured – device_clk (blue), lane_clk (green), conv (gold), sampl_clk (purple)

  • Dashed – s_axi_aclk (grey), div40 (gold dashed)

The graphs can also be generated standalone without running the full pipeline:

from pathlib import Path
from adidt.xsa.viz.clock_graph import ClockGraphGenerator

merged_dts = Path("out/adrv9009_zcu102.dts").read_text()
result = ClockGraphGenerator().generate(merged_dts, Path("out/"), "adrv9009_zcu102")
print(result["clock_dot"])    # always present
print(result["clock_d2"])     # always present
# result["clock_dot_svg"] and result["clock_d2_svg"] when tools are available

Exceptions

Exception

Raised when

XsaParseError

The .xsa ZIP contains no .hwh file, or the XML is malformed

ConfigError

A required JESD204 parameter (F or K) is missing from the config

ParityError

Strict parity mode is enabled and one or more required roles are missing

SdtgenNotFoundError

The sdtgen / lopper binary cannot be found on PATH

SdtgenError

sdtgen exits with a non-zero return code