Hardware CI
The Hardware Tests workflow in .github/workflows/hardware-test.yml
selects hardware through the labgrid coordinator. See
Release hardware validation for the completed release qualification and
Runtime JESD overlay validation for the required overlay kernels.
Discovery and test selection
The workflow calls a local copy of hw-matrix.yml (upstream
tfcollins/labgrid-plugins commit
3f6cd9321f2d54edf2110f1d91a3af582ea368d7) with dynamic_mode: true.
The local addition prepares ordinary kernels before acquire-place;
the upstream pre-pytest hook runs after acquisition and cannot do this safely.
Coordinator place
metadata supplies the runner routing; .github/supported-boards.yml filters
supported daughter-board tags. The current allowlist contains ad9081,
adrv9371, adrv9009, adrv9009zu11eg, and daq3. An allowlist entry
is not proof that matching hardware is available or validated.
Runs are triggered manually, on pushes to main, nightly at 08:00 UTC,
and for pull requests carrying the hw-test label. The reusable workflow
owns discovery and scheduling. The inherited direct/coordinator jobs remain
disabled; routing uses dynamic metadata rather than a static node manifest.
Each selected leg receives BOARD, CARRIER, LG_ENV, and
LG_COORDINATOR. Its test command selects:
Full-DTB tests matching
test/hw/*${BOARD}*${CARRIER}*_hw.py.Overlay tests matching
test/hw/xsa/test_*${BOARD}*${CARRIER}*_overlay.py.
PetaLinux tests are excluded from this workflow’s selection. An empty selection
fails. After pytest, check_hardware_results.py requires passing JUnit
results without failures or errors; an all-skipped run cannot qualify hardware.
Runner preparation
Register the self-hosted runner and give it the label selected by the place’s
coordinator runner tag. It needs access to the coordinator and exporter,
the board’s boot artifacts, and the appropriate FPGA tools.
.github/scripts/install-adidt-venv.sh installs the checkout with dev
extras and checksum-verified CIM v1.2.4 into a Python 3.12 environment at ~/.cache/adidt-ci/datax-py312-venv. It also installs the AD9371
clock-model requirements and exposes the supported Vivado 2025.1 sdtgen
launcher in that environment. Missing tools or imports fail setup before
hardware acquisition. Hardware requirements select pylibiio<1 to match
the runners’ libiio 0.x ABI. Setup verifies that the Python binding loads before
acquiring a place. The labgrid plugin pin includes serial-aware JTAG resources
and exporter-owned recovery payload paths.
.github/scripts/prepare-hardware-env.sh then:
Loads optional board-specific artifact settings from
~/.config/pyadi-dt/hardware/$BOARD-$CARRIER.env. Override the directory withADIDT_HARDWARE_CONFIG_DIR.Sanitizes
PATHand verifies GNUas, labgrid, pytest, andsdtgen.Prepares a private labgrid environment from the live place tags. TFTP deployment disables SD autoboot; ZynqMP deployment registers the pinned production JTAG strategy and accepts either Ethernet port.
SD-mux environments use the pinned client’s current storage-driver template.
The managed TFTP server advertises the runner’s interface used to reach the
coordinator, which connects it to the lab management network. Set
ADIDT_TFTP_SERVER_ADDRESS in the per-board runner configuration to select
a DUT-facing address explicitly.
Kernel and DTB overrides are published through the strategy’s location-aware artifact cache. Each generated DTB carries a unique validation property that the boot test checks in the running device tree.
Keep operational labgrid environments private. Optional Prism upload is
controlled by PRISM_UPLOAD_ENABLED and uses the explicitly passed
PRISM_EMAIL and PRISM_PASSWORD secrets. These values are not test
artifacts.
Prepared CIM kernels
Kernel compilation, Zynq uImage packaging, source/toolchain pinning, and
build caches are provided by the public
DataX manifests adi-linux
target, driven by CIM. Hardware CI
uses public dependencies and requires no private dependency token. Existing
kernel overrides and independently qualified modular overlay artifacts remain
supported.
Prepare only the platform needed by the selected tests, before acquiring a
place. An installed CIM executable and an explicit, reviewed manifest source
and full Git commit are required for builds (there is no implicit main or
package installation). Install the host build dependencies listed in the CIM
target’s os-dependencies.yml separately. For example, for ZC706:
# Set these to the reviewed manifest repository and full commit containing
# the self-contained adi-linux target (both releases and platforms).
: "${CIM_MANIFEST_SOURCE:?set the reviewed CIM manifest repository}"
: "${CIM_MANIFEST_COMMIT:?set its full reviewed Git commit SHA}"
python .github/scripts/prepare_cim_kernel.py \
--platform zynq --cim /path/to/installed/cim \
--source "$CIM_MANIFEST_SOURCE" --version "$CIM_MANIFEST_COMMIT" \
--workspace "$HOME/cim-kernels/2023_R2/$CIM_MANIFEST_COMMIT-zynq" \
> /tmp/adidt-kernel.env
# Only source the output if preparation succeeded.
source /tmp/adidt-kernel.env
The default release remains 2023_R2. Opt in to 2026-R1 with
ADIDT_CIM_RELEASE=2026-R1 in the runner environment or per-board file,
or pass --release 2026-R1 to the Python helper (CLI takes precedence).
Only these exact two spellings are accepted. All combinations initialize the
single self-contained adi-linux target. The helper explicitly passes
KERNEL_RELEASE, KERNEL_PLATFORM, KERNEL_OUTPUT, and KERNEL_JOBS
to make sdk-build; it does not depend on CIM’s default release or platform.
For direct CIM use, KERNEL_RELEASE defaults to 2023_R2 and
KERNEL_PLATFORM defaults to zynq. For example, in an initialized
CIM workspace:
make sdk-build KERNEL_RELEASE=2026_R1 KERNEL_PLATFORM=zynqmp KERNEL_JOBS=4
2026-R1 here means the analogdevicesinc/linux tag
xlnx_2026.1.0 at commit
b47bbbe8ca7bc582c96251fa30d86e55de363f68; it is not a mutable branch.
The legacy source remains 2023_R2 at
86d61468a7856e952c7ca237f798d86d6abd2e27.
For a manual 2026-R1 build, use the command above with --release 2026-R1
and a separate workspace such as
$HOME/cim-kernels/2026-R1/$CIM_MANIFEST_COMMIT-zynq.
The public label 2026-R1 maps to CIM’s internal helper/provenance key
2026_R1. The preparation helper explicitly sets KERNEL_OUTPUT to preserve
its output artifacts/2026_R1/<platform>/artifacts.json for 2026-R1 and
artifacts/<platform>/artifacts.json for 2023_R2. Existing manifests at
other paths can still be selected explicitly.
Source both emitted exports: the image manifest and ADIDT_CIM_RELEASE.
CI workspaces include the release in their names, and the release is propagated
through GITHUB_ENV to pytest. CIM owns its release-aware build cache;
pyadi-dt never searches a shared legacy cache or silently falls back to another
release. Explicit manifest reuse must match the selected source ref and commit.
Missing or mismatched provenance fails before acquisition; it does not trigger
an automatic rebuild. Legacy CIM manifests without a release field remain valid
when their source pins match 2023_R2.
The helper uses cim init, cim makefile, and make sdk-build. It refuses
to overwrite a workspace; to reuse its results, export the existing manifest
path instead of rebuilding. It validates the handoff before emitting a
shell-quoted export. It does not install CIM, reserve boards, or modify runner
configuration. Run the command with set -e or explicitly check its exit
status before sourcing its output. Prepared-image and disabled modes do not
invoke CIM and do not require source/version/workspace arguments.
For persistent runners, put the resulting export in the existing per-board
$BOARD-$CARRIER.env file. The matrix runs
prepare-hardware-kernels.sh before acquisition, loads that same file, and
validates explicit ordinary images/manifests. Without them it builds using
CIM_MANIFEST_SOURCE, CIM_MANIFEST_COMMIT (a full immutable SHA), and
ADIDT_CIM_EXECUTABLE (an installed absolute executable path recommended).
The default manifest source is https://github.com/tfcollins/datax-manifests.git at
6efed11c826f35f5e3a5da3c10ebd54c309f25fa. Override settings through the
runner environment or per-board file. CI installs checksum-verified CIM v1.2.4
in the Python 3.12 hardware venv. For manual runs, supply an installed CIM
executable. New workspaces are release- and run-scoped under
ADIDT_CIM_WORKSPACE_ROOT, a writable /mnt/onetb/scratch mount when
available, or RUNNER_TEMP. For cache reuse provision a persistent manifest
explicitly.
Fabric-only legs do not build ARM kernels; disabled mode and image overrides
bypass CIM entirely. Do not build on disk-constrained runners: stage verified
CIM artifacts built on another host and update their absolute image paths and
checksums, or explicitly select a boot-ready external image.
Profiles declaring runtime_modules require their separately qualified
modular kernels and matching modules. The pre-acquisition step checks the
selected overlay profile before requiring an explicit overlay image (or a
qualified generic image override). Existing ADIDT_OVERLAY_KERNEL_IMAGE_ZYNQ
and module settings are preserved. Profiles without runtime module unloading use the selected ordinary kernel
unless an overlay image is explicitly supplied. Their hardware tests check
configfs support on the board.
AD9081/ZCU102, AD9371/ZC706 and ADRV9009/ZC706 declare their JESD clients in
runtime_modules. Their overlay tests boot a modular kernel with the
matching modules from ADIDT_OVERLAY_MODULES_ARCHIVE. The helper
.github/scripts/build-runtime-overlay-kernel.sh supports zynq,
zynqmp and microblaze. For ZynqMP it emits Image and
modules.tar.gz from the selected disposable ADI Linux source tree.
The helper applies the required JESD teardown patch before compilation and
verifies its direction when checking a previously patched source tree.
Select those files with ADIDT_OVERLAY_KERNEL_IMAGE_ZYNQMP and
ADIDT_OVERLAY_MODULES_ARCHIVE in the per-board runner configuration.
The handoff is a runner-local JSON object with these required fields:
{
"schema_version": 1,
"platform": "zynq",
"kernel_image": "/absolute/path/to/uImage",
"sha256": "<64 hexadecimal characters>",
"provenance": {
"source": {
"ref": "2023_R2",
"commit": "86d61468a7856e952c7ca237f798d86d6abd2e27"
}
}
}
CIM additionally records source, toolchain, configuration and packaging provenance. pyadi-dt allows extra provenance fields and checks the schema, expected platform, selected release source ref/commit, non-empty regular image file, absolute image path and SHA-256. Keep the manifest and its image together on the runner; copying just the JSON does not relocate the absolute image path. Do not modify images while tests are running. No consumer-side packaging or implicit cache fallback occurs.
Selection order for each platform is:
ADIDT_KERNEL_IMAGE_ZYNQ/ADIDT_KERNEL_IMAGE_ZYNQMP: explicit prebuilt image, still honored when kernel replacement is otherwise disabled.ADI_XSA_BUILD_KERNEL=0(alsofalseorno): retain the existing kernel and return no replacement, ignoring CIM manifests.ADIDT_KERNEL_ARTIFACTS_ZYNQ/ADIDT_KERNEL_ARTIFACTS_ZYNQMP: validate and use the manifest image; missing/invalid input is a hard error.
Hardware collection preflights the selected module profiles before labgrid
fixtures run, while --collect-only remains usable without artifacts.
Overlay-only image overrides take priority for overlay modules, not ordinary
full-DTB tests. When manually reserving a place outside pytest, perform kernel
preparation/validation before the explicit labgrid-client acquire command.
Exporter service
Exporters publish the serial, power, JTAG, and other resources used by the
coordinator. The repository’s installation convention uses one
labgrid-exporter.service per host and /etc/labgrid/exporter.yaml.
See Labgrid exporter systemd service for installation and service operation.
Generated-DTB deployment
A successful stock-image boot does not qualify a generated tree. Tests stamp the generated DTB and verify its unique marker in Linux. TFTP tests require a strategy that consumes the staged files; recovery strategies that boot only the existing SD tree are unsuitable for those tests.
The ZU11EG test uses production JTAG bootstrap followed by U-Boot’s serial S-record loader. It verifies the complete RAM payload CRC, the marker in both U-Boot and Linux, four online CPUs, both PHYs, JESD DATA, and RX DMA. See Release hardware validation for prerequisites and a local test command.
Full kernel-log collection allows 120 seconds for a busy serial transport to deliver the complete ring buffer. This timeout does not truncate diagnostics or relax boot, JESD, capture, or kernel-fault checks.
For runtime overlays, use the matching modular kernels, module bundles, and
base trees described in Runtime JESD overlay validation. Installing
pyadi-dt does not update a board’s kernel. Overlay tests verify live-tree
application and removal as well as JESD and DMA on each reload.
Local runs and evidence
Use the same checkout and prepared environment as CI. From a Bash shell at the
repository root, set LG_ENV to an existing private configuration for the
selected place, then run:
export VENV_DIR="$HOME/.cache/adidt-ci/datax-py312-venv"
export LG_COORDINATOR=10.0.0.41:20408
export BOARD=adrv9009 CARRIER=zc706
source .github/scripts/prepare-hardware-env.sh
"$VENV_DIR/bin/labgrid-client" -p nemo acquire
trap '"$VENV_DIR/bin/labgrid-client" -p nemo release' EXIT
"$VENV_DIR/bin/python" -m pytest -p no:genalyzer -v -s \
test/hw/xsa/test_adrv9009_zc706_overlay.py \
--junitxml=/tmp/adrv9009-overlay.xml
"$VENV_DIR/bin/python" .github/scripts/check_hardware_results.py \
/tmp/adrv9009-overlay.xml
The shared board fixture powers down the board on teardown, including failed boots. Retain failed reports as well as passing evidence. The workflow collects generated DTS/DTB/DTBO files, kernel and serial logs, and JUnit reports. Record the tested commit and artifact checksums alongside those results.
Local DT-emission parity
Run the System-API parity checks before deploying changed device wiring:
python -m pytest test/devices/test_system_adrv9371_zc706_dts_parity.py \
test/devices/test_system_ad9081_dts_parity.py
Reference fixtures live under test/devices/fixtures. Refresh a fixture only
from a reviewed reference or verified generated tree; a parity comparison
alone does not establish live hardware coverage.
Troubleshooting
No matching leg: inspect the reusable workflow’s discovery output, coordinator daughter-board/carrier tags, runner routing, and the allowlist.
Empty or skipped-only test results: check filename selection, pytest feature markers, and missing prerequisites. Do not treat this as a pass.
Wrong tree after boot: inspect the prepared strategy and staged-file consumption, and retain the marker mismatch. Do not substitute a stock boot.
ZU11EG JTAG reaches the wrong host: verify exporter resolution.
ADIDT_JTAG_HOSToverrides JTAG resource hosts for the test process and restores them during teardown.Overlay rejected or modules busy: check the kernel/module match and topology teardown sequence. The harness does not force module removal or bypass the JESD notifier.
FMCDAQ3 serial command truncation: the BootFabric fixture paces writes at a minimum of 2 ms per byte to accommodate UART Lite’s receive FIFO.