Release Operator Runbook

This runbook covers validation, publication, verification, and recovery for a pyadi-dt release. The Publish Release workflow builds on manual dispatch but publishes only when an annotated v* tag is pushed.

The current hardening candidate records current software evidence and outstanding release gates. The historical validation summary retains earlier hardware scope and limits. The 2026-09-05 readiness audit contains the investigation history. Refresh affected checks for a new release commit.

One-time setup

PyPI trusted publisher

Before the first release, sign in to PyPI and add a pending trusted publisher with these exact values:

  • PyPI project name: pyadi-dt

  • Owner: analogdevicesinc

  • Repository: pyadi-dt

  • Workflow: release.yml

  • Environment: pypi

After the first successful upload, verify that the pending publisher became a publisher for the newly created project.

GitHub environment

Create a GitHub environment named pypi. Require a release reviewer and limit deployment refs to tags matching v*. The PyPI job requests OIDC only inside this environment; no PyPI API token is required.

Prepare and validate

  1. Confirm the target version agrees in pyproject.toml and adidt/__init__.py and has a non-empty ## [X.Y.Z] section in CHANGELOG.md.

  2. Run the local contract and package checks from a clean checkout:

    git fetch origin --tags
    git switch main
    git pull --ff-only origin main
    test -z "$(git status --porcelain)"
    python .github/scripts/release_preflight.py --tag vX.Y.Z
    pytest
    rm -rf build dist
    python -m build
    twine check dist/*
    

    The hosted build stages only .whl and .tar.gz files into pypi-dist/ using .github/scripts/stage-pypi-artifacts.sh, and validates that directory on both dry runs and tag builds. SHA256SUMS stays with the GitHub release assets; it must not enter the PyPI action’s upload directory.

  3. Run the hosted dry run from the candidate branch (or main after merge). The candidate tag does not need to exist yet:

    gh workflow run release.yml --ref YOUR_CANDIDATE_BRANCH -f tag=vX.Y.Z
    gh run watch --exit-status
    

    Confirm the validation, Python 3.10–3.14, build, wheel-install, and CLI smoke-test jobs pass. The GitHub Release and PyPI jobs must be skipped.

  4. Confirm all required main workflows—including hardware, Kuiper/Ubuntu Debian packaging, and native system packaging—are green for the exact commit to be tagged. The native workflow builds on Debian 12, Fedora 42, and macOS 15 rather than cross-packaging those artifacts on Ubuntu.

    Hardware jobs must select tests and produce at least one passing testcase; skip-only jobs are failures. This minimum gate does not certify every test path: review individual skips and record unavailable boards separately. Generated-DTB evidence requires a boot strategy that actually deploys the staged DTB, rather than booting the existing SD tree.

Hardware and security gates

Hardware CI prepares kernels from the pinned public DataX adi-linux target before acquiring boards. Rerun the matrix for the exact release candidate and inspect per-board JUnit counts, boot logs, and individual skips. Record unavailable boards separately. The migration removes the private dependency credential requirement.

CodeQL is defined in .github/workflows/codeql.yml for Python and GitHub Actions. Advanced setup requires GitHub’s managed default setup to be disabled; keep this non-secret repository setting aligned with the committed workflow. No C/C++ autobuild is required for vendored device-tree binding headers.

Tag and publish

Record and inspect the exact release commit before tagging:

git switch main
git pull --ff-only origin main
test -z "$(git status --porcelain)"
RELEASE_SHA=$(git rev-parse HEAD)
git show --stat "$RELEASE_SHA"
git tag -a vX.Y.Z "$RELEASE_SHA" -m "Release vX.Y.Z"
test "$(git cat-file -t refs/tags/vX.Y.Z)" = tag
git push origin refs/tags/vX.Y.Z

The tag push is the only event that permits the workflow’s GitHub Release and PyPI jobs to run. Approve the pypi environment deployment only after checking that the run’s tag, commit SHA, version, changelog, tests, and built artifacts are correct.

Verify the published release

  1. Confirm Publish Release completed successfully for the tagged SHA.

  2. Confirm both packaging workflows completed for the same tag. The release must contain Kuiper/Ubuntu .deb files plus the Debian 12 .deb, Fedora 42 .rpm, and macOS 15 .pkg artifacts. Each job installs and smoke-tests its package before upload.

  3. Verify the GitHub Release contains the wheel, source distribution, release notes, all native system packages, and the SHA256SUMS manifest file.

  4. Verify checksum manifest integrity:

    gh release download vX.Y.Z -D /tmp/adidt-verify-assets
    cd /tmp/adidt-verify-assets
    sha256sum -c SHA256SUMS
    python .github/scripts/release_manifest.py verify --manifest SHA256SUMS --dir .
    
  5. Verify PyPI and smoke-test the immutable published package:

    python -m venv /tmp/adidt-release-verify
    /tmp/adidt-release-verify/bin/python -m pip install --no-cache-dir pyadi-dt==X.Y.Z
    /tmp/adidt-release-verify/bin/python -c \
      'import adidt, importlib.metadata as m; assert adidt.__version__ == m.version("pyadi-dt") == "X.Y.Z"'
    /tmp/adidt-release-verify/bin/adidtc --help
    
  6. Verify the public documentation still serves successfully.

Recover from partial failure

Release files on PyPI are immutable. Never move or reuse a version after any artifact for it has been accepted by PyPI.

  • Validation/build failed before publication: fix main, delete the failed remote tag only if neither PyPI nor a release artifact was published, rerun the dry run, and create a new annotated tag on the corrected commit.

  • PyPI upload partially succeeded: rerun the failed jobs. Publishing uses skip-existing, so accepted files are retained and missing files can resume. Do not rebuild different bytes for the same version.

  • GitHub Release failed after PyPI succeeded: rerun the failed job. The workflow creates a missing release or uploads artifacts to an existing one with --clobber and updates SHA256SUMS.

  • System-package attachment failed: rerun the failed Debian or native-system package workflow for the original tag; do not retag.

  • Checksum manifest out of sync: re-sync the release manifest using the helper script:

    python .github/scripts/release_manifest.py upsert-release --tag vX.Y.Z
    
  • A bad package was fully published: keep the tag and release as an audit record, document the problem, bump to a new version, and publish a corrective release. PyPI versions cannot be replaced safely.