Release hardening candidate — 2026-11-10
This candidate is the fix/release-hardening branch based on 92e6fc8. It is
not tagged or released. GitHub checks and artifacts identify the exact PR head
commit; repeat the release dry run and hardware checks for the final commit
before tagging. No previous hardware result qualifies this branch.
Software checks
The candidate fixes all ten findings from the main-branch review:
PyPI-safe metadata: Git-only lab tools moved to source requirements.
A clean, isolated wheel
[xsa]installation exercises imports, profile discovery and CLI help;requestsis declared in the extra.Nested AXI children retain their structure; compiled DTB path checks verify generated IP is under the bus. Both ADRV9040 layouts resolve SDTGen-style
gic_a53references in the merged DTS and overlay.Both PetaLinux pipeline entry points execute; ZynqMP output uses
gic_a53.Typed and raw implicit JESD framing agree after topology detection, including partial ORX settings and explicit
F=1overrides.MCP reads actual DTS and DTB fixtures by short name, full path and compatible.
Failed release-asset downloads fail checksum refresh.
Tag workflows use a shared queue that retains all pending publication runs.
Type checking and dependency audit preserve nonzero checker exits; the existing clock/MxFE type errors are fixed with generic model types.
CodeQL is an explicit Python/Actions workflow, avoiding C/C++ fixture headers.
Local validation after the DataX hardware-CI migration and serial-log fix:
1117 passed, 15 skipped.
Regression coverage includes kernel handoff, preparation, release selection,
pre-acquisition checks, and job-owned reservation cleanup.
Ruff and ty 0.0.100 passed. The renamed import rule is updated so hosted
checking exits successfully.
Bandit passed against the existing baseline, and the runtime dependency audit
reported no known vulnerabilities. Source/wheel builds, twine check, clean
wheel [xsa] installation, and strict Sphinx dirhtml builds passed.
Reproduce the software checks from the candidate checkout:
pytest -q
ruff check adidt test
ty check adidt/model/ adidt/xsa/build/builders/ adidt/devices/ adidt/system.py adidt/tools/
bandit -r adidt -c .bandit -b .bandit-baseline.json
pip-audit -r requirements.txt
python -m build
python .github/scripts/verify-release-wheel.py dist/*.whl --smoke-xsa
twine check dist/*
sphinx-build -W --keep-going -b dirhtml doc/source doc/build/dirhtml
The final fresh-context review found a generic typed framing regression;
its reproducer failed before the topology-aware default resolution fix and
passed afterward, together with the full suite. The hosted release build also runs the clean-wheel
smoke check; building a wheel or passing twine check alone does not establish
PyPI upload acceptance.
Outstanding release gates
Hardware CI now uses public tfcollins/datax-manifests at
6efed11c826f35f5e3a5da3c10ebd54c309f25fa, driven by checksum-verified CIM
v1.2.4. The adi-linux target prepares artifacts before board acquisition,
with consumer-side source pin and image checksum validation. The earlier
authentication failure
is superseded by this migration. Exact-head hardware results must be reviewed
before release qualification.
At 91ae339, five board legs passed. ZU11EG booted its generated DTB but
timed out while streaming the full kernel log under the shell driver’s
30-second command limit, including on the single failed-leg retry. Bulk
kernel-log reads now allow a bounded 120 seconds and retain the complete
diagnostics. The regression test failed under the original limit and passed
with the corrected budget. Final per-board results and their exact head are
recorded in PR #126.
The ZU11EG SD root filesystem also reported an inode error; earlier passing boots already warned that it was mounted with errors. This requires separate lab maintenance before broader hardware qualification. No filesystem repair or image replacement is part of this change.
The earlier C/C++ CodeQL run failed with “No source files found.” The committed advanced workflow replaces language autodetection with Python and Actions. Managed default setup must be disabled for advanced SARIF uploads to work.
ADRV9040 validation remains software-only with representative HWH fixtures and a controlled SDTGen base. Real SDTGen/Vivado execution, physical boot, JESD training and RF operation are unqualified. External firmware, ACE profiles and gain tables remain user-supplied. No new Kuiper release compatibility is claimed.
No tag, GitHub Release or PyPI publication is produced by this hardening work. Hardware evidence is limited to the exact-head board tests recorded in the PR. Trusted publishing and the release-reviewer environment still require operator verification per the runbook.