Declarative Devices

The adidt.devices package is the single source of truth for how ADI hardware maps to device-tree nodes. Every modeled device is a small pydantic class whose fields are the DT properties it emits — no Jinja2 templates, no intermediate context dicts. A device’s render_dt method returns the DTS text directly.

Design in three pieces

1. Typed fields with DT-property aliases. Each field on a Device subclass carries the exact DT property name via Field(alias="adi,..."). The Python attribute is the human-facing handle; the alias is the on-disk name.

class HMC7044(ClockDevice):
    compatible: ClassVar[str] = "adi,hmc7044"
    dt_header: ClassVar[dict] = {"#clock-cells": 1, "#jesd204-cells": 2}
    dt_flags: ClassVar[tuple] = ("jesd204-device",)

    vcxo_hz: int = Field(..., alias="adi,vcxo-frequency")
    pll2_output_hz: int = Field(..., alias="adi,pll2-output-frequency")
    pll1_ref_autorevert: bool = Field(False, alias="adi,pll1-ref-autorevert-enable")

The adidt.devices._dt_render renderer walks these fields, formats each value by its Python type, and emits:

adi,vcxo-frequency = <122880000>;
adi,pll2-output-frequency = <2949120000>;
adi,pll1-ref-autorevert-enable;

2. Field markers for non-scalar cases. Fields that don’t map 1:1 to a DT value use adidt.devices._fields markers, applied via typing.Annotated:

  • DtSubnodes — a dict[key, child] renders as child DT nodes (e.g. HMC7044 channels).

  • DtSkip — excludes a field from rendering (Python-only state, ports, etc.).

  • DtBits64 — emit /bits/ 64 <N> for sampling/converter frequencies that don’t fit in a 32-bit cell.

3. An ``extra_dt_lines`` hook for coupled properties. Properties that need System-supplied context (phandles, gpio_label) or that render as tied pairs (clocks + clock-names) are emitted by overriding extra_dt_lines(context).

def extra_dt_lines(self, context: dict | None = None) -> list[str]:
    ctx = context or {}
    if self.clkin0_ref is not None:
        return [
            f"clocks = <&{self.clkin0_ref}>;",
            'clock-names = "clkin0";',
        ]
    return []

Component device models

Clock distributors and PLLs:

  • adidt.devices.clocks.HMC7044

  • adidt.devices.clocks.AD9523_1

  • adidt.devices.clocks.AD9528

  • adidt.devices.clocks.AD9528_1

  • adidt.devices.clocks.ADF4382

Converters / MxFE transceivers:

  • adidt.devices.converters.AD9081 (with AD9081Adc/AD9081Dac)

  • adidt.devices.converters.AD9084 (with AD9084Adc/AD9084Dac)

  • adidt.devices.converters.AD9172

  • adidt.devices.converters.AD9680

  • adidt.devices.converters.AD9144

  • adidt.devices.converters.AD9152

RF transceivers:

  • adidt.devices.transceivers.ADRV9003 — Navassa ADRV9003 (two RX, one TX)

  • adidt.devices.transceivers.ADRV9009 — reused for ADRV9025/9026/9029 (Talise silicon) and for AD9371/ADRV9371 (Mykonos silicon). The kernel binding differs per chip: set compatible_strings=["adi,ad9371"] plus node_name_base="ad9371-phy" for AD9371, otherwise the ADRV9009 default applies.

FPGA-side JESD204 IP overlays:

  • adidt.devices.fpga_ip.Adxcvr — AXI ADXCVR overlay

  • adidt.devices.fpga_ip.Jesd204Overlay — AXI JESD204 RX/TX overlay

  • adidt.devices.fpga_ip.TplCore — AXI TPL core overlay

Composition layer

The composition API lives in adidt.eval, adidt.fpga, and adidt.system:

import adidt

fmc = adidt.eval.ad9081_fmc()
fmc.converter.set_jesd204_mode(18, "jesd204c")
fmc.converter.adc.sample_rate = int(250e6)
fmc.converter.adc.cddc_decimation = 4
fmc.converter.adc.fddc_decimation = 4

fpga = adidt.fpga.zcu102()

system = adidt.System(name="ad9081_zcu102", components=[fmc, fpga])
system.connect_spi(bus_index=0, primary=fpga.spi[0],
                   secondary=fmc.clock.spi, cs=0)
system.connect_spi(bus_index=1, primary=fpga.spi[1],
                   secondary=fmc.converter.spi, cs=0)
system.add_link(source=fmc.converter.adc, sink=fpga.gt[0],
                sink_reference_clock=fmc.dev_refclk,
                sink_core_clock=fmc.core_clk_rx,
                sink_sysref=fmc.dev_sysref)

print(system.generate_dts())
  • adidt.system.System — collects devices + connection records, produces a BoardModel, delegates to BoardModelRenderer for DTS emission.

  • adidt.eval.EvalBoard subclasses (ad9081_fmc, ad9084_fmc, adrv937x_fmc) pre-wire a clock chip and a converter with the schematic-level channel assignments a specific FMC expects, and expose named clock-output aliases (fmc.dev_refclk, fmc.fpga_sysref, …).

  • adidt.fpga.FpgaBoard subclasses (zcu102, vpk180, zc706) hold platform constants: address-cells, PS clock label/index, GPIO controller, SPI masters, GT lane count, default QPLL selection.

Writing a new device

See Authoring a new device class for the full walkthrough — class hierarchy, end-to-end call flow from adidt.system.System.generate_dts() through adidt.devices._dt_render.render_node(), and cookbook recipes for adding a new clock, converter / transceiver, or eval-board / FPGA-board class. adidt.devices.clocks.hmc7044 is the canonical full reference implementation.

End-to-end hardware verification

Hardware tests live in test/hw/. Each one exercises every stage — XSA parsing → sdtgen → DTS generation → DTB compile → labgrid boot → IIO + JESD204 link verification on real hardware — and covers all three supported boot strategies (SD-card, TFTP, and MicroBlaze/JTAG):

Test module

Board + carrier

Boot strategy

Path

test_ad9081_zcu102_system_hw.py

AD9081 + ZCU102

BootFPGASoC

Declarative adidt.System

test_ad9081_zcu102_xsa_hw.py

AD9081 + ZCU102

BootFPGASoC

AD9081Builder

test_adrv9009_zcu102_hw.py

ADRV9009 + ZCU102

BootFPGASoC

ADRV9009Builder

test_adrv9371_zc706_hw.py

ADRV9371 + ZC706

BootFPGASoCTFTP

ADRV937xBuilder

test_fmcdaq3_vcu118_hw.py

FMCDAQ3 + VCU118

BootFabric (JTAG)

Prebuilt simpleImage (smoke test)

Tests support two connection modes, selected by .env at the project root (loaded via pytest-dotenv):

  • Coordinator mode — set LG_COORDINATOR=<host>:<port> plus LG_ENV=<test/hw/env/*.yaml>. The env YAML binds a RemotePlace to the coordinator-published resources.

  • Direct mode — set LG_ENV=<local_yaml> only.

Each board family has a dedicated single-target env file under test/hw/env/: mini2.yaml (ZCU102 + AD9081), bq.yaml (ZC706 + ADRV9371), and nuc.yaml (VCU118 + FMCDAQ3). The combined test/hw/env/all.yaml exposes all three as named targets.

Example — run the ADRV9371+ZC706 test via a coordinator:

LG_COORDINATOR=10.0.0.41:20408 \
LG_ENV=test/hw/env/bq.yaml \
pytest test/hw/test_adrv9371_zc706_hw.py

Copy .env.example to .env for the supported variables. The skip guard in each hw test module requires one of LG_COORDINATOR or LG_ENV to be set.

Prepared kernel images

The session-scoped built_kernel_image_* fixtures consume checksum-verified artifacts.json files produced by the pinned DataX adi-linux target. Set ADIDT_KERNEL_ARTIFACTS_ZYNQ or ADIDT_KERNEL_ARTIFACTS_ZYNQMP before pytest. CI prepares kernels before acquiring a board.

Explicit ADIDT_KERNEL_IMAGE_ZYNQ and ADIDT_KERNEL_IMAGE_ZYNQMP image paths take precedence. Set ADI_XSA_BUILD_KERNEL=0 to use the board’s existing kernel. Runtime overlays require a separately qualified modular image and matching modules. See Hardware CI for preparation and release selection.