XSA → Device Tree: AD9081 on ZCU102
This example walks through the full XSA-to-overlay pipeline for the AD9081-FMCA-EBZ evaluation board on the ZCU102 (Zynq UltraScale+).
The script lives at examples/xsa/ad9081_zcu102_xsa_parse.py and uses
examples/xsa/system_top.xsa — the Vivado 2023.2 reference design bitfile
for this board.
Design Overview
Item |
Value |
|---|---|
FPGA |
xczu9eg-ffvb1156-2 (ZCU102) |
Converter |
AD9081 (MxFE), SPI-controlled |
JESD204 RX |
|
JESD204 TX |
|
JESD mode |
204B, M=8 L=4 S=1 Np=16 → F=4, K=32 |
Clock gen |
HMC7044 external – RX ch 12, TX ch 13 |
Prerequisites
pip install "pyadi-dt[xsa]"
pip install pyadi-jif[cplex] # or [gekko] – solver only needed for clock opt
Running the Example
python examples/xsa/ad9081_zcu102_xsa_parse.py
Expected output:
============================================================
AD9081 + ZCU102: XSA → Device Tree overlay
============================================================
Step 1 – Parsing XSA …
FPGA part : xczu9eg-ffvb1156-2
JESD RX : axi_mxfe_rx_jesd_rx_axi base=0x84a90000 lanes=4
JESD TX : axi_mxfe_tx_jesd_tx_axi base=0x84b90000 lanes=4
Clock gen : hmc7044_car clocks=[...]
Step 2 – Resolving JESD204 parameters via adijif …
JESD mode (RX): mode=10.0 F=4 K=32 L=4 M=8
JESD mode (TX): mode=9 F=4 K=32 L=4 M=8
Step 3 – Generating DTS overlay …
Overlay written to: examples/xsa/output/ad9081_zcu102.dtso
Generated Overlay
examples/xsa/output/ad9081_zcu102.dtso:
/dts-v1/;
/plugin/;
&amba {
axi_mxfe_rx_jesd_rx_axi: axi-jesd204-rx@84a90000 {
compatible = "adi,axi-jesd204-rx-1.0";
reg = <0x0 0x84a90000 0x0 0x1000>;
interrupts = <0 54 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&hmc7044_car 0>, <&hmc7044 12>, <&hmc7044_car 1>;
clock-names = "s_axi_aclk", "device_clk", "lane_clk";
adi,octets-per-frame = <4>;
adi,frames-per-multiframe = <32>;
#sound-dai-cells = <0>;
};
axi_mxfe_tx_jesd_tx_axi: axi-jesd204-tx@84b90000 {
compatible = "adi,axi-jesd204-tx-1.0";
reg = <0x0 0x84b90000 0x0 0x1000>;
interrupts = <0 55 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&hmc7044_car 0>, <&hmc7044 13>, <&hmc7044_car 1>;
clock-names = "s_axi_aclk", "device_clk", "lane_clk";
adi,octets-per-frame = <4>;
adi,frames-per-multiframe = <32>;
#sound-dai-cells = <0>;
};
};
Pipeline Walkthrough
Step 1 – Parse and patch the XSA
XsaParser.parse() extracts axi_jesd204_rx and axi_jesd204_tx modules
from the hardware handoff XML embedded in the XSA ZIP archive.
The Vivado 2023.2 HWH uses a slightly older schema than the parser’s primary fixture. The script patches the topology with the correct values:
Field |
Parser reads |
Actual HWH element |
Patched value |
|---|---|---|---|
|
|
|
|
|
|
|
4 |
|
|
|
|
|
port named |
port named |
54 / 55 |
A synthetic ClkgenInstance named hmc7044_car is added so NodeBuilder
can resolve the device-clock nets to a DTS label. The HMC7044 drives both
clocks externally — there is no axi_clkgen in this design.
Step 2 – Resolve JESD204 parameters with adijif
import adijif as jif
sys = jif.system("ad9081", "hmc7044", "xilinx", 122.88e6, solver="CPLEX")
sys.fpga.setup_by_dev_kit_name("zcu102")
sys.converter.adc.sample_clock = 4e9 / (4 * 4) # 250 MSPS
sys.converter.dac.sample_clock = 12e9 / (8 * 6) # 250 MSPS
# … configure datapath …
modes_rx = jif.utils.get_jesd_mode_from_params(
sys.converter.adc, M=8, L=4, S=1, Np=16, jesd_class="jesd204b"
)
# → mode 10.0: F=4, K=32
get_jesd_mode_from_params performs a pure table lookup against the AD9081
operating modes — it does not invoke the constraint solver, so it works
without cpoptimizer or gekko installed.
Step 3 – Render and write the overlay
from adidt.xsa.build.node_builder import NodeBuilder
from adidt.xsa.merge.merger import DtsMerger
cfg = {
"jesd": {"rx": {"F": 4, "K": 32}, "tx": {"F": 4, "K": 32}},
"clock": {"hmc7044_rx_channel": 12, "hmc7044_tx_channel": 13},
}
nodes = NodeBuilder().build(topology, cfg)
DtsMerger().merge(base_dts, nodes, output_dir, "ad9081_zcu102")
NodeBuilder renders the Jinja2 templates (jesd204_fsm.tmpl) into DTS
node strings. DtsMerger wraps them in a /plugin/; overlay targeting the
&amba bus label.
AD9081 link-mode selection behavior
For AD9081 MXFE pipelines, JESD link modes are no longer hardcoded. The builder resolves mode values in this order:
cfg["ad9081"]["rx_link_mode"]/cfg["ad9081"]["tx_link_mode"]cfg["jesd"]["rx"]["mode"]/cfg["jesd"]["tx"]["mode"]Inference from the link framing
(M, L, Np, S), using the mode each framing has in the ADI kernel reference device trees:M=8, L=4, Np=16-> RX10, TX9M=4, L=8, Np=16-> RX18, TX17
Framing left out of the configuration is read from the XSA’s transport-layer
cores. If no explicit mode is provided and the framing does not identify
exactly one mode, generation fails with ConfigError so invalid link mode
assumptions are not emitted into DTS.
Full Pipeline (with sdtgen)
When lopper is installed the adidtc xsa2dt command runs all five stages,
including SDT base-DTS generation and HTML visualisation:
adidtc xsa2dt examples/xsa/system_top.xsa config.json \
--output-dir out/ad9081_zcu102
Where config.json contains:
{
"jesd": {
"rx": { "F": 4, "K": 32 },
"tx": { "F": 4, "K": 32 }
},
"clock": {
"hmc7044_rx_channel": 12,
"hmc7044_tx_channel": 13
}
}
Compiling the Overlay
dtc -@ -I dts -O dtb \
-o examples/xsa/output/ad9081_zcu102.dtbo \
examples/xsa/output/ad9081_zcu102.dtso
The -@ flag preserves external symbol references (the &amba phandle)
required for overlay application at runtime via configfs.
Loading the Overlay at Runtime
With CONFIG_OF_OVERLAY=y in the target kernel (the default in Kuiper
2023_R2 and later), a .dtbo can be applied on a running system via
configfs. After copying the .dtbo to the target (e.g. /tmp/):
# Apply: creates an entry, writes the path, kernel applies the overlay
mkdir -p /sys/kernel/config/device-tree/overlays/ad9081_zcu102
echo -n /tmp/ad9081_zcu102.dtbo \
> /sys/kernel/config/device-tree/overlays/ad9081_zcu102/path
# Remove: drivers are unbound, phandles added by the overlay are torn down
rmdir /sys/kernel/config/device-tree/overlays/ad9081_zcu102
The hardware test test/hw/xsa/test_ad9081_zcu102_overlay.py exercises
the full lifecycle (load → verify JESD DATA + DMA loopback → unload →
reload) against a live ZCU102. Reuse its helpers in
test/hw/hw_helpers.py (compile_dtso_to_dtbo, deploy_dtbo_via_shell,
load_overlay, unload_overlay) when building your own runtime
overlay flow.