Source Synchronous Interface

This page presents a possible design solution for a source synchronous interface, which can be used to interface any converter that has a source synchronous data interface. The main focus is on the generic interface architecture; information regarding FPGA vendor specific hardware modules and IPs can be found on the respective FPGA manufacturer site, some of which are linked in the References section below.

What is a Source Synchronous Interface?

A source synchronous interface is a common interface type for chip-to-chip communication. The base idea behind the interface is to send a copy of the clock along with the data, which simplifies the timing model of the interface. This interface type is a successor of the system synchronous interface, where both the source and destination IC receive the clock from a common source (clock generator IC).

Architecture

Source synchronous interface implementation

In general, a source synchronous interface consists of a clock reception module, which contains all the necessary IO resource instances to receive the digital interface clock from the device. Depending on the device type, it may also contain a data reception and/or a data transmission module. The interface exposed to the FPGA logic is a simplified FIFO interface in the CORE_CLK domain, made of per-channel enable, valid and data signals, like the Write FIFO interface of the Generic AXI ADC IP core.

The CORE_CLK can have the same frequency as the PHY_CLK, or an integer division of the PHY_CLK frequency. The general rule of thumb is to keep the CORE_CLK frequency below 200 MHz, since it is used throughout the data path and a too high CORE_CLK can significantly reduce the timing margins, making it difficult (or impossible) to close timing.

If the frequency of the PHY_CLK is too high, SERDES macros are used to convert the interface clock and data rate into a more manageable level.

Implementation with AMD Xilinx FPGAs

Files

Name

Description

library/xilinx/common/ad_data_clk.v

Clock reception module, contains an input clock buffer and a global clock buffer for distribution.

library/xilinx/common/ad_data_in.v

Data reception module, general architecture: ibuf -> idelay -> iddr.

library/xilinx/common/ad_data_out.v

Data transmission module, general architecture: oddr -> odelay -> obuf.

library/xilinx/common/ad_serdes_clk.v

Clock reception module for SERDES architecture, general architecture: ibuf -> mmcm.

library/xilinx/common/ad_serdes_in.v

Data reception module, general architecture: ibuf -> idelay -> iserdes.

library/xilinx/common/ad_serdes_out.v

Data transmission module, general architecture: oserdes -> obuf.

References

Implementation with Intel/Altera FPGAs

Note

The Intel/Altera implementation of this interface is not documented yet.