Creating a new IP
Here is a quick start guide about creating a new IP. You can start from these
files and modify them as you need.
Here is the code for a fan control IP: library/axi_fan_control.
In this tutorial, we will make a led control IP, using AXI. In this case,
<module_name> will be replaced in code with axi_led_control for Xilinx
and axi_led_control_intel for Intel.
Verilog File
Consider you want to make a new IP with the name <module_name>.
You must edit the verilog file so that it has the same name (e.g. axi_led_control.v).
After that, feel free to write the verilog code for your purpose.
You can also use other instances of modules, but be sure to include them after,
in the tcl file, under the <other_components> list.
Register Map
The register map is defined in a docs/regmap/adi_regmap_*.txt file and follows a special syntax.
One file can have more than one register map, and they are bounded by the header:
TITLE
[USING <regmap_to_inherit> ...]
<title> (<ip_name>)
<unique_id>
ENDTITLE
Example:
TITLE
SPI Engine (axi_spi_engine)
AXI_SPI_ENGINE
ENDTITLE
The USING method is only present if the register map imports other register
maps for look-up.
The register and fields are defined with the following syntax:
REG
<address>
[WHERE n IS ...]
<name>
<description>
ENDREG
FIELD
[31:0] <default>
[WHERE n IS ...]
<description>
<access>
ENDFIELD
For example:
REG
0x00000001
VERSION
Version of the peripheral.
Follows semantic versioning. Current version 1.00.71.
ENDREG
FIELD
[31:16] 0x00000001
VERSION_MAJOR
RO
ENDFIELD
FIELD
[15:8] 0x00000001
VERSION_MINOR
RO
ENDFIELD
FIELD
[7:0] 0x00000071
VERSION_PATCH
RO
ENDFIELD
The WHERE line is only present if using ranged register/fields.
Noticed that the description can be multi-line and can also include Sphinx syntax, parsed during build. The file content is always 90-columns wide. There are multiple ways to define the default value for a field. All parameter values used for defining or calculating the default value of a field must be a configuration parameter. In cases where expressions are used to calculate the field values, these must be compatible SystemVerilog, as the expressions are used in the simulation environment as well.
FIELD
[31:0]
SCRATCH
RO
Value of the Scratch field is undefined.
In a simulation environment this value appears as X for all bits.
ENDFIELD
FIELD
[31:0] 0x12345678
VERSION
RO
Value of the Version is hardcoded in the IP.
ENDFIELD
FIELD
[31:0] ID
PERIPHERAL_ID
RO
Value of the ID configuration parameter.
In case of multiple instances, each instance will have a unique ID.
ENDFIELD
FIELD
[31:0] SPECIAL = (VALUE1+(VALUE2-VALUE3)*VALUE4)/VALUE5
SPECIAL
RO
Value of the SPECIAL field is calculated using an expression.
Example of simple operations
ENDFIELD
FIELD
[31:0] SPECIAL = (VALUE1>VALUE2)?VALUE3:VALUE4
SPECIAL
RO
Value of the SPECIAL field is calculated using an expression.
Example of conditional calculation
ENDFIELD
FIELD
[31:0] SPECIAL = `MAX(VALUE1,`MIN(VALUE2,VALUE3))
SPECIAL
RO
Value of the SPECIAL field is calculated using an expression.
Example of min and max value calculation
ENDFIELD
FIELD
[31:0] SPECIAL = $clog2(VALUE1**VALUE2)
SPECIAL
RO
Value of the SPECIAL field is calculated using an expression.
Example of log2 and exponentiation calculation
ENDFIELD
Examples:
docs/regmap/adi_regmap_adc.txt, uses
WHEREdocs/regmap/adi_regmap_axi_ad35xxr.txt, uses
USING
Importing with Using Method
The USING method allows looking up a register map to import register and
fields.
A register map can look up multiple register maps by repeating the method for
each register map, for example:
TITLE
USING COMMON_REGS
USING COMMON_REGS_EXTRA
My IP (my_ip)
MY_IP
ENDTITLE
If using the USING method for look-up, registers and fields are imported
with the following syntax:
REG
<reg_to_import>
ENDREG
FIELD
[<field_to_import> ...]
ENDFIELD
That means, only include the register/field name, and nothing else. For example:
REG
CNTRL_1
ENDREG
FIELD
SDR_DDR_N
SYMB_8_16B
ENDFIELD
If inheriting registers from multiple register maps, consider explicitly setting the source register map:
REG
COMMON_EXTRA.CTRL
ENDREG
FIELD
SOME_FIELD
ENDFIELD
Some considerations:
Imported registers shall have non-imported fields, for example, when importing a register that is reserved for custom implementation.
Imported fields must be inside an imported register, since the field name is not unique.
Multiple fields can be imported from a single
FIELDgroup.Multiple register maps can be used for lookup. Add each in a different
USINGmethod.
Ranged Registers and Fields
Registers and fields can use a special n variable and the WHERE method
to define an incrementing/repeating register/field. There is an option increase
the address increment value by an additional parameter. This parameter must be
in hexadecimal format as well.
The syntax is WHERE n IS FROM <lower> TO <UPPER>, for example, for registers:
REG
0x0102 + n
WHERE n IS FROM 0 TO 15
CHAN_CNTRLn_3
DAC Channel Control & Status (channel - 0)
ENDREG
REG
0x0102 + 0x16*n
WHERE n IS FROM 0 TO 15
CHAN_CNTRLn_3
DAC Channel Control & Status (channel - 0)
ENDREG
And for fields:
FIELD
[n]
WHERE n IS FROM 0 TO 31
ES_RESETn
RW
Controls the EYESCANRESET pin of the GTH/GTY transceivers for lane n.
ENDFIELD
To ease the process of creating a new regmap with imported registers you can use the generic adc/dac templates that include all available registers:
Xilinx
TCL File
The tcl file should be named <module_name_ip>.tcl (ex: axi_led_control_ip.tcl).
Here you should keep the two lines that source our scripts :
source ../scripts/adi_env.tcl
source $ad_hdl_dir/library/scripts/adi_ip_xilinx.tcl
Then take a look at the commands
adi_ip_create <module_name>
adi_ip_files <module_name> [list <other_components>]
These commands create the IP and add the dependencies for it.
By <other_components> we refer to the modules we were talking about above,
that must be included in the tcl file. Also, <other_components> must include
the verilog file for the IP itself, named <module_name>.v.
If your new IP uses AXI Lite for register control, then the next command is
adi_ip_properties <module_name>
It is used to initialize properties like memory and so on. If the IP does not use AXI, then you should use
adi_ip_properties_lite <module_name>
At the end of the file don’t forget to save the IP by using this command
ipx::save_core [ipx::currentcore]
If you need more help, here is an example of an IP called axi_led_control. You can open it side by side with the tcl file from the original axi_fan_control and apply the same logic to make your changes.
# ip
source ../scripts/adi_env.tcl
source $ad_hdl_dir/library/scripts/adi_ip_xilinx.tcl
adi_ip_create axi_led_control
adi_ip_files axi_led_control [list \
"$ad_hdl_dir/library/common/up_axi.v" \
"axi_led_control.v"]
adi_ip_properties axi_led_control
set cc [ipx::current_core]
ipx::save_core $cc
Makefile
In this file you will also have to change/add paths to every file in <other_components>
list, using GENERIC_DEPS.
Make sure to also change LIBRARY_NAME and XILINX_DEPS to match the name for the new IP.
If you need more help, here is an example of an IP called axi_led_control. You can open it side by side with the Makefile from the original axi_fan_control and apply the same logic to make your changes.
LIBRARY_NAME := axi_led_control
GENERIC_DEPS += ../common/up_axi.v
GENERIC_DEPS += axi_led_control.v
XILINX_DEPS += axi_led_control_ip.tcl
include ../scripts/library.mk
Now you can run the famous make in command line from the IP directory.
After that, <module_name> will be accessible within vivado for future integrations.
Intel
TCL File
The tcl file should be named <module_name_hw>.tcl (ex: axi_led_control_intel_hw.tcl) These first 4 lines of code you should keep:
package require qsys 14.0
package require quartus::device
source ../scripts/adi_env.tcl
source ../scripts/adi_ip_intel.tcl
After that, the next line creates the new IP:
ad_ip_create <module_name> {entity_name}.
The module_name is the name of the IP you are creating, but entity_name will be the one visible inside Quartus IP Catalogue.
Next, you must add the other components used for creating the IP. For this, we will use the ad_ip_files command:
ad_ip_files <module_name> [list <other_components>]
The <other_components> list is referring to any other verilog file imported
or used.
It must also include the verilog file for the IP itself (<module_name>.v).
Now let’s add an instance of AXI:
ad_ip_intf_s_axi s_axi_aclk s_axi_aresetn 10
This command instantiates an interface using axi. The parameters refer to the ports of the interface, while the number refers to the width of the data bus.
There should be added an interface for every port of the IP. In this example, there is only one port left: led_on. This port is also external, so that’s what conduit is there for.
add_interface led_on_if conduit end
add_interface_port led_on_if led_on data Output 1
The last line is related to the port in the verilog file. In this case, led_on.
The other parameters refer to <signal_type> <direction> <width_expression>.
In Quartus there is no need to save the core or run make afterwards. It is smart enough to search for _hw.tcl in the library directory. Although, you might need to add the path to the new IP in the IP Catalogue.
If you want to see the whole file, here is an example named axi_led_control_intel.
package require qsys 14.0
package require quartus::device
source ../scripts/adi_env.tcl
source ../scripts/adi_ip_intel.tcl
ad_ip_create axi_led_control_intel {AXI LED CONTROL}
ad_ip_files axi_led_control_intel [list \
$ad_hdl_dir/library/common/up_axi.v \
axi_led_control_intel.v]
#axi4 subordinate
ad_ip_intf_s_axi s_axi_aclk s_axi_aresetn 10
#output led
add_interface led_on_if conduit end
add_interface_port led_on_if led_on data Output 1
Makefile
You don’t need to run make for the IP to be visible in the Catalogue. Yet, here is the Makefile for the example mentioned before:
LIBRARY_NAME := axi_led_control_intel
GENERIC_DEPS += ../common/up_axi.v
GENERIC_DEPS += axi_led_control_intel.v
INTEL_DEPS += axi_led_control_intel_hw.tcl
include ../scripts/library.mk
This example was made starting from the axi_ad9361 IP found in our repo, under the library directory: library/axi_ad9361.
Lattice
TCL File
The tcl file which creates the IP must be named by the following standard:
<top_module_name>_ltt.tcl. We set the LIBRARY_NAME := <top_module_name>
in the Makefile and run the tcl script based on that naming standard.
The tcl file must start with two tcl dependencies:
source ../../scripts/adi_env.tcl
source $ad_hdl_dir/library/scripts/adi_ip_lattice.tcl
The adi_env.tcl sets some build related and versioning variables, and the
default hdl directory variable. The adi_ip_lattice.tcl file contains all the
procedures for creating IPs in the ipl namespace. The IP procedures can be
called like: ipl::<procedure_name>.
Namespace for Lattice IP packaging
There are two main parts of procedures and structures in this namespace:
IP related procedures and descriptors for users:
$::ipl::ip- This describes an IP itself. It is used to set a new IP instance like:set ip $::ipl::ip. After the instance is correctly configured, it is used to generate an actual IP on a specified path. This instance is updated by every IP related procedure like:set ip [<some_ip_procedure> -ip $ip]except theipl::generate_ipandipl::parse_module. You will see later on in example.ipl::general- Sets the IP structure with the specified general IP parameters.ipl::parse_module- This module is used to parse the data of the IP top module, it’s input parameter is the file path of the top module and it returns a structure with the top module’s data which is parameter for other procedures.ipl::add_ports_from_module- It is used to set the IP structure with the port’s data from the module data which is set byipl::parse_moduleipl::add_memory_map- Sets the IP structure with a new memory map, the name of this memory map must be used for slave memory mapped interface configuration.ipl::add_address_space- Sets the IP structure with an address space, the name of this address space must be used for master memory mapped interface configuration.ipl::add_axi_interfaces- Automatically adds AXI interfaces based on parsed module data from top module.ipl::add_interface- Sets the IP structure with an interface instance.ipl::add_interface_by_prefix- Sets the IP structure with an interface by filtering ports by prefix from module data parsed withipl::parse_modulewhen a naming standard like<verilog_prefix>_<standard_port_name>is used.ipl::add_ip_files- Sets the IP structure with IP file dependenciesipl::add_ip_files_auto- Sets the IP structure with the specified file dependencies by searching them in the specified-spathfolder-sdepthdeep.ipl::set_parameter- Sets the IP structure with a configuration parameter which will appear in the IP GUI also.ipl::ignore_ports- Ignores/Hides a list of ports by a Python expression which usually depends on the value of a Verilog parameter.ipl::ignore_ports_by_prefix- Ignores/Hides ports which are matching with a specified prefix from the ports’ names in the parsed ports from the top module, by a Python expression which usually depends on the value of a Verilog parameter.ipl::generate_ip- Generates the IP on specified path, if no path parameter then in default IP download directory of Lattice Propel Builder.
Custom IP interface related descriptors and procedures for users:
$::ipl::if- This describes an IP interface structure, it is used to set a new interface instance like:set if $::ipl::ifipl::create_interface- Creates a custom interface.ipl::generate_interface- Generates a custom interface from the structure set byipl::create_interface.
Example for creating an IP
The following section is a generic example for creating IPs which is trying to simulate most of the available options when creating a new IP.
source ../../scripts/adi_env.tcl
source $ad_hdl_dir/library/scripts/adi_ip_lattice.tcl
# Parsing ports and parameters from top module.
# In order to this procedure to work correctly please define your top module
# by following the HDL coding guideline.
set mod_data [ipl::parse_module ./<top_module_name>.v]
# Initializing the IP structure.
set ip $::ipl::ip
# Adding all the ports to the IP from $mod_data.
set ip [ipl::add_ports_from_module -ip $ip -mod_data $mod_data]
# Adding parameters from the $mod_data. This procedure automatically adds
# all the parameters found in top module, but it is useful only if we use
# them as they are and the ordering and grouping of them does not count.
# NOTE: Do not use it if you want to organize the GUI parameters, in that
# case you should add the parameters manually by the following
# ipl::set_parameter procedure.
set ip [ipl::add_parameters_from_module -ip $ip -mod_data $mod_data]
#Getting the name of the top module. <top_module_name>
set mod_name [dict get $mod_data mod_name]
# Setting the general IP parameters.
# There are two optional parameters for this procedure: -max_radiant_version
# -max_esi_version
set ip [ipl::general \
-vlnv "analog.com:ip:$mod_name:1.0" \
-display_name "<Display name of the IP>" \
-supported_products {*} \
-supported_platforms {esi radiant} \
-category "<IP Category>" \
-keywords "<keywords related to the IP>" \
-min_radiant_version "2023.2" \
-min_esi_version "2023.2" \
-href "<https://example_webpage/ip>" \
-ip $ip]
# If the IP has AXI interfaces and the naming standard
# <interface_name>_<standard_ip_portname> is used then you can use the
# following procedure to add all the AXI interfaces to the IP.
# The supported interfaces are AXI4, AXI4-Lite and AXI4-Stream.
set ip [ipl::add_axi_interfaces -ip $ip -mod_data $mod_data]
# You can define memory maps for every slave memory mapped interface.
# You must use its name in the following 'ipl::add_interface' procedure at
# '-mem_map_ref' option, then the memory map defined here will be used
# for the memory mapped interface we are following to define.
set ip [ipl::add_memory_map -ip $ip \
-name "<interface_name>_mem_map" \
-description "<interface description>" \
-baseAddress 0 \
-range 65536 \
-width 32]
# You can add interface manually by defining it with a portmap.
# Make sure that the standard port names match the port names in defined
# interfaces. You must define a '-mem_map_ref' anytime you add a memory mapped
# interface, otherwise the option is not used. If no memory map with that
# reference is created the procedure creates a default memory map
# automatically with the specified '-mem_map_ref'.
set ip [ipl::add_interface -ip $ip \
-inst_name <interface_name> \
-display_name "<interface display name>" \
-description "<interface description>" \
-master_slave slave \
-portmap [list {"s_apb_paddr" "PADDR"} \
{"s_apb_penable" "PENABLE"} \
{"s_apb_prdata" "PRDATA"} \
{"s_apb_pready" "PREADY"} \
{"s_apb_pselx" "PSELx"} \
{"s_apb_pslverr" "PSLVERR"} \
{"s_apb_pwdata" "PWDATA"} \
{"s_apb_pwrite" "PWRITE"}] \
-mem_map_ref <interface_name>_mem_map \
-vlnv {amba.com:AMBA3:APB:r1p0}]
# In most of the cases the containing folder names are describing the vlnv
# for the existing interfaces as in the following example:
# lscc/propel/<tool_version>/builder/rtf/ip/interfaces/amba.com/AMBA3/APB/r1p0
# If you want to update a memory map you can use this anytime.
# The identifier of a memory map is its '-name' which is referred as
# '-mem_map_ref' at ipl::add_interface procedure.
set ip [ipl::add_memory_map -ip $ip \
-name "<interface_name>_mem_map" \
-description "<interface description>" \
-baseAddress 0 \
-range 65536 \
-width 32]
# When you add a master memory mapped interface you can define a memory map
# for it. If you do not define it separately it will be created automatically
# when you add the interface and specify the '-addr_space_ref' option
# at ipl::add_interface procedure.
set ip [ipl::add_address_space -ip $ip \
-name "<interface_name>_aspace" \
-range 0x100000000 \
-width 32]
# Example adding a master memory mapped interface.
set ip [ipl::add_interface -ip $ip \
-inst_name <interface_name> \
-display_name "<interface display name>" \
-description "<interface description>" \
-master_slave master \
-portmap [list {"s_apb_paddr" "PADDR"} \
{"s_apb_penable" "PENABLE"} \
{"s_apb_prdata" "PRDATA"} \
{"s_apb_pready" "PREADY"} \
{"s_apb_pselx" "PSELx"} \
{"s_apb_pslverr" "PSLVERR"} \
{"s_apb_pwdata" "PWDATA"} \
{"s_apb_pwrite" "PWRITE"}] \
-addr_space_ref <interface_name>_aspace \
-vlnv {amba.com:AMBA3:APB:r1p0}]
# Example adding parameters to the IP.
# You must use the Verilog parameter name at '-id' option.
# You can check the Lattice Propel Builder IP Packager documentation for parameter
# use cases as Setting Nodes at:
# https://www.latticesemi.com/view_document?document_id=54003
# The same options in the tables are used here as options for the procedure.
# If you want parameters to appear in the same <Subgoup> in the same <Tabgroup>
# you must add them one after another in the preferred order.
set ip [ipl::set_parameter -ip $ip \
-id <verilog_parameter> \
-type param \
-value_type int \
-conn_mod <verilog_module_name> \
-title {<Title>} \
-options {[('Option 1', 0), ('Option 2', 1), ('Option 3', 2)]} \
-editable {(<some_parameter> == 0)} \
-default 0 \
-output_formatter nostr \
-group1 {<Subgoup>} \
-group2 {<Tabgroup>}]
set ip [ipl::set_parameter -ip $ip \
-id DATA_WIDTH \
-type param \
-value_type int \
-conn_mod <verilog_module_name> \
-title {<Title>} \
-options {[16, 32, 64, 128, 256, 512, 1024, 2048]} \
-default 64 \
-output_formatter nostr \
-group1 {<Subgoup>} \
-group2 {<Tabgroup>}]
set ip [ipl::set_parameter -ip $ip \
-id ENABLE \
-type param \
-value_type int \
-conn_mod <verilog_module_name> \
-title {<Title>} \
-options {[(True, 1), (False, 0)]} \
-default 0 \
-output_formatter nostr \
-group1 {<Subgoup>} \
-group2 {<Tabgroup>}]
# Two options to ignore and hide ports in the GUI.
set ip [ipl::ignore_ports_by_prefix -ip $ip \
-mod_data $mod_data \
-v_prefix s_apb \
-expression {(ENABLE == 0)}]
set ip [ipl::ignore_ports -ip $ip \
-portlist {s_apb_paddr s_apb_pwdata} \
-expression {(ENABLE == 0)}]
# Defining the rtl file dependencies. The files defined here will be copied
# to 'rtl' folder in the generated IP directory. The 'rtl' output directory
# must be used for the rtl files.
# For constraint files the 'ldc' folder must be used at '-dpath' option.
# The following are the standard directories by purpose:
# eval, plugin, doc, rtl, testbench, driver, ldc.
# You can check the Lattice Propel Builder IP Packager documentation for more
# information at: https://www.latticesemi.com/view_document?document_id=54003
set ip [ipl::add_ip_files -ip $ip -dpath rtl -flist [list \
"<path>/<dependency0>.v" \
"<path>/<dependency1>.sv"]
# You can also create your own interfaces.
# The options for ports are the following:
# -n <logical_name>
# -d <in/out> #direction
# -p <required/optional> #presence
# -w <port_width>
# -q <clock/reset/data/address> #qualifier #default is data
# We usually put these in a separate script for make, but you can use it here.
set if [ipl::create_interface
-vlnv {analog.com:ADI:fifo_wr:1.0}
-directConnection true \
-isAddressable false \
-description "ADI fifo wr interface" \
-ports {
{-n DATA -d out -p required}
{-n EN -d out -p required -w 1}
{-n OVERFLOW -w 1 -p optional -d in}
{-n SYNC -p optional -w 1 -d out}
{-n XFER_REQ -p optional -w 1 -d in}
}]
# This will generate the interface in ./<vendor> directory and in
# the default interface directory of Lattice Propel Builder
# (~/PropelIPLocal/interfaces) if the LATTICE_DEFAULT_PATHS env variable
# is exported like: 'export LATTICE_DEFAULT_PATHS=1' before running the
# script or running make.
# You can remove it by deleting the interface folder from this directory.
# You can use a second path parameter to generate it on a specified path.
# For make it is a dedicated file for generating interfaces namely
# 'library/interfaces_ltt/interfaces_ltt.tcl' where you can add new
# interfaces and edit the 'library/interfaces_ltt/Makefile' to work
# correspondingly.
ipl::generate_interface $if
# You can add it to the IP.
set ip [ipl::add_interface -ip $ip \
-inst_name fifo_wr \
-display_name fifo_wr \
-description fifo_wr \
-master_slave slave \
-portmap { \
{"fifo_wr_en" "EN"} \
{"fifo_wr_din" "DATA"} \
{"fifo_wr_overflow" "OVERFLOW"} \
{"fifo_wr_xfer_req" "XFER_REQ"} \
} \
-vlnv {analog.com:ADI:fifo_wr:1.0}]
# Generating the IP given as first parameter on the path given as the second
# parameter. Without the second parameter the IP will be generated in
# ./ltt directory and in the default IP download directory of
# Lattice Propel Builder (~/PropelIPLocal) if the LATTICE_DEFAULT_PATHS
# env variable is exported like:
# 'export LATTICE_DEFAULT_PATHS=1' before running the script or running make.
ipl::generate_ip $ip
Simulation IPs (Lattice Propel Builder / QuestaSim)
Some Lattice verification flows require packaging simulation-only helpers (bus
models, behavioral VIP, top-level harnesses) as standard Propel Builder
IPs so they can be instantiated from system_v_pb.tcl and exported toward
QuestaSim. When creating these IPs:
- Set the VLNV (<vendor>:<library>:<name>:<version>) library to
-vlnv <vendor>:sim_model:<name>:<version>. This is mandatory: it differentiates simulation helpers from synthesizable IPs and gives the block-design scripts a dedicated namespace for referencing them.
- Keep the
namefield identical to the top module name, this is the field used to select the top module for the IP.
- Keep the
- Reference the IP from the project’s
system_v_pb.tclso Propel Builder instantiates it alongside the DUT and VIP blocks.
- Reference the IP from the project’s
Example resources for these flows:
- Verification IP example:
library/spi_engine/sim/spi_sdo_sin_tb includes the Propel Builder wrapper around the SPI Engine stimulus.
- VIP instantiation and verification block design script example:
projects/ad738x_fmc/lfcpnx/system_v_pb.tcl shows how the simulation VLNV is wired next to the DUT.
See also Running the simulation design (where available) for how these IPs plug into the Questasim make targets.
Makefile
In this file you will also have to change/add paths to every file dependency for
the IP, using GENERIC_DEPS for generic dependencies, LATTICE_DEPS for
Lattice specific file dependencies, LATTICE_INTERFACE_DEPS for Lattice
interface dependencies. We set the Lattice interface dependencies when we need
custom interfaces to LATTICE_INTERFACE_DEPS := interfaces_ltt where
interfaces_ltt means the hdl/library/interfaces_ltt directory where the
make script will enter in order to generate the interfaces defined there. If you
want to add a new interface, you can add it to
hdl/library/interfaces_ltt/interfaces_ltt.tcl file then update the
hdl/library/interfaces_ltt/Makefile correspondingly.
Make sure you set the LIBRARY_NAME correctly.
The following is an example for Makefile:
LIBRARY_NAME := <top_module_name>
GENERIC_DEPS += ../common/up_axi.v
GENERIC_DEPS += <top_module_name>.v
LATTICE_DEPS += <top_module_name>_ltt.tcl
LATTICE_INTERFACE_DEPS += interfaces_ltt
include ../scripts/library.mk
Now you can run make from the IP directory.
After that the IP will be accessible in Lattice Propel Builder.