ADMX6001-EBZ HDL project
channel 10GSPS digitizer featuring the low noise 12-bit high-speed ADC AD9213 and the 20-bit precision ADC AD4080. The dual-path design achieves true low noise digitization in the broad band from DC to 5GHz. By biasing the ADC driver ADL5580 with the precision DAC LTC2664, it is capable of handling unipolar and bipolar signals at various DC levels, maximizing utility of the input dynamic range of AD9213. This design is ideal for high performance time-domain instruments such as time-of-flight mass spectrometry (TOFMS), distributed fiber optic sensing (DFOS), and digital oscilloscope.
The ADMX6001-EBZ reference design is a processor based (e.g. Microblaze) embedded system.
The design implements a high-speed receive chain using JESD204B and a precision data path using the custom interface IP AXI AD408X.
The receive chain transports the captured samples from ADC to the system memory (DDR). Before transferring the data to DDR the samples are stored in a buffer implemented on block rams from the FPGA fabric (util_adcfifo).
All cores from the receive chain are programmable through an AXI-Lite interface.
Supported boards
Supported devices
Supported carriers
Evaluation board |
Carrier |
FMC slot |
|---|---|---|
FMC+ |
Block design
Block diagram
The data path and clock domains are depicted in the below diagrams:
Important
The Rx links (AD9213 ADC Path) operate with the following parameters:
Rx parameters: L=16, M=1, F=2, S=16, NP=16, N=16
Sample Rate: 10 GSPS
Dual link: No
RX_DEVICE_CLK: 312.25 MHz (Lane Rate/40)
REF_CLK: 625 MHz (Lane Rate/20)
JESD204B Lane Rate: 12.5 Gbps
QPLL0
Clock scheme
CPU/Memory interconnects addresses
The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).
Check-out the table below to find out the conditions.
Instance |
Zynq/Microblaze |
|---|---|
axi_ad4080_adc |
0x44A0_0000 |
rx_ad9213_tpl_core |
0x44A1_0000 |
axi_ad4080_dma |
0x44A3_0000 |
axi_ad9213_xcvr |
0x44A6_0000 |
hmc7044_spi |
0x44A7_1000 |
ad4080_spi |
0x44A7_2000 |
adl5580_spi |
0x44A7_3000 |
ltc2664_spi |
0x44A7_4000 |
axi_ad9213_jesd |
0x44A9_0000 |
axi_ad9213_dma |
0x44B0_0000 |
SPI connections
SPI type |
SPI manager instance |
SPI subordinate |
CS |
|---|---|---|---|
PL |
axi_spi |
AD9213 |
0 |
PL |
hmc7044_spi |
HMC7044 |
0 |
PL |
hmc7044_spi |
ADF4371 |
1 |
PL |
ltc2664_spi |
LTC2664 |
0 |
PL |
adl5580_spi |
ADL5580 |
0 |
PL |
ad4080_spi |
AD4080 |
0 |
GPIOs
To know how the Software GPIO numbers are calculated, check out GPIOs - HDL Architecture page.
GPIO Signal |
Direction |
HDL no. |
MicroBlaze |
|---|---|---|---|
ltc2664_tgp |
INOUT |
55 |
55 |
ltc2664_clr |
INOUT |
54 |
54 |
ltc2664_ldac |
INOUT |
53 |
53 |
adl5580_en |
INOUT |
52 |
52 |
ada4945_disable |
INOUT |
51 |
51 |
adg5419_ctrl |
INOUT |
50 |
50 |
adrf5203_ctrl[2:0] |
INOUT |
49:47 |
49:47 |
hmc7044_sync_req |
INOUT |
46 |
46 |
ad9213_rstb |
INOUT |
45 |
45 |
dig_ext_gpio[1:0] |
INOUT |
44:43 |
44:43 |
dig_ext_p |
INOUT |
42 |
42 |
dig_ext_n |
INOUT |
41 |
41 |
dig_ext_hs_p |
INOUT |
40 |
40 |
dig_ext_hs_n |
INOUT |
39 |
39 |
ad4080_gpio[3:2] |
INOUT |
38:37 |
38:37 |
ad9213_gpio[4:0] |
INOUT |
36:32 |
36:32 |
Legend
GPIO signal = name of the GPIO in the HDL project
Direction = from the FPGA point of view
HDL no. = HDL GPIO EMIO range
MicroBlaze = Software GPIO (Linux GPIO numbers) to be used in device trees
Interrupts
Below are the Programmable Logic interrupts used in this project.
Instance name |
IRQ number |
|---|---|
axi_ad9213_jesd |
6 |
axi_ad4080_dma |
7 |
axi_ad9213_dma |
8 |
hmc7044_spi |
12 |
ad4080_spi |
13 |
adl5580_spi |
14 |
ltc2664_spi |
15 |
Building the HDL project
The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository.
Then go to the projects/admx6001_ebz location and run the make command by typing in your command prompt:
Linux/Cygwin/WSL
~$
cd hdl/projects/admx6001_ebz/vcu118
~/hdl/projects/admx6001_ebz/vcu118$
make
A more comprehensive build guide can be found in the Build an HDL project user guide.
Resources
More information
Support
Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.
For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.
For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.
It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.