HDL
HDL
  • JESD204B/C Link Receive Peripheral
    • Features
    • Files
    • Block Diagram
    • AXI JESD204 RX Synthesis Configuration Parameters
    • JESD204 RX Synthesis Configuration Parameters
    • AXI JESD204 RX Signal and Interface Pins
    • JESD204 RX Signal and Interface Pins
    • Register Map
    • Theory of Operation
      • Interfaces and Signals
        • Register Map Configuration Interface
        • JESD204 Control Signals
        • Transceiver Interface (RX_PHYn)
        • User Data Interface (RX_DATA)
      • Configuration Interface
        • Peripheral Identification and HDL Synthesis Settings
        • Interrupt Handling
        • Link Control
        • Multi-link Control
        • Link Configuration
        • SYSREF Handling
        • Link Status
        • Lane Status
          • 8B/10B Link Lane Status Fields
          • 64B/66B Link Lane Status Fields
        • 8B/10B Link ILAS Configuration Data
        • Clock Monitor
      • Interrupts
    • 8B/10B Link
      • 8B/10B Link State Machine
        • RESET phase
        • WAIT FOR PHY phase
        • CGS phase
        • DATA phase
      • 8B/10B Multi-endpoint RX link establishment
    • 64B/66B Link
      • 64B/66B Link State Machine
        • RESET phase
        • WAIT BS phase
        • BLOCK SYNC phase
        • DATA phase
      • 64B/66B Link Extended MultiBlock Alignment State Machine
        • EMB INIT State
        • EMB HUNT State
        • EMB LOCK State
    • Dual clock operation
    • 64b/66b Link latency reduction
    • Software Support
    • Restrictions
    • Additional Information
    • Supported Devices
      • JESD204B Analog-to-Digital Converters
      • JESD204B RF Transceivers
      • JESD204B/C Mixed-Signal Front Ends
    • Technical Support
    • More Information
HDL
  • User Guide
    • Introduction
    • Git repository
    • Releases
      • Projects List and Dependencies
        • Projects list and dependencies for main
        • Projects list and dependencies for hdl_2026_r1
        • Projects list and dependencies for hdl_2023_r2
        • Projects list and dependencies for hdl_2022_r2
        • Projects list and dependencies for hdl_2021_r2
        • Projects list and dependencies for hdl_2021_r1
        • Projects list and dependencies for hdl_2019_r2
        • Projects list and dependencies for hdl_2019_r1
        • Projects list and dependencies for hdl_2018_r2
        • Projects list and dependencies for hdl_2018_r1
        • Projects list and dependencies for hdl_2017_r1
        • Projects list and dependencies for hdl_2016_r2
        • Projects list and dependencies for hdl_2015_r1
      • Resource Utilization
        • Resource utilization for main
        • Resource utilization for hdl_2026_r1
        • Resource utilization for hdl_2023_r2
        • Resource utilization for hdl_2022_r2
        • Resource utilization for hdl_2021_r2
        • Resource utilization for hdl_2021_r1
        • Resource utilization for hdl_2019_r2
    • Build an HDL project
    • Build the BOOT.BIN
    • Build the boot.scr
    • Build the Intel Boot Image
    • HDL architecture
    • IP cores
      • Creating a new IP
      • Use ADI IPs into your own project
      • Interfaces
      • Source Synchronous Interface
      • Generic AXI ADC
      • Generic AXI DAC
    • Porting HDL projects
    • Customize HDL projects
    • Debugging with XSDB
    • HDL coding guidelines
    • Documentation guidelines
    • Contributing to HDL
    • Third party forks
  • IP Cores
    • I3C Controller
      • Host Interface
      • Core Module
      • Interface
    • JESD204 Interface Framework
      • System Architecture
      • Generic JESD204 block designs
      • JESD204B/C Link Transmit Peripheral
      • JESD204B/C Link Receive Peripheral
      • ADC JESD204B/C Transport Peripheral
      • DAC JESD204B/C Transport Peripheral
      • Xilinx FPGAs Transceivers Wizard
      • AMD Versal Adaptive SoC Transceiver Subsystem
      • Troubleshooting JESD204 TX links
      • JESD204 Component-Level Testbenches
    • SPI Engine
      • Execution Module
      • AXI Module
      • Offload Module
      • Interconnect Module
      • Control Interface
      • Offload Control Interface
      • SPI Bus Interface
      • Instruction Set Specification
      • Pipeline Delays
      • Tutorial - PulSAR ADC
    • AXI AD35XXR
    • AXI AD408X
    • AXI AD485X
    • AXI AD7405
    • AXI AD7606X
    • AXI AD7616
    • AXI AD7768
    • AXI AD777X
    • AXI AD9265
    • AXI AD9361
      • TDD Mode Support
    • AXI AD9467
    • AXI AD9740
    • AXI AD9783
    • AXI AD9963
    • AXI ADA4355
    • AXI ADAQ8092
    • AXI ADRV9001
    • AXI HMCAD15XX
    • AXI LTC235X
    • AXI LTC2387
    • Data Offload
    • AXI DMAC
    • AXI HDMI RX
    • AXI HDMI TX
    • AXI ADC Decimate
    • AXI ADC Trigger
    • AXI ADF4030
    • AXI ADXCVR
    • AXI CLK Generator
    • AXI Clock Monitor
    • AXI DAC Interpolate
    • AXI Fan Control
    • AXI Laser Driver
    • AXI Logic Analyzer
    • AXI PWM Generator
    • AXI System ID
    • AXI TDD
    • CN0363
      • CN0363 DMA Sequencer
      • CN0363 Phase Data Sync
    • AD Direct Digital Synthesis
    • Corundum Network Stack
      • Corundum Core
      • Corundum Ethernet Core
        • VCU118
        • K26
    • SPI Slave
    • AXI Stream FIFO
    • Asymmetric AXI Stream FIFO
    • Util Extract
    • Util MII to RMII
    • Channel CPACK Utility
    • Channel UPACK Utility
    • Util RFIFO
    • Util Sigma Delta SPI
    • Util VAR FIFO
    • Util WFIFO
    • Intel Specific IPs
      • Util Clock Divider
    • AMD Xilinx Specific IPs
      • UTIL_ADXCVR
  • Projects
    • AD-QUADMXFE1-EBZ
    • AD353XR
    • AD35XXR-EVB
    • AD4052-ARDZ
    • AD4062-ARDZ
    • AD4080-FMC-EVB
    • AD4110-SDZ
    • AD411X-AD717X
    • AD4134-FMC
    • AD4170-ASDZ
    • AD4630-FMC
    • AD469X-EVB
    • AD485X-FMCZ
    • AD4880-FMC-EVB
    • AD5529R-ARDZ
    • AD5706R
    • AD5758-SDZ
    • AD5766-SDZ
    • AD57XX-ARDZ
    • AD6676EVB
    • AD7124-ASDZ
    • AD7134-FMC
    • AD719X-ASDZ
    • AD738X-FMC
    • AD7405-FMC
    • AD7606X-FMC
    • AD7616-SDZ
    • AD7768-1-EVB
    • AD7768-EVB
    • AD777X-FMCZ
    • AD9081-FMCA-EBZ
    • AD9081-FMCA-EBZ-X-BAND
    • AD9083-EVB
    • AD9084-EBZ
    • AD916X-FMC
    • AD9208-DUAL-EBZ
    • AD9209-FMCA-EBZ
    • AD9213-DUAL-EBZ
    • AD9213-EVB
    • AD9265-FMC
    • AD9434-FMC
    • AD9467-FMC
    • AD9656-FMC
    • AD9694-FMC
    • AD9695-FMC
    • AD9740-FMC
    • AD9783-EBZ
    • ADA4355-FMC
    • ADAQ23875
    • ADAQ7980-SDZ
    • ADAQ8092-FMC
    • ADAR3000
    • ADMX100X-EVB
    • ADMX6001-EBZ
    • ADRD8012-01Z
    • ADRV9001
    • ADRV9001-DUAL
    • ADRV9009
    • ADRV9009-ZU11EG
    • ADRV9026
    • ADRV903X
    • ADRV904X
    • ADRV9361Z7035
    • ADRV9364Z7020
    • ADRV9371X
    • ADV7511
    • ADV7513
    • ARRADIO
    • CN0363
    • CN0506
    • CN0540
    • CN0561
    • CN0577
    • CN0579
    • CN0585
    • DAC-FMC-EBZ
    • DAQ2
    • DAQ3
    • DC2677A
    • FMCOMMS2/3/4
      • FMCOMMS2 FIR FILTER
    • FMCOMMS5
    • FMCOMMS8
    • FMCOMMS11
    • HMCAD1520
    • JUPITER-SDR
    • LTC2378-FMC
    • M2K
    • MAX96724
    • PLUTO
    • QUAD-ADA4356
    • QUAD-ADAQ7768-1
    • QUAD-QUAD-MXFE
    • PULSAR-ADC
    • PULSAR-LVDS-ADC
    • ADMX6020M
    • TEST-CAPI-SELFTEST
  1. IP Cores
  2. JESD204 Interface Framework

JESD204B/C Link Receive Peripheral

s_axis_axi_aclks_axi_aresetnrx_ilas_configrx_eventrx_statuscore_clkcore_reset_extdevice_clkrx_cfgirqcore_resetdevice_resetaxi_jesd204_rx

The ADI JESD204B/C Link Receive Peripheral implements the Link layer handling of a JESD204 receive logic device. Implements the 8B/10B based link layer defined in JESD204C standard that is similar to the Link layer defined in JESD204B.

This includes handling of the SYSREF and SYNC~ and controlling the link state machine accordingly, as well as performing per lane descrambling and character replacement.

It implements the 64B/66B-based Link layer defined in the JESD204C standard. This includes handling of the SYSREF, per lane decoding of sync header, descrambling, CRC checking of data blocks and error monitoring.

The type of Link layer is selectable during implementation phase through the LINK_MODE synthesis parameter.

It has been designed for interoperability with Analog Devices JESD204 ADC converter products. To form a complete JESD204 receive logic device, it has to be combined with a PHY layer and transport layer peripheral.

Features

  • Backwards compatibility with JESD204B;

  • 64B/66B Link layer defined in JESD204C;

  • Subclass 0 and Subclass 1 support;

  • Deterministic Latency (for Subclass 1 operation);

  • Runtime reconfigurability through memory-mapped register interface (AXI4-Lite);

  • Interrupts for event notification;

  • Diagnostics;

  • Max Lanerate with 8B/10B mode: 15 Gbps;

  • Max Lanerate with 64B/66B mode: 32 Gbps;

  • Low Latency;

  • Independent per lane enable/disable.

Files

Important

To use this wrapper in your project, you need to use the procedure adi_axi_jesd204_rx_create to instantiate it.

Name

Description

axi_jesd204_rx.v

Verilog source for the peripheral.

axi_jesd204_rx_ip.tcl

TCL script to generate the Vivado IP-integrator project for the peripheral.

Block Diagram

JESD204B/C Rx Link Layer

AXI JESD204 RX Synthesis Configuration Parameters

Name

Description

Default Value

Choices/Range

ID

Instance identification number.

0

NUM_LANES

Maximum number of lanes supported by the peripheral.

1

NUM_LINKS

Maximum number of links supported by the peripheral.

1

LINK_MODE

Decoder selection of the link layer: 1 - 8B/10B mode; 2 - 64B/66B mode.

1

64B66B (2), 8B10B (1)

ENABLE_LINK_STATS

Enable Link Stats.

0

DATA_PATH_WIDTH

Data path width in bytes. Set it to 4 in case of 8B/10B, 8 in case of 64B/66B

4

JESD204 RX Synthesis Configuration Parameters

Name

Description

Default Value

Choices/Range

NUM_LANES

Maximum number of lanes supported by the peripheral.

1

NUM_LINKS

Maximum number of links supported by the peripheral.

1

NUM_INPUT_PIPELINE

Num Input Pipeline.

1

NUM_OUTPUT_PIPELINE

Num Output Pipeline.

1

LINK_MODE

Decoder selection of the link layer: 1 - 8B/10B mode; 2 - 64B/66B mode.

1

64B66B (2), 8B10B (1)

DATA_PATH_WIDTH

Data path width in bytes. Set it to 4 in case of 8B/10B, 8 in case of 64B/66B.

4

ENABLE_FRAME_ALIGN_CHECK

Enable Frame Align Check.

1

ENABLE_FRAME_ALIGN_ERR_RESET

Enable Frame Align Err Reset.

0

ENABLE_CHAR_REPLACE

Enable Char Replace.

0

ASYNC_CLK

Set this parameter to 1 if the link clock and the device clocks have different frequencies, or if they have the same frequency but a different source. If set, synchronizing logic and a gearbox of ratio DATA_PATH_WIDTH:TPL_DATA_PATH_WIDTH is inserted to do the rate conversion. If not set, TPL_DATA_PATH_WIDTH must match DATA_PATH_WIDTH, the same clock must be connected to clk and device_clk inputs.

1

TPL_DATA_PATH_WIDTH

Data path width in bytes towards transport layer. Must be greater or equal to DATA_PATH_WIDTH. Must be a power of 2 integer multiple of the F parameter.

4

SYSREF_IOB

Place SYSREF in IOB.

True

AXI JESD204 RX Signal and Interface Pins

Physical Port

Logical Port

Direction

Dependency

s_axi_awaddr AWADDR

in [13:0]

s_axi_awprot AWPROT

in [2:0]

s_axi_awvalid AWVALID

in

s_axi_awready AWREADY

out

s_axi_wdata WDATA

in [31:0]

s_axi_wstrb WSTRB

in [3:0]

s_axi_wvalid WVALID

in

s_axi_wready WREADY

out

s_axi_bresp BRESP

out [1:0]

s_axi_bvalid BVALID

out

s_axi_bready BREADY

in

s_axi_araddr ARADDR

in [13:0]

s_axi_arprot ARPROT

in [2:0]

s_axi_arvalid ARVALID

in

s_axi_arready ARREADY

out

s_axi_rdata RDATA

out [31:0]

s_axi_rresp RRESP

out [1:0]

s_axi_rvalid RVALID

out

s_axi_rready RREADY

in

Physical Port

Logical Port

Direction

Dependency

s_axi_aclk CLK

in

Physical Port

Logical Port

Direction

Dependency

s_axi_aresetn RST

in

Physical Port

Logical Port

Direction

Dependency

core_cfg_lanes_disable lanes_disable

out [0:0]

core_cfg_links_disable links_disable

out [0:0]

core_cfg_octets_per_multiframe octets_per_multiframe

out [9:0]

core_cfg_octets_per_frame octets_per_frame

out [7:0]

core_cfg_disable_char_replacement disable_char_replacement

out

core_cfg_disable_scrambler disable_scrambler

out

core_cfg_frame_align_err_threshold frame_align_err_threshold

out [7:0]

device_cfg_octets_per_multiframe device_octets_per_multiframe

out [9:0]

device_cfg_octets_per_frame device_octets_per_frame

out [7:0]

device_cfg_beats_per_multiframe device_beats_per_multiframe

out [7:0]

device_cfg_lmfc_offset device_lmfc_offset

out [7:0]

device_cfg_sysref_oneshot device_sysref_oneshot

out

device_cfg_sysref_disable device_sysref_disable

out

device_cfg_buffer_early_release device_buffer_early_release

out

device_cfg_buffer_delay device_buffer_delay

out [7:0]

core_ctrl_err_statistics_reset err_statistics_reset

out

core_ctrl_err_statistics_mask err_statistics_mask

out [6:0]

Physical Port

Logical Port

Direction

Dependency

core_ilas_config_valid valid

in [0:0]

core_ilas_config_addr addr

in [1:0]

core_ilas_config_data data

in [31:0]

Physical Port

Logical Port

Direction

Dependency

device_event_sysref_alignment_error sysref_alignment_error

in

device_event_sysref_edge sysref_edge

in

core_event_frame_alignment_error frame_alignment_error

in

core_event_unexpected_lane_state_error unexpected_lane_state_error

in

Physical Port

Logical Port

Direction

Dependency

core_status_ctrl_state ctrl_state

in [1:0]

core_status_lane_cgs_state lane_cgs_state

in [1:0]

core_status_lane_emb_state lane_emb_state

in [2:0]

core_status_lane_ifs_ready lane_ifs_ready

in [0:0]

core_status_lane_latency lane_latency

in [13:0]

core_status_lane_frame_align_err_cnt lane_frame_align_err_cnt

in [7:0]

core_status_err_statistics_cnt err_statistics_cnt

in [31:0]

status_synth_params0 synth_params0

in [31:0]

status_synth_params1 synth_params1

in [31:0]

status_synth_params2 synth_params2

in [31:0]

Physical Port

Logical Port

Direction

Dependency

irq INTERRUPT

out

Physical Port

Direction

Dependency

Description

core_clk

in

Bus rx_status_rx_event_rx_ilas_config_rx_cfg is synchronous to this clock domain.

core_reset_ext

in

core_reset

out

Bus rx_status_rx_event_rx_ilas_config_rx_cfg is synchronous to this reset signal.

device_clk

in

Device clock for the JESD204 interface. Its frequency must be link clock * DATA_PATH_WIDTH / TPL_DATA_PATH_WIDTH

device_reset

out

Reset active high synchronous with the Device clock.

JESD204 RX Signal and Interface Pins

Physical Port

Logical Port

Direction

Dependency

cfg_lanes_disable lanes_disable

in [0:0]

cfg_links_disable links_disable

in [0:0]

cfg_octets_per_multiframe octets_per_multiframe

in [9:0]

cfg_octets_per_frame octets_per_frame

in [7:0]

cfg_disable_scrambler disable_scrambler

in

cfg_disable_char_replacement disable_char_replacement

in

cfg_frame_align_err_threshold frame_align_err_threshold

in [7:0]

device_cfg_octets_per_multiframe device_octets_per_multiframe

in [9:0]

device_cfg_octets_per_frame device_octets_per_frame

in [7:0]

device_cfg_beats_per_multiframe device_beats_per_multiframe

in [7:0]

device_cfg_lmfc_offset device_lmfc_offset

in [7:0]

device_cfg_sysref_oneshot device_sysref_oneshot

in

device_cfg_sysref_disable device_sysref_disable

in

device_cfg_buffer_delay device_buffer_delay

in [7:0]

device_cfg_buffer_early_release device_buffer_early_release

in

ctrl_err_statistics_reset err_statistics_reset

in

ctrl_err_statistics_mask err_statistics_mask

in [6:0]

Physical Port

Logical Port

Direction

Dependency

status_ctrl_state ctrl_state

out [1:0]

status_lane_cgs_state lane_cgs_state

out [1:0]

status_lane_emb_state lane_emb_state

out [2:0]

status_err_statistics_cnt err_statistics_cnt

out [31:0]

status_lane_ifs_ready lane_ifs_ready

out [0:0]

status_lane_latency lane_latency

out [13:0]

status_lane_frame_align_err_cnt lane_frame_align_err_cnt

out [7:0]

status_synth_params0 synth_params0

out [31:0]

status_synth_params1 synth_params1

out [31:0]

status_synth_params2 synth_params2

out [31:0]

Physical Port

Logical Port

Direction

Dependency

ilas_config_valid valid

out [0:0]

ilas_config_addr addr

out [1:0]

ilas_config_data data

out [31:0]

Physical Port

Logical Port

Direction

Dependency

device_event_sysref_alignment_error sysref_alignment_error

out

device_event_sysref_edge sysref_edge

out

event_frame_alignment_error frame_alignment_error

out

event_unexpected_lane_state_error unexpected_lane_state_error

out

Physical Port

Logical Port

Direction

Dependency

phy_data rxdata

in [31:0]

phy_charisk rxcharisk

in [3:0]

phy_disperr rxdisperr

in [3:0]

phy_notintable rxnotintable

in [3:0]

phy_header rxheader

in [1:0]

phy_block_sync rxblock_sync

in [0:0]

Physical Port

Direction

Dependency

Description

clk

in

Link clock for the JESD204 interface. Must be line clock/40 for correct operation in 8B/10B mode, line clock/66 in 64B/66B mode. Bus rx_cfg_rx_ilas_config_rx_event_rx_status is synchronous to this clock domain.

reset

in

Reset active high synchronous with the Link clock Bus rx_cfg_rx_ilas_config_rx_event_rx_status is synchronous to this reset signal.

device_clk

in

Bus rx_data is synchronous to this clock domain.

device_reset

in

Bus rx_data is synchronous to this reset signal.

sysref

in

JESD204 SYSREF signal.

lmfc_edge

out

lmfc_clk

out

sync

out [0:0]

LINK_MODE = 1

sync[m-1:0] is JESD204 SYNC~ (or SYNC_N) signals, available in 8B/10B mode. (0 <= m < NUM_LINKS)

phy_en_char_align

out

LINK_MODE = 1

Enable transceiver character alignment.

rx_data

out [31:0]

Received data.

rx_valid

out

rx_eof

out [3:0]

rx_sof

out [3:0]

rx_eomf

out [3:0]

rx_somf

out [3:0]

Register Map

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x0 0x0 VERSION

Version of the peripheral. Follows semantic versioning. Current version 1.03.a.

[31:16] VERSION_MAJOR RO 0x0001

[15:8] VERSION_MINOR RO 0x03

[7:0] VERSION_PATCH RO 0x61

0x1 0x4 PERIPHERAL_ID

[31:0] PERIPHERAL_ID RO

Value of the ID configuration parameter.

0x2 0x8 SCRATCH

[31:0] SCRATCH RW

Scratch register useful for debug.

0x3 0xc IDENTIFICATION

[31:0] IDENTIFICATION RO 0x32303452

Peripheral identification (‘2’, ‘0’, ‘4’, ‘R’).

0x4 0x10 SYNTH_NUM_LANES

[31:0] SYNTH_NUM_LANES RO

Number of supported lanes.

0x5 0x14 SYNTH_DATA_PATH_WIDTH

[31:16] RESERVED RO 0x0000

[15:8] TPL_DATA_PATH_WIDTH RO 0x02

Data path width in octets at Transport Layer interface. Available starting from version 1.07.a;

[7:0] SYNTH_DATA_PATH_WIDTH RO 0x02

Log2 of internal data path width in octets. Represents the datapath width towards the physical interface.

0x6 0x18 SYNTH_1

Core description register.

[31:19] RESERVED RO 0x0000

[18] ENABLE_CHAR_REPLACE RO 0x0

This bit reflects the presence of character replacement monitoring logic for cases when scrambling is disabled. Available starting from version 1.07.a;

[17] ENABLE_FRAME_ALIGN_ERR_RESET RO 0x0

If this bit is set in case of frame misalignment is detected the core resets itself. No software intervention is required. If the bit is not set and misalignment is detected the software must restart the link. Available starting from version 1.07.a;

[16] ENABLE_FRAME_ALIGN_CHECK RO 0x1

This bit reflects the presence of frame alignment monitor. Available starting from version 1.07.a;

[12] ASYNC_CLK RO ASYNC_​CLK

This bit is set if link clock and device clock are connected to different sources. This is useful for supporting modes where datapath width is not integer multiple of F. Available starting from version 1.07.a;

[9:8] DECODER RO

Decoder presence:

  • 01 - 8B10B decoder

  • 10 - 64B66B decoder

[7:0] NUM_LINKS RO

Maximum supported links. Valid for 8B/10B encoder.

0x10 0x40 SYNTH_ELASTIC_BUFFER_SIZE

[31:0] SYNTH_ELASTIC_BUFFER_SIZE RO 0x00000100

Elastic buffer size in octets.

0x20 0x80 IRQ_ENABLE

[31:0] IRQ_ENABLE RW 0x00000000

Interrupt enable.

0x21 0x84 IRQ_PENDING

[31:0] IRQ_PENDING RW1CV 0x00000000

Pending and enabled interrupts.

0x22 0x88 IRQ_SOURCE

[31:0] IRQ_SOURCE RW1CV 0x00000000

Pending interrupts.

0x30 0xc0 LINK_DISABLE

JESD204B link disable.

[31:1] RESERVED RO 0x00000000

[0] LINK_DISABLE RW 0x1

0 = Enable link, 1 = Disable link.

0x31 0xc4 LINK_STATE

JESD204B link state.

[31:2] RESERVED RO 0x00000000

[1] EXTERNAL_RESET RO

0 = External reset de-asserted, 1 = External reset asserted.

[0] LINK_STATE RO 0x1

0 = Link enabled, 1 = Link disabled.

0x32 0xc8 LINK_CLK_FREQ

[20:0] LINK_CLK_FREQ ROV

Ratio of the link_clk frequency relative to the s_axi_aclk. Format is 16.16.

0x33 0xcc DEVICE_CLK_FREQ

[20:0] DEVICE_CLK_FREQ ROV

Ratio of the device_clk frequency relative to the s_axi_aclk. Format is 16.16. Available starting from version 1.07.a;

0x40 0x100 SYSREF_CONF

SYSREF configuration

[31:2] RESERVED RO 0x00000000

[1] SYSREF_ONESHOT RW 0x0

In oneshot mode only the first occurrence of the SYSREF signal is used for alignment.

[0] SYSREF_DISABLE RW 0x0

Enable/Disable SYSREF handling.

0x41 0x104 SYSREF_LMFC_OFFSET

SYSREF LMFC offset

[31:10] RESERVED RO 0x000000

[9:0] SYSREF_LMFC_OFFSET RW 0x000

Offset between SYSREF event and internal LMFC event in octets.

0x42 0x108 SYSREF_STATUS

SYSREF status

[31:2] RESERVED RO 0x00000000

[1] SYSREF_ALIGNMENT_ERROR RW1CV 0x0

Indicates that an external SYSREF event has been observed that was unaligned to a previously observed event.

[0] SYSREF_DETECTED RW1CV 0x0

Indicates that an external SYSREF event has been observed.

0x80 0x200 LANES_DISABLE

Enabled/Disabled lanes.

[n] LANE_DISABLEn RW 0x0

Enable/Disable n-th lane (0 = enabled, 1 = disabled). Where n is from 0 to 31.

0x84 0x210 LINK_CONF0

JESD204B link configuration.

[31:19] RESERVED RO 0x0000

[23:16] OCTETS_PER_FRAME RW 0x00

Number of octets per frame - 1 (F).

[15:10] RESERVED RO 0x00

[9:0] OCTETS_PER_MULTIFRAME RW 0x003

Number of octets per multi-frame - 1 (K x F). In 64B/66B mode represents the number of octets per extended multiblock.

0x85 0x214 LINK_CONF1

JESD204B link configuration.

[31:2] RESERVED RO 0x00000000

[1] CHAR_REPLACEMENT_DISABLE RW 0x0

Enable/Disable user data alignment character replacement (0 = enabled, 1 = disabled). Valid for 8B/10B encoder.

[0] DESCRAMBLER_DISABLE RW 0x0

Enable/Disable user data descrambling (0 = enabled, 1 = disabled).

0x86 0x218 MULTI_LINK_DISABLE

Enable/Disable links in case of a multi-link architecture. Valid for 8B/10B encoder.

[n] LINK_DISABLEn RW 0x0

Enable/Disable n-th link (0 = enabled, 1 = disabled). Where n is from 0 to 31.

0x87 0x21c LINK_CONF4

JESD204B link configuration.

[31:8] RESERVED RO 0x000000

[7:0] TPL_BEATS_PER_MULTIFRAME RW 0x00

Number of beats per multi-frame - 1 (K x F / TPL_DATA_PATH_WIDTH) at interface to Transport Layer. In 64B/66B mode represents the number of octets per extended multiblock. Available starting from version 1.07.a;

0x90 0x240 LINK_CONF2

JESD204B link configuration.

[31:17] RESERVED RO 0x0000

[16] BUFFER_EARLY_RELEASE RW 0x0

Elastic buffer release point.

[15:10] RESERVED RO 0x00

[9:2] BUFFER_DELAY RW 0x00

Buffer release opportunity offset from LMFC.

[1:0] RESERVED RO 0x0

0x91 0x244 LINK_CONF3

JESD204B error statistics configuration.

[31:15] RESERVED RO 0x00000

[14] MASK_INVALID_HEADER RW 0x0

If set, invalid header errors are not counted; Valid for 64B/66B encoder.

[13] MASK_UNEXPECTED_EOMB RW 0x0

If set, unexpected end of multiblock errors are not counted; Valid for 64B/66B encoder.

[12] MASK_UNEXPECTED_EOEMB RW 0x0

If set, unexpected end of extended multiblock errors are not counted; Valid for 64B/66B encoder.

[11] MASK_CRC_MISMATCH RW 0x0

If set, CRC mismatch errors are not counted. Valid for 64B/66B encoder.

[10] MASK_UNEXPECTEDK RW 0x0

If set, unexpected k errors are not counted. Valid for 8B/10B encoder.

[9] MASK_NOTINTABLE RW 0x0

If set, not in table errors are not counted. Valid for 8B/10B encoder.

[8] MASK_DISPERR RW 0x0

If set, disparity errors are not counted. Valid for 8B/10B encoder.

[7:1] RESERVED RO 0x00

[0] RESET_COUNTER RW 0x0

If set, resets the error counter

0xa0 0x280 LINK_STATUS

JESD204B link status.

[31:2] RESERVED RO 0x00000000

[1:0] STATUS_STATE ROV 0x0
  • State of the 8B/10B link state machine.

    • 0 = RESET

    • 1 = WAIT_FOR_PHY

    • 2 = CGS

    • 3 = SYNCHRONIZED

  • State of the 64B/66B link state machine.

    • 0 = RESET

    • 1 = WAIT_BS

    • 2 = BLOCK_SYNC

    • 3 = DATA

0xc0 + 0x8*n 0x300 + 0x20*n LANEn_STATUS

Where n is from 0 to 31.

[31:11] RESERVED RO 0x000000

[10:8] EMB_STATE RO 0x0

State of Extended multiblock alignment:

  • 001 - EMB_INIT

  • 010 - EMB_HUNT

  • 100 - EMB_LOCK

Valid for 64b66b encoder.

[7:6] RESERVED RO 0x0

[5] ILAS_READY ROV 0x0

ILAS configuration data received.

[4] IFS_READY ROV 0x0

Frame synchronization state.

[3:2] RESERVED RO 0x0

[1:0] CGS_STATE ROV 0x0

State of the lane code group synchronization. (0 = INIT, 1 = CHECK, 2 = DATA)

0xc1 + 0x8*n 0x304 + 0x20*n LANEn_LATENCY

Where n is from 0 to 31.

[31:14] RESERVED RO 0x00000

[13:0] LATENCY ROV 0x0000

For 8b10b mode: represents the lane latency in octets; For 64b66b mode: represents the delay from the received EOEMB indicator to the next (SYSREF aligned) LEMC edge in octets. In other words, this amount of data is stored in the elastic buffer before it gets released on the LEMC edge. Must be greater than 64. Its max value is KxF octets. Where LEMC period = KxF/8 link clock periods.

0xc2 + 0x8*n 0x308 + 0x20*n LANEn_ERROR_STATISTICS

Where n is from 0 to 31.

[31:0] ERROR_REGISTER RO 0x00000000

This register shows the number of total errors for this lane. Errors counted depend on the configuration in LINK_CONF3. It must always be manually reset.

0xc3 + 0x8*n 0x30c + 0x20*n LANEn_LANE_FRAME_ALIGN_ERR_CNT

Where n is from 0 to 31.

[7:0] ERROR_REGISTER RO 0x00

This register shows the number of frame alignment errors for this lane. It resets with a link restart.

0xc4 + 0x8*n 0x310 + 0x20*n LANEn_ILAS0

Received ILAS config data for the n-th lane. Where n is from 0 to 31.

[31:28] RESERVED RO 0x0

[27:24] BID RO 0x0

BID (Bank ID) field of the ILAS config sequence.

[23:16] DID RO 0x00

DID (Device ID) field of the ILAS config sequence.

[15:0] RESERVED RO 0x0000

0xc5 + 0x8*n 0x314 + 0x20*n LANEn_ILAS1

Received ILAS config data for the n-th lane. Where n is from 0 to 31.

[31:29] RESERVED RO 0x0

[28:24] K RO 0x00

K (Frames per multi-frame) field of the ILAS config sequence - 1.

[23:16] F RO 0x00

F (Octets per frame) field of the ILAS config sequence - 1.

[15] SCR RO 0x0

SCR (Scrambling enabled) field of the ILAS config sequence.

[14:13] RESERVED RO 0x0

[12:8] L RO 0x00

L (Number of lanes) field of the ILAS config sequence - 1.

[7:5] RESERVED RO 0x0

[4:0] LID RO 0x00

LID (Lane ID) field of the ILAS config sequence.

0xc6 + 0x8*n 0x318 + 0x20*n LANEn_ILAS2

Received ILAS config data for the n-th lane. Where n is from 0 to 31.

[31:29] JESDV RO 0x0

JESDV (JESD204 version) field of the ILAS config sequence.

[28:24] S RO 0x00

S (Samples per frame) field of the ILAS config sequence - 1.

[23:21] SUBCLASSV RO 0x0

SUBCLASSV (JESD204B subclass) field of the ILAS config sequence.

[20:16] NP RO 0x00

N’ (Total number of bits per sample) field of the ILAS config sequence - 1.

[15:14] CS RO 0x0

CS (Control bits per sample) field of the ILAS config sequence.

[13] RESERVED RO 0x0

[12:8] N RO 0x00

N (Converter resolution) field of the ILAS config sequence - 1.

[7:0] M RO 0x00

M (Number of converters) field of the ILAS config sequence - 1.

0xc7 + 0x8*n 0x31c + 0x20*n LANEn_ILAS3

Received ILAS config data for the n-th lane. Where n is from 0 to 31.

[31:24] FCHK RO 0x00

FCHK (Checksum) field of the ILAS config sequence.

[23:8] RESERVED RO 0x0000

[7] HD RO 0x0

HD (High-density) field of the ILAS config sequence.

[6:5] RESERVED RO 0x0

[4:0] CF RO 0x00

CF (control words per frame) field of the ILAS config sequence

Theory of Operation

The JESD204B/C receive peripheral consists of two main components: the register map and the link processor.

Both components are fully asynchronous and are clocked by independent clocks. The register map is in the s_axi_aclk clock domain, while the link processor is in the clk and device_clk clock domain.

The register map is used to configure the operational parameters of the link processor as well as to query the current state of the link processor.

The link processor itself is responsible for handling the JESD204 link layer protocol.

Interfaces and Signals

Register Map Configuration Interface

The register map configuration interface can be accessed through the AXI4-Lite S_AXI interface. The interface is synchronous to the s_axi_aclk. The s_axi_aresetn signal is used to reset the peripheral and should be asserted during system startup until the s_axi_aclk is active and stable. De-assertion of the reset signal should be synchronous to s_axi_aclk.

JESD204 Control Signals

The sync and sysref signals correspond to the SYNC~ and SYSREF signals of the JESD204 specification.

The sync signal is asserted by the peripheral during link initialization and must be connected to the corresponding JESD204 ADC converter devices on the same link.

The sysref signal is generated externally and is optional. It is only required to achieve deterministic latency in subclass 1 mode operation. If the sysref signal is not connected software needs to configure the peripheral accordingly to indicate this.

When the sysref signal is used, in order to ensure correct operation, it is important that setup and hold of the external signal relative to the device_clk signal are met. Otherwise, deterministic latency cannot be guaranteed.

Transceiver Interface (RX_PHYn)

For each lane, the peripheral has one corresponding RX_PHY interface. These interfaces accept the physical layer data from the downstream physical layer transceiver peripheral.

The physical layer is responsible for clock recovery, character alignment, de-serialization as well an 8b10b decoding.

User Data Interface (RX_DATA)

User data is provided on the AXI4-Stream RX_DATA interface. The interface is a reduced AXI4-Stream interface and only features the TVALID flow control signal, but not the TREADY flow control signal. The behavior of the interface is as if the TREADY signal was always asserted. This means as soon as rx_valid is asserted, a continuous stream of user data must be accepted from rx_data.

../../../_images/wavedrom-1.svg

After reset and during link initialization, the rx_valid signal is deasserted. As soon as the User Data Phase is entered, the rx_valid will be asserted to indicate that the peripheral is now providing the processed data at the rx_data signal. The rx_valid signal stays asserted until the link is either deactivated or reinitialized.

JESD204B/C Rx link layer octets mapping

Typically, the RX_DATA interface is connected to a JESD204 transport layer peripheral that deframes the data and passes it to the application layer. The internal data path width of the peripheral is 4, this means that 4 octets per lane are processed in parallel. When in the user data phase, the peripheral provides 4 octets for each lane in each beat.

This means that RX_DATA interface is DATA_PATH_WIDTH * 8 * NUM_LANES bits wide. With each block of consecutive DATA_PATH_WIDTH * 8 bits corresponding to one lane. The lowest DATA_PATH_WIDTH * 8 bits correspond to the first lane, while the highest DATA_PATH_WIDTH * 8 bits correspond to the last lane.

E.g. for 8B/10B mode where DATA_PATH_WIDTH=4. Each lane specific 32-bit block corresponds to 4 octets each 8 bits wide. The temporal ordering of the octets is from LSB to MSB, this means the octet placed in the lowest 8 bits was received first, the octet placed in the highest 8 bits was received last.

Data corresponding to lanes that have been disabled should be ignored and their value is undefined.

Configuration Interface

The peripheral features a register map configuration interface that can be accessed through the AXI4-Lite S_AXI port. The register map can be used to configure the peripherals operational parameters, query the current status of the device and query the features supported by the device.

Peripheral Identification and HDL Synthesis Settings

The peripheral contains multiple registers that allow the identification of the peripheral as well as the discovery of features that were configured at HDL synthesis time. Apart from the SCRATCH register, all registers in this section are read-only and write access to them will be ignored.

The VERSION (0x000) register contains the version of the peripheral. The version determines the register map layout and general features supported by the peripheral. The version number follows semantic versioning. Increments in the major number indicate backward incompatible changes, increments in the minor number indicate backward compatible changes, patch letter increments indicate bug fix.

The PERIPHERAL_ID (0x004) register contains the value of the ID HDL configuration parameter that was set during synthesis. Its primary function is to allow to distinguish between multiple instances of the peripheral in the same design.

The SCRATCH (0x008) register is a general purpose 32-bit register that can be set to an arbitrary values. Reading the register will yield the value previously written (the value will be cleared when the peripheral is reset). Its content does not affect the operation of the peripheral. It can be used by software to test whether the register map is accessible or store custom peripheral associated data.

The IDENTIFICATION (0x00c) register contains the value of "204R". This value is unique to this type of peripheral and can be used to ensure that the peripheral exists at the expected location in the memory mapped IO register space.

The SYNTH_NUM_LANES (0x010) register contains the value of the NUM_LANES HDL configuration parameter that was set during synthesis. It corresponds to the maximum of lanes supported by the peripheral. Possible values are between 1 and 32.

The SYNTH_DATA_PATH_WIDTH (0x014) register contains the value of the internal data path width per lane in octets. This is how many octets are processed in parallel on each lane and affects the restrictions of possible values for certain runtime configuration registers. The value is encoded as the log2() of the data path width. Possible values are:

  1. Internal data path width is 2;

  2. Internal data path width is 4;

  3. Internal data path width is 8.

The SYNTH_ELASTIC_BUFFER_SIZE (0x040) register describes the maximum amount of octets that the elastic buffer can hold. This puts a limit on the maximum local-multi-frame-clock (LMFC) / local-multiblock-clock (LEMC) period (subclass 1) as well as the maximum skew between individual lanes (subclass 0). Both must be less than the elastic buffer size.

Interrupt Handling

Interrupt processing is handled by 3 closely related registers. All 3 registers follow the same layout, each bit in the register corresponds to one particular interrupt.

When an interrupt event occurs it is recorded in the IRQ_SOURCE (0x088) register. For a recorded interrupt event, the corresponding bit is set to 1. If an interrupt event occurs while the bit is already set to 1, it will stay set to 1.

The IRQ_ENABLE (0x080) register controls how recorded interrupt events propagate. An interrupt is considered to be enabled if the corresponding bit in the IRQ_ENABLE register is set to 1, it is considered to be disabled if the bit is set to 0.

Disabling an interrupt will not prevent it from being recorded, but only its propagation. This means if an interrupt event was previously recorded while the interrupt was disabled and the interrupt is being enabled the interrupt event will then propagate.

An interrupt event that has been recorded and is enabled propagates to the IRQ_PENDING (0x084) register. The corresponding bit for such an interrupt will read as 1. Disabled or interrupts for which no events have been recorded will read as 0. Also if at least one interrupt has been recorded and is enabled the external irq signal will be asserted to signal the IRQ event to the upstream IRQ controller.

A recorded interrupt event can be cleared (or acknowledged) by writing a 1 to the corresponding bit to either the IRQ_SOURCE or IRQ_PENDING register. It is possible to clear multiple interrupt events at the same time by setting multiple bits in a single write operation.

For more details regarding interrupt operation see the interrupts section of this document.

Link Control

The LINK_DISABLE (0x0c0) register is used to control the link state and switch between enabled and disabled. While the link is disabled its state machine will remain in reset and it will not react to any external event like the SYSREFsignal.

Writing a 0 to the LINK_DISABLE register will enable the link. While the link state is changing from disabled to enabled it will go through a short initialization procedure, which will take a few clock cycles. To check whether the initialization procedure has completed and the link is fully operational the LINK_STATE (0x0c4) register can be checked. The LINK_STATE ([0]) bit will contain a 0 when the link is fully enabled and will contain a 1 while it is disabled or going through the initialization procedure.

Writing a 1 to the LINK_DISABLE register will immediately disable the link.

The EXTERNAL_RESET ([1]) bit in the LINK_STATE register indicates whether the external link reset signal is asserted (1) or de-asserted (0). When the external link reset is asserted the link is disabled regardless of the setting of LINK_DISABLE. The external link reset is controlled by the fabric and might be asserted if the link clock is not stable yet.

Multi-link Control

A multi-link is a link where multiple converter devices are connected to a single logic device (FPGA). All links involved in a multi-link are synchronous and established at the same time. For an 8B/10B RX link, this means that the SYNC~ signal needs to be propagated from the FPGA to each converter.

For an 8B/10B link the MULTI_LINK_DISABLE register allows activating or deactivating each SYNC~ lines independently. This is useful when depending on the use case profile some converter devices are supposed to be disabled.

Link Configuration

The link configuration registers control certain aspects of the runtime behavior of the peripheral. Since the JESD204 standard does now allow changes to link configuration while the link is active the link configuration registers can only be modified while the link is disabled. As soon as it is enabled the configuration registers turn read-only and any writes to them will be ignored.

The LANES_DISABLE (0x200) register allows to disable individual lanes. Each bit in the register corresponds to a particular lane and indicates whether that lane is enabled or disabled. Bit 0 corresponds to the first lane, bit 1 to the second lane and so on. A value of 0 for a specific bit means the corresponding lane is enabled, a value of 1 means the lane is disabled. A disabled lane will not receive any data when the link is otherwise active. By default, all lanes are enabled.

The LINK_CONF0 register configures the octets-per-frame and frames-per-multi-frame settings of the link. The OCTETS_PER_FRAME ([18:16]) field should be set to the number of octets-per-frame minus 1 (F - 1). The OCTETS_PER_MULTIFRAME ([7:0]) field should be set to the number of octets-per-frame multiplied by the number of frames-per-multi-frame minus 1 (FxK - 1). For correct operation FxK must be a multiple of 4. In 64B/66B mode this field matches and also represents the number of octets per extended multiblock (Ex32x8 - 1).

The LINK_CONF1 register allows disabling optional link level processing stages. The DESCRAMBLER_DISABLE ([0]) bit controls whether descrambling of the received user data is enabled or disabled. A value of 0 enables descrambling and a value of 1 disables it. In 64B/66B mode descrambling must be always enabled. The CHAR_REPLACEMENT_DISABLE ([1]) bit controls whether alignment character replacement is performed or not. A value of 0 enables character replacement and a value of 1 disables it. If character replacement is disabled and an alignment character is received (/F/ or /A/) a unexpected K-character error is raised.

For correct operation, character replacement must be disabled when descrambling is disabled otherwise undefined behavior might occur.

Both the transmitter as well as receiver device on the JESD204 link need to be configured with the same settings for scrambling/descrambling and character replacement for correct operation.

Character replacement is used only in 8B/10B links and completely disregarded in 64B/66B mode.

The LINK_CONF2 register controls the behavior of elastic buffer. The BUFFER_EARLY_RELEASE ([16]) bit configures when the data is released from the elastic buffer to the RX_DATA port. If the bit is set to 0 the data will be released at the earliest configured release point after all lanes are ready. When the bit is set to 1 the data will be released as soon as all lanes are ready. The former gives deterministic latency and is required for subclass 1 operation, the later gives minimum latency.

The BUFFER_DELAY ([11:0]) field allows to configure the buffer release opportunity point relative to the local-multi frame-clock (LMFC)/ local-multiblock-clock (LEMC). A setting of 0 indicates that the release opportunity is aligned to the LMFC/LEMC edge. A setting of X indicates that it trails the LMFC/LEMC edge by X octets.

../../../_images/wavedrom-2.svg

The BUFFER_DELAY field must be set to a multiple of 4. Writing a value that is not a multiple of 4 will be rounded down to the next multiple of 4. For correct operation, the BUFFER_DELAY field must also be set to a value smaller than the number of octets per multi-frame (FxK).

This mechanism can be used to reduce overall latency while still maintaining deterministic latency if the maximum link latency (overall valid PVT settings) is known.

SYSREF Handling

The external SYSREF signal is used to align the internal local multiframe clocks (LMFC)/ local-multiblock-clock (LEMC) between multiple devices on the same link.

The SYSREF_CONF (0x100) register allows to configure the behavior of the SYSREF capture circuitry. Setting the SYSREF_DISABLE ([0]) bit to 1 disables the SYSREF handling. All external SYSREF events are ignored and the LMFC/LEMC is generated internally. For Subclass 1 operation, SYSREF handling should be enabled and for Subclass 0 operation it should be disabled.

The SYSREF_LMFC_OFFSET (0x104) register allows to modify the offset between the SYSREF rising edge and the rising edge of the LMFC/LEMC.

For optimal operation it is recommended that all device on a JESD204 link should be configured in a way so that the total offset between the value of the SYSREF_LMFC_OFFSET register must be set to a value smaller than the configured number of octets-per-multiframe (OCTETS_PER_MULTIFRAME), otherwise undefined behavior might occur.

The SYSREF_STATUS (0x108) register allows to monitor the status of the SYSREF signals. SYSREF_DETECTED ([0]) bit indicates that the peripheral as observed a SYSREF event. The SYSREF_ALIGNMENT_ERROR ([1]) bit indicates that a SYSREF event has been observed which was unaligned, in regards to the LMFC/LEMC period, to a previously recorded SYSREF event.

All bits in the SYSREF_STATUS register are write-to-clear. All bits will also be cleared when the link is disabled.

Note that the SYSREF_STATUS register will not record any events if SYSREF operation is disabled or the JESD204 link is disabled.

Link Status

All link status registers are read-only. While the link is disabled, some of the link status registers might contain bogus values. Their content should be ignored until the link is fully enabled.

The STATUS_STATE ([1:0]) field of the LINK_STATUS (0x280) register indicates the state of the 8B/10B link state machine or 64B/66B link state machine depending on the selected decoder.

Possible values for a 8B/10B link are:

  • RESET (0x0): The link is currently disabled;

  • WAIT FOR PHY (0x1): The controller waits for the PHY level component to be ready;

  • CGS (0x2): The controller is waiting for one or more lanes to complete the CGS phase;

  • DATA (0x3): All lanes are in the data phase and the link is properly established.

Possible values for a 64B/66B link are:

  • RESET (0x0): The link is currently disabled;

  • WAIT BLOCK SYNC (0x1): The controller waits for all enabled lanes to reach sync header alignment;

  • BLOCK SYNC (0x2): All enabled lanes from the PHY reached sync header alignment phase;

  • DATA (0x3): All enabled lanes reached the multi-block synchronization phase, elastic buffer released the data and the link is properly established.

The state of each individual lane can be queried from the lane status registers.

Lane Status

Each lane has a independent status register (LANEn_STATUS (0x300)) that indicates the current state of the lane.

8B/10B Link Lane Status Fields

The CGS_STATE ([1:0]) indicates the current state of the lane code group synchronization:

  • INIT (0x0): Lane is not synchronized;

  • CHECK (0x1): Lane is in the process of synchronizing, at least some /K/ synchronization characters have been observed;

  • DATA (0x2): Lane is synchronized and ready to receive data.

The IFS_READY ([4]) bit indicates that initial frame synchronization has completed for the lane and the lane is receiving either ILAS data or user data.

The LANEn_LATENCY (0x304) register holds the duration in octets between when the SYNC~ signal was de-asserted and when the frame synchronization for this particular lane has completed. The LANEn_LATENCY register only holds valid data if the IFS_READY bit of the LANEn_STATUS register is set.

64B/66B Link Lane Status Fields

The EMB_STATE ([10:8]) indicates the current state of the Extended Multi-Block alignment state machine:

  • EMB_INIT (3’b001): Wait for sync header alignment and for an end of extended multiblock (EoEMB) indicator;

  • EMB_HUNT (3’b010): Keep track and monitor consecutive EoEMBs until a threshold is reached;

  • EMB_LOCK (3’b100): Asserted by receiver to indicate that extended multiblock alignment has been achieved.

8B/10B Link ILAS Configuration Data

If the JESD204 transmitter emits an initial lane alignment sequence (ILAS) the configuration data embedded in the second multi-frame of the ILA sequence is captured by the peripheral and stored in a set of four per-lane registers (LANEn_ILAS0, LANEn_ILAS1, LANEn_ILAS2 and LANEn_ILAS3). ILAS_READY ([5]) bit in the corresponding LANEn_STATUS register indicates whether the ILAS configuration data has been captured for a specific lane. The data in the LANEn_ILASx registers is only valid when that bit is asserted.

The received ILAS configuration data can be used to verify that the transmitter device is using the expected configuration and that the lane and device mapping is correct.

Clock Monitor

The LINK_CLK_FREQ (0x0c8) register allows to determine the clock rate of the link clock (clk) relative to the AXI interface clock (s_axi_aclk). This can be used to verify that the link clock is running at the expected rate.

The DEVICE_CLK_FREQ (0x0cc) register allows to determine the clock rate of the device clock (device_clk) relative to the AXI interface clock (s_axi_aclk). This can be used to verify that the device clock is running at the expected rate.

The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock, this corresponds to a resolution of 1.523kHz per LSB. A raw value of 0 indicates that the link clock is currently not active.

Interrupts

The core does not generate interrupts.

8B/10B Link

../../../_images/axi_jesd204_rx_204c_8b10b.svg

8B/10B Link State Machine

../../../_images/jesd204_rx_state_machine.svg

The peripheral can be in one of four main operating phases: RESET, WAIT FOR PHY, CGS, or DATA. Upon reset the peripheral starts in the RESET phase. The WAIT FOR PHY and CGS phases are used during the initialization of the JESD204 link. The DATA phase is used during normal operation when user data is received across the JESD204 link.

RESET phase

The RESET phase is the default state entered during reset. While disabled the peripheral will stay in the RESET phase. When enabled, the peripheral will transition from the RESET phase to the WAIT FOR PHY phase.

If at any point the peripheral is disabled, it will automatically transition back to the RESET state.

Lanes that have been disabled in the register map configuration interface, will behave as if the link was in the RESET state regardless of the actual state.

WAIT FOR PHY phase

During the WAIT FOR PHY phase the peripheral will wait for all PHY controllers for all enabled lanes to be ready for operation. Once this condition is satisfied the controlled will transition to the CGS phase.

CGS phase

During the CGS phase the peripheral will assert the external ~SYNC signal and expects the connected JESD204 transmitter to send /K/ characters.

Each lane will independently the incoming data stream for /K/ characters and adjust its state machine according to the received characters.

Once all enabled lanes have entered the DATA state the link state will transition from the CGS phase to the DATA phase.

DATA phase

The DATA phase is the main operating mode of the peripheral. In this phase it will transmit transport layer data at the RX_DATA port. When the peripheral enters the DATA phase the valid signal of the RX_DATA interface will be asserted to indicate that transport layer data is now available.

By default the data received on each lane is descrambled. Descrambling can optionally be disabled via the register map configuration interface. Descrambling is enabled or disabled for all lanes equally.

Scrambling reduces data-dependent effects, which can affect both the analog performance of the data converter as well as the bit-error rate of JESD204 serial link, therefore it is highly recommended to enable scrambling for the link.

The peripheral also performs per-lane alignment character monitoring. When alignment character replacement is enabled the JESD204 transmitter replaces under certain predictable conditions (i.e. the receiver can recover the replaced character) the last octet in a frame or multi-frame. Replaced characters at the end of a frame, that is also the end of a multi-frame, are replaced by the /A/ character. Replaced characters at the end of a frame, that is not the end of a multi-frame, are replaced by the /F/ character. If a alignment character is received the peripheral checks that the it is in the expected position, either the end of a frame or the end of a multi-frame, and reports an error if a lane has become misaligned. This allows to detect alignment errors and allows the application to re-initialize the link.

Alignment character monitoring can optionally be disabled via the register map configuration interface. Alignment character monitoring is enabled or disabled for all lanes equally. If alignment character monitoring is disabled, no errors are reported when a misaligned alignment character is received.

Data on the RX_DATA port corresponding to a disabled lanes are undefined and should be ignored.

8B/10B Multi-endpoint RX link establishment

In a multi-endpoint configuration one link receive peripheral connects to several endpoints/converter devices. In such cases the link is established only when all enabled endpoints reach the DATA phase. For that all endpoints must pass through CGS and ILAS stages.

Depending on the software implementation that controls the converter devices the endpoints can be enabled at different moments. The link receive peripheral will receive the CGS characters and do character alignment until for all enabled endpoints lanes succeeds that and signalize that through the de-assertion of SYNC~ signal.

In the below example we have a multi-point link of four endpoints (NUM_LINKS = 4):

../../../_images/quadmxfe_linkbringup_204b_adc.svg

Note

The physical layer is not depicted on purpose. JTXn represents the link layer counterpart in the converter device/endpoint n

The steps of the link bring-up are presented below:

  • 1 - Link receive peripheral is enabled, will assert its SYNC~ signal to indicate to the endpoints it is ready to receive and align to the CGS characters. All SYNC~ signal to all enabled endpoints assert in the same time;

  • 2,3,4,5 - JESD transmit block of DAC enabled, will start sending CGS characters until its SYNC~ pin is not pulled low. The timing depends on the software implementation that controls the DAC;

  • 6 - In Subclass 1 (SC1) SYSREF is captured and LMFC in the FPGA and converter device is adjusted;

  • 7 - Once the CGS characters are received correctly on all enabled lanes, on the next Frame clock boundary in SC0 or LMFC boundary in SC1 the SYNC~ is de-asserted. All SYNC~ signal to all enabled endpoints de-assert in the same time. In SC1 if SYSREF is not captured the link receive peripheral will stay in CGS state and will keep SYNC~ asserted.;

  • 8 - Once all enabled endpoints (not masked by MULTI_LINK_DISABLE) observe the de-assert of the SYNC~ signal, on the next Frame clock boundary for SC0 or the next LMFC boundary for SC1, will start sending the ILAS sequence, then after typically 4 LMFC periods later the actual DATA.

64B/66B Link

The 64-bit wide datapath of the link layer is fairly simple, the data received from the PHY is sent through a mandatory descrambler block to an elastic buffer that serves as an aligner cross lanes. Each beat of the datapath contains a block of data of 8 octets.

For each lane the control path starts from the 2-bit sync header connected to the header decoder that tracks and monitors multiblock and extended multiblock markers from the stream, reconstructs the 32-bit sync word corresponding to every multiblock and extracts the received CRC from it. The CRC is calculated for every multiblock and is compared against the received CRC. The mismatches are recorded by the error monitor block.

Beside the CRC errors the error monitor records invalid end of multiblock, end of extended multiblock and invalid sync header errors. The source of every error can be masked from the corresponding bit of the LINK_CONF3 register.

../../../_images/axi_jesd204_rx_204c_64b66b.svg

64B/66B Link State Machine

The peripheral can be in one of four main operating phases: RESET, WAIT BS, BLOCK SYNC, or DATA. Upon reset the peripheral starts in the RESET phase. The WAIT BS and BLOCK SYNC phases are used during the initialization of the JESD204 link. The DATA phase is used during normal operation when user data is received across the JESD204 link.

../../../_images/jesd204c_rx_state_machine.svg

RESET phase

The RESET phase is the default state entered during reset. While disabled the peripheral will stay in the RESET phase. When enabled the peripheral will transition from the RESET phase to the WAIT FOR PHY phase.

If at any point the peripheral is disabled it will automatically transition back to the RESET state.

WAIT BS phase

During the WAIT BS phase the peripheral will wait for all PHY controllers for all enabled lanes to reach sync header alignment state ensuring the sync header stream separation from the data blocks. Once this condition is satisfied the controlled will transition to the BLOCK SYNC phase.

If one of the enabled lanes loses the the sync header alignment the link will fall back to WAIT BS state.

BLOCK SYNC phase

The BLOCK SYNC state ensures all enabled lanes achieved sync header alignment or block synchronization phase in other terms. During this state the peripheral will wait for all enabled lanes to reach extended multiblock alignment and the elastic buffer get released. Once each enabled lane is extended multiblock aligned for each lane the data blocks are stored in the elastic buffer then are released at a well defined moment relative to the SYSREF signal.

DATA phase

The DATA phase is the main operating mode of the peripheral. In this phase it will transmit transport layer data at the RX_DATA port. When the peripheral enters the DATA phase the valid signal of the RX_DATA interface will be asserted to indicate that transport layer data is now available.

64B/66B Link Extended MultiBlock Alignment State Machine

For each lane a state machine is used to detect the boundary of the extended multiblocks by tracking well defined markers in the sync header stream. Once the boundary is detected for each lane the corresponding data stream can be aligned across all enabled lanes. This is done through the elastic buffer.

../../../_images/jesd204c_rx_emb_state_machine.svg

EMB INIT State

The EMB INIT is the default state of the state machine, all disabled lanes stay in this state. The state is left only when the lane is enabled, the PHY controller of the corresponding lane is sync header aligned and a valid end of extended multiblock marker is detected in the sync header stream.

At any moment the PHY loses sync header alignment the state machine will fall back to the EMB INIT state.

EMB HUNT State

In the EMB HUNT state the state machine will look after four consecutive correct extended multiblock indicators, once this is achieved the state machine enters the EMB LOCK state. In case invalid end of multiblock or end of extended multiblock markers are detected the state machine falls back to the EMB INIT state.

EMB LOCK State

In the EMB LOCK state the monitoring of multiblock and extended multiblock indicators is continued. In case of eight consecutive indicators are incorrect the state machine will return in the EMB INIT state. This state ensures the validity of the 32-bit sync words constructed from the sync header stream. For each multiblock the calculated CRC of the previous multiblock is extracted from the current sync word.

Dual clock operation

In case ASYNC_CLK parameter is set, a gearbox with 4:N (204B) or 8:N (204C) ratio is enabled in the link layer peripherals, where N depends on the F parameter of the link. The goal of the gearbox is to have at the transport layer interface a data width that contains an integer number of frames per every device clock cycle (each beat) so an integer number of samples can be delivered/consumed to/from the application layer aligned to SYSREF ensuring deterministic latency in modes where N’=12 or F!=1,2,4.

../../../_images/dual_clock_operation.svg

The gearbox ratio corresponds with the ratio of the link layer interface data width towards physical layer and transport layer in octets. The interface width towards the physical layer in 8B/10B (204B) mode depends on the DATA_PATH_WIDTH synthesis parameter, and can be either 4 octets (default) or 8 octets. In 204B mode the util_adxcvr supports only data width of 4 octets. In 64b66b (aka 204C) mode the data width towards the physical interface is always 8 octets.

The data path width towards the transport layer is defined by the TPL_DATA_PATH_WIDTH synthesis parameter.

The following rules apply:

  • TPL_DATA_PATH_WIDTH >= DATA_PATH_WIDTH;

  • TPL_DATA_PATH_WIDTH = m x F; where m is a positive integer, power of 2.

The link clock and device clock ratio should be the inverse of the DATA_PATH_WIDTH : TPL_DATA_PATH_WIDTH ratio.

In this context the link clock will be lane rate/40 or lane rate/80 for 204B depending on DATA_PATH_WIDTH and lane rate/66 for 204C 64B/66B, however the device clock could vary based in the F parameter.

64b/66b Link latency reduction

Deterministic latency can be reduced by adjusting the release point of the elastic buffer in RX link layer. By default the release point of the elastic buffer is at the edge of LEMC. In case of 64b66b link the LATENCY register will indicate how many octets will the elastic buffer store before the default release point for that specific lane. The release point can be adjusted to bring it closer to the last arrival lane (that will have the least octets in the buffer) so minimizing the buffer usage and the latency in turn. The LATENCY must be measured over multiple power-ups and bring-up sequence. Identify the slowest arrival lane (min value of the register). If multiple parallel links must be synchronized all lanes from all links must be included in the process.

Once the slowest lane delay is identified, before enabling the links, SW needs to set the register BUFFER_DELAY (0x240) from all parallel Rx links if exists based on the following formula:

\[Buffer Delay = \frac{(F*K - min(LatencyRegs) + 32)}{TPLDW} + 4\]

Where:

  • Buffer Delay - register 0x240 of the core;

  • F*K - is the size of a multiframe in octets;

  • LatencyRegs - is the measured latency of each lane observed during consecutive link bring-ups measured for all Rx links, see regs (0x304 + n*0x20) where n = 0..L-1 ; L is number of lanes;

  • TPLDW - TPL datapath width in octets. Can be read from the SYNTH_DATA_PATH_WIDTH (0x14) reg TPL_DATA_PATH_WIDTH field.

This value it the absolute minimum. It is recommended to increase it slightly to have a better margin against power-up to power-up latency variations.

Software Support

Warning

To ensure correct operation it is highly recommended to use the Analog Devices provided JESD204 software packages for interfacing the peripheral. Analog Devices is not able to provide support in case issues arise from using custom low-level software for interfacing the peripheral.

  • JESD204 Receive Linux Driver Support

Restrictions

During the design of the peripheral, the deliberate decision was made to support only a subset of the features mandated by the JESD204 standard for receiver logic devices.

The reasoning here is that the peripheral has been designed to interface to Analog Devices JESD204 ADC converter devices and features that are either not required or not supported by those converter devices would otherwise lie dormant in peripheral and never be used.

Instead, the decision was made to not implement those unneeded features, even when the JESD204 standard requires them for general purpose JESD204 receiver logic devices. As Analog Devices ADC converter devices with new requirements are released the peripheral will be adjusted accordingly.

This approach allows for a leaner design using less resources, allowing for lower pipeline latency and a higher maximum device clock frequency.

The following lists where the peripheral deviates from the standard:

  • No subclass 2 support. JESD204 subclass 2 has, due to its implementation details, restricted applicability and is seldom a viable option for a modern high-speed data converter system. To achieve deterministic latency, it is recommend to use subclass 1 mode;

  • Reduced number of octets-per-frame settings. The JESD204 standard allows for any value between 1 and 256 to be used for the number of octets-per-frame;

  • The following octets-per-frame are supported by the peripheral: 1, 2, 4 and 1. (No longer applies starting from 1.07.a);

  • Reduced number of frames-per-multi-frame settings. The following values are supported by the peripheral: 1-32, with the additional requirement that F*K is a multiple of 4. In addition F*K needs to be in the range of 4-256;

  • No support for alignment character replacement when scrambling is disabled. (No longer applies starting from 1.07.a).

Additional Information

  • JESD204 Glossary

Supported Devices

JESD204B Analog-to-Digital Converters

  • AD6673: 80 MHz Bandwidth, Dual IF Receiver

  • AD6674: 385 MHz BW IF Diversity Receiver

  • AD6676: Wideband IF Receiver Subsystem

  • AD6677: 80 MHz Bandwidth, IF Receiver

  • AD6684: 135 MHz Quad IF Receiver

  • AD6688: RF Diversity and 1.2GHz BW Observation Receiver

  • AD9207: 12-Bit, 6 GSPS, JESD204B/JESD204C Dual Analog-to-Digital Converter

  • AD9208: 14-Bit, 3GSPS, JESD204B, Dual Analog-to-Digital Converter

  • AD9209: 12-Bit, 4GSPS, JESD204B/C, Quad Analog-to-Digital Converter

  • AD9213: 12-Bit, 10.25 GSPS, JESD204B, RF Analog-to-Digital Converter

  • AD9234: 12-Bit, 1 GSPS/500 MSPS JESD204B, Dual Analog-to-Digital Converter

  • AD9250: 14-Bit, 170 MSPS/250 MSPS, JESD204B, Dual Analog-to-Digital Converter

  • AD9625: 12-Bit, 2.6 GSPS/2.5 GSPS/2.0 GSPS, 1.3 V/2.5 V Analog-to-Digital Converter

  • AD9656: Quad, 16-Bit, 125 MSPS JESD204B 1.8 V Analog-to-Digital Converter

  • AD9680: 14-Bit, 1.25 GSPS/1 GSPS/820 MSPS/500 MSPS JESD204B, Dual Analog-to-Digital Converter

  • AD9683: 14-Bit, 170 MSPS/250 MSPS, JESD204B, Analog-to-Digital Converter

  • AD9690: 14-Bit, 500 MSPS / 1 GSPS JESD204B, Analog-to-Digital Converter

  • AD9691: 14-Bit, 1.25 GSPS JESD204B, Dual Analog-to-Digital Converter

  • AD9694: 14-Bit, 500 MSPS JESD204B, Quad Analog-to-Digital Converter

  • AD9695: 14-Bit, 1300 MSPS/625 MSPS, JESD204B, Dual Analog-to-Digital Converter Analog-to-Digital Converter

  • AD9083: 16-Channel, 125 MHz Bandwidth, JESD204B Analog-to-Digital Converter

  • AD9094: 8-Bit, 1 GSPS, JESD204B, Quad Analog-to-Digital Converter

JESD204B RF Transceivers

  • AD9371: SDR Integrated, Dual RF Transceiver with Observation Path

  • AD9375: SDR Integrated, Dual RF Transceiver with Observation Path and DPD

  • ADRV9009: SDR Integrated, Dual RF Transceiver with Observation Path

  • ADRV9008-1: SDR Integrated, Dual RF Receiver

  • ADRV9008-2: SDR Integrated, Dual RF Transmitter with Observation Path

JESD204B/C Mixed-Signal Front Ends

  • AD9081: MxFE Quad, 16-Bit, 12GSPS RFDAC and Quad, 12-Bit, 4GSPS RFADC

  • AD9082: MxFE QUAD, 16-Bit, 12GSPS RFDAC and DUAL, 12-Bit, 6GSPS RFADC

  • AD9986: 4T2R Direct RF Transmitter and Observation Receiver

  • AD9988: 4T4R Direct RF Receiver and Transmitter

Technical Support

Analog Devices will provide limited online support for anyone using the core with Analog Devices components (ADC, DAC, Clock, etc) via the EngineerZone under the GPL license. If you would like deterministic support when using this core with an ADI component, please investigate a commercial license. Using a non-ADI JESD204 device with this core is possible under the GPL, but Analog Devices will not help with issues you may encounter.

More Information

  • JESD204 High-Speed Serial Interface Support

  • HDL User Guide

  JESD204B/C Link Transmit Peripheral ADC JESD204B/C Transport Peripheral
©2023-2025, Analog Devices, Inc. | Made with Sphinx & Doctools