Skip to content

GDB Toolbox reference

Each GDB Toolbox script is defined in a JSON file. The following GDB Toolbox script includes numbered fields that are described in the table below:

{
  "name": "Analyze Faults",                                  // ①
  "description": "Analyzes faults and exceptions...",        // ②
  "core": "arm",                                              // ③
  "firmwarePlatform": "zephyr",                               // ④
  "soc": "MAX32690",                                          // ⑤
  "commands": [                                               // ⑥
    {
      "command": "source {defaultScriptsDirectory}/fault-analyzer-arm.gdb", // ⑫
      "actions": [                                            // ⑬
        {
          "type": "appendFile",                               // ⑭
          "filePath": "gdb_toolbox/reports/${input:filename}.md", // ⑮
          "content": "${markdownReport}"
        }
      ]
    }
  ],
  "inputs": [                                                 // ⑦
    {
      "id": "filename",                                       // ⑧
      "type": "inputBox",                                     // ⑨
      "title": "Log Filename",                                // ⑩
      "prompt": "Enter a name for the log file"               // ⑪
    }
  ]
}
# Field Type Description Required
1 name string The display name of the script as shown in the GDB Toolbox UI. ✅ Yes
2 description string A short description of the script. Appears in the Toolbox UI tooltip. ✅ Yes
3 core array Specifies the supported core type, for example: arm, riscv. Filters visibility during debug sessions. ❌ No
4 firmwarePlatform string Filters script visibility by platform. For example: zephyr, msdk. ❌ No
5 soc string Filters script visibility by SoC name. For example: MAX32690. ❌ No
6 commands array A list of GDB commands to run when the script is executed. ✅ Yes
7 inputs array A list of user input prompts. ❌ No

Fields inside each inputs object

# Field Type Description Required
8 id string Unique identifier for the prompt, referenced as ${input:<id>} in the commands[] and actions[] sections. ✅ Yes
9 type string The type of input prompt: inputBox for text entry or quickPick for predefined choices. ✅ Yes
10 title string The title of the input prompt displayed in the UI. ❌ No
11 prompt string The message displayed to the user, asking for input. ❌ No
- choices array A list of predefined choices for quickPick inputs, such as ["A", "B", "C"]. ✅ Yes

Fields inside each commands object

# Field Type Description Required
12 command string The GDB command to execute. Supports variables like ${input} or ${gdbOutput}. See Variables for details. ✅ Yes
13 actions array A list of actions to run after the command. ❌ No

Fields inside each actions object

# Field Type Description Required
14 type string The type of action to perform, such as: log, writeFile, appendFile, showMessage. See Action types for details. ✅ Yes
15 (varies) varies Additional fields required depend on the type. ✅ Yes

Action types

Each action must include a type, followed by additional fields that depend on the action type.

{
  "type": "appendFile",
  "filePath": "gdb_toolbox/reports/fault_analyzer.md",
  "content": "${markdownReport}"
}

The table below lists supported action types and their associated fields:

Type Example fields Description Example
appendFile filePath, content Appends output to an existing file in the project directory. View
conditional condition, then, else Runs actions conditionally using a Jexl expression. The expression can refer to variables defined earlier in the script using setVariable. If the condition evaluates to true, the then actions run; otherwise, the else actions run (if provided). View
log message Writes a message to the Debug Console. View
openDisassembly1 Opens the disassembly view at the current program counter (PC) address for the selected core. Useful for low-level inspection during a paused debug session.1 View
openFile filePath, lineNumber Opens a file in the editor. If lineNumber is provided, the editor scrolls to that line. lineNumber must be a number. View
setVariable name, regex Extracts a value from the GDB response using a regex with a capturing group. Only the first capturing group is stored. View
showMessage message, level Displays a pop-up message in the UI. level must be one of info, warning, or error. Defaults to info if not provided. View
writeFile filePath, content Writes output to a file in the project directory. View

Variables

GDB Toolbox scripts support variables to make commands and actions dynamic. You can prompt users for input, reuse extracted values, or insert built-in values like timestamps.

For example, this script prompts the user for a command, then writes the GDB output to a timestamped log file:

{
  "name": "Run GDB Command and Save Output",
  "description": "Lets you choose a GDB command and saves the output to a log file.",
  "commands": [
    {
      "command": "${input:command}",
      "actions": [
        {
          "type": "writeFile",
          "filePath": "logs/output_${timestamp}.log",
          "content": "${gdbOutput}"
        }
      ]
    }
  ],
  "inputs": [
    {
      "id": "command",
      "type": "quickPick",
      "title": "Select a Command",
      "prompt": "Choose a command to run:",
      "choices": ["info registers", "info threads", "bt"]
    }
  ]
}

The table below lists supported variables and how they can be used:

Variable Description Supported fields
${gdbOutput} Captures the output of the GDB command in the current commands section. content, message
${input} Prompts the user to enter a value. command, filePath, content
${input:<id>} Prompts the user for input by referencing the id defined in the inputs[] section. command, filePath, content
${markdownReport} Inserts a preformatted Markdown version of GDB output. See Example content
${<name>}2 Variable set by setVariable. See Example filePath, content, message, condition
${timestamp} Inserts current ISO 8601 timestamp. filePath, content

  1. Due to a limitation in the Cortex-Debug extension, the openDisassembly action cannot currently navigate to a user-defined address. ↩↩

  2. Use ${<name>} after defining it with a setVariable action. For example, if you use "name": "pc_value", reference it later as ${pc_value}. Only the first capturing group from the regex is stored. ↩