Skip to content

About the GDB Toolbox

The GDB Toolbox provides access to both default and user-defined JSON-based scripts that help inspect program state during a halted debug session. These scripts run GDB commands and capture their output, making it easy to automate debugging tasks. You can create and manage custom scripts using templates or by copying and extending default scripts to enhance functionality.

The Toolbox works with MSDK, SHARC-FX, and Zephyr projects, and supports both single-core and multi-core debug sessions.

Tip

For information on other debugging tools such as breakpoints, watch, and call stack, see Debug an application.

GDB Toolbox scripts

When you create a CFS workspace, the gdb_toolbox folder is automatically added to the .cfs directory within the workspace.

GDB Toolbox GDB Toolbox

This folder contains the scripts used by the GDB Toolbox and includes the Configs and GDB subdirectories.

Configs directory

The configs directory contains the default GDB Toolbox JSON scripts that define which GDB commands to run.

The following default scripts are added to your workspace when it's created and cover common tasks such as dumping memory, analyzing stack usage, or detecting system faults:

Script name Description Supported cores Supported firmware platform1
Analyze Crash Analyzes a crash and generates a JSON report of faulting threads. Core agnostic Zephyr
Analyze Faults Analyzes system faults and exceptions such as hard faults or bus errors. Reads and decodes fault status registers, and prints a fault summary. ARM MSDK, Zephyr
Analyze Global Heap Analyzes heap usage and prints a JSON report showing total heap size (total), currently used memory (used), and the peak memory usage (max). Core agnostic Zephyr
Analyze Stack Performs a detailed analysis of stack usage. Traverses stack frames, prints local variables and arguments, and calculates used and remaining stack space. Core agnostic MSDK
Analyze Stack High-water Mark Analyzes the maximum stack depth reached during runtime using a known fill pattern. Requires the stack painter to be run beforehand. Core agnostic MSDK
Dump Memory Dumps the current memory state to a log file. Core agnostic MSDK, Zephyr, SHARC-FX
Dump Registers Dumps the current register state to a log file. Core agnostic MSDK, Zephyr, SHARC-FX
Interrupt Status Analyzes IRQ and system handlers by reading the NVIC state to identify enabled, active, and pending interrupts, and their associated handlers. ARM MSDK
Paint Stack Fills the stack with a known pattern (0xDEADBEEF) to enable runtime analysis of maximum stack usage. Must be run before the High-water Mark script. Core agnostic MSDK
Thread Analyzer Analyzes all active threads and extracts each thread’s stack usage, register state, and call trace. Core agnostic Zephyr

GDB directory

The gdb directory stores optional GDB scripts that are referenced by the JSON scripts.

GDB scripts (.gdb files) are plain text files that contain either raw GDB commands or Python code using the GDB Python API. Most scripts in this directory use native GDB commands, but advanced scripts such as Thread Analyzer leverage Python for intelligent analysis. These scripts are referenced in Toolbox JSON configs.

For example, the Thread Analyzer Toolbox script includes a source field that points to a thread-analyzer.gdb GDB script in the gdb directory:

{
  "name": "Analyze Threads",
  "description": "Analyzes threads in the target application.",
  "commands": [
    {
      "command": "source {defaultScriptsDirectory}/thread-analyzer.gdb",
      "actions": [{}]
    }
  ]
}

For an introduction to GDB scripting, refer to the GDB manual – Command Files and User-defined Commands.

For advanced scripting using Python, refer to the GDB Python API documentation.


  1. Only compatible scripts are shown during a debug session. This context-awareness ensures you only run scripts that are supported by the active project. ↩