Skip to content

GDB Commands

Use the following commands to interact with the GNU Debugger (GDB) and debug your program. Many of the commands have shortcuts that can be used to save time and keystrokes.

Command Shortcut Description
ctrl+c N/A Halt the current program execution
continue c Resume execution
step s Step into the function
step [value] s 10 Step the next 10 source lines
next n Run the next line in the function (step over)
next [value] n 10 Run the next 10 lines in current function
until [value] u 20 Run until line 20 of the current file
finish f Run to the end of the function or stack frame

Breakpoints

Command Shortcut Description
break main b main Break on main () entry
break on function b main.c:func Break on function () in main.c
break on line b main.c:18 Break on line 18 of main.c
break on condition b main.c:18 if foo > 20 Break if foo > 20 (boolean condition)
break and delete tbreak main Fire once and deletes itself
info breakpoints N/A Lists all breakpoints
ignore 2 20 N/A Ignore breakpoint 21 for the first 20 times
disable 2 N/A Disable breakpoint 21
delete 2 N/A Delete breakpoint 21

Watchpoints

Command Description
watch foo Watch foo
watch myarray[10].val Watch .val in myarray[10]
watch *0x1000FEFE Watch memory addr 0x1000FEFE
watch foo if foo > 20 Conditional watch (foo >20)
watch foo if foo + x > 20 Complex conditional expression
info watchpoints Lists all watchpoints
delete 2 Delete watchpoint 21

Stack Backtrace

Command Shortcut Description
backtrace bt Display a stack backtrace (function call history)
frame Display the current stack frame
up Move up the stack
down Move down the stack

Info

Command Description
info locals List all local variables
info variables List all global variables
info args List all function arguments
info registers List all registers
info breakpoints List all breakpoints
info watchpoints List all watchpoints

Print

Command Shortcut Description
print p Print the value of a variable or expression
print variable p foo Print the value of foo
print multiple p foo+bar Print the complex expression of foo plus bar
print/hex () p/x &main Print the address of main()
print/hex () p/x $r4 Print the value of register r4 in hex
print array () p/a (uint32_t[8])0x1234 Print the array of 8 u32s at address 0x1234

Variables

Variable Description
a Address
b Byte, 1B
c Character
d Decimal point
f Float
g Giant, 8B
h Halfworld, 2B
i Instruction
o Octal integer
s String
t Binary integer
u Unsigned decimal int
w Word, 4B
x Hex integer
z Padded hex

Examine

FMT is a repeat count, followed by a format and size letter.

Command Shortcut Description
examine/[FMT] x Examine the count in format and size
examine variable x foo Show address of variabe foo
examine () x/4c 0x581F Show four characters at address 0x581F
examine () x/4xw &main Show four words in hex at main()

examine source code

Command Description
list Show scr for the current location
list *0x1234 Show source for address 0x1234
list main.C:func Show source for func() from main.C
disas func List ASM code for func()
find /b 0x0, 0x10000, 'H', 'e', 'l', 'l', 'o' 0x581f search for a byte pattern between 0x0 to 0x10000
x/s 0x581f Examine string at address 0x581f

Find

Command Description
find Scan a specific address range for a pattern or known value

Multiple image support

Command Description
add-symbol-file Adds new ELF file into the same GDB session

  1. Breakpoint and watchpoint numbers can be determined by viewing the $bpnum variable immediately after creation. ↩↩↩↩