no-OS
Loading...
Searching...
No Matches
axi_jesd204_rx Struct Reference

#include <axi_jesd204_rx.h>

Public Attributes

const char * name
 
uint32_t base
 
uint32_t version
 
uint32_t num_lanes
 
uint32_t data_path_width
 
uint32_t tpl_data_path_width
 
struct jesd204_rx_config config
 
uint32_t device_clk_khz
 
uint32_t lane_clk_khz
 
enum jesd204_encoder encoder
 
struct no_os_clk_desc * lane_clk
 
struct axi_clkgen * device_clkgen
 
struct jesd204_dev * jdev
 
struct no_os_gpio_desc * gt_reset_pll
 
struct no_os_gpio_desc * gt_reset_dp
 
struct no_os_gpio_desc * gt_reset_done
 

Member Data Documentation

◆ base

uint32_t axi_jesd204_rx::base

Base address

◆ config

struct jesd204_rx_config axi_jesd204_rx::config

Rx coniguration

◆ data_path_width

uint32_t axi_jesd204_rx::data_path_width

Data path width

◆ device_clk_khz

uint32_t axi_jesd204_rx::device_clk_khz

Device Clock in KHz

◆ device_clkgen

struct axi_clkgen* axi_jesd204_rx::device_clkgen

Optional device-clock generator. When set, the link FSM trims it to the per-path device clock (link_rate * data_path_width / tpl_data_path_width), like Linux; NULL leaves it unchanged.

◆ encoder

enum jesd204_encoder axi_jesd204_rx::encoder

Selected Encoder

◆ gt_reset_done

struct no_os_gpio_desc* axi_jesd204_rx::gt_reset_done

◆ gt_reset_dp

struct no_os_gpio_desc* axi_jesd204_rx::gt_reset_dp

◆ gt_reset_pll

struct no_os_gpio_desc* axi_jesd204_rx::gt_reset_pll

Optional GT reset GPIOs (Versal)

◆ jdev

struct jesd204_dev* axi_jesd204_rx::jdev

JESD204 FSM device

◆ lane_clk

struct no_os_clk_desc* axi_jesd204_rx::lane_clk

Lane Clock

◆ lane_clk_khz

uint32_t axi_jesd204_rx::lane_clk_khz

Lane Clock in KHz

◆ name

const char* axi_jesd204_rx::name

Device Name

◆ num_lanes

uint32_t axi_jesd204_rx::num_lanes

◆ tpl_data_path_width

uint32_t axi_jesd204_rx::tpl_data_path_width

TPL data path width

◆ version

uint32_t axi_jesd204_rx::version

Version of the Peripheral


The documentation for this struct was generated from the following file: