no-OS
Loading...
Searching...
No Matches
axi_jesd204_rx.h File Reference

Driver for the Analog Devices AXI-JESD204-RX peripheral. More...

#include <stdint.h>
#include <stdbool.h>
#include "jesd204.h"
#include "no_os_clk.h"
#include "no_os_gpio.h"
Include dependency graph for axi_jesd204_rx.h:

Classes

struct  jesd204_rx_config
 
struct  axi_jesd204_rx
 
struct  jesd204_rx_init
 JESD204B/C Receive Peripheral Initialization Structure. More...
 

Functions

int32_t axi_jesd204_rx_lane_clk_enable (struct axi_jesd204_rx *jesd)
 JESD204 RX Lane Clock Enable.
 
int32_t axi_jesd204_rx_lane_clk_disable (struct axi_jesd204_rx *jesd)
 JESD204 RX Lane Clock Disable.
 
uint32_t axi_jesd204_rx_status_read (struct axi_jesd204_rx *jesd)
 Read status of the JESD204 Receive Peripherial. Prints the link-level status; when JESD204_DUMP_LANE_STATUS is defined it also prints the per-lane info for every lane (Linux "jesd_status" style).
 
int32_t axi_jesd204_rx_laneinfo_read (struct axi_jesd204_rx *jesd, uint32_t lane)
 Read JESD204 RX Lane Info.
 
bool axi_jesd204_rx_check_lane_status (struct axi_jesd204_rx *jesd, uint32_t lane)
 Check JESD204 RX Lane Status.
 
int32_t axi_jesd204_rx_watchdog (struct axi_jesd204_rx *jesd)
 JESD204 RX Watchdog.
 
int32_t axi_jesd204_rx_init_legacy (struct axi_jesd204_rx **jesd204, const struct jesd204_rx_init *init)
 Device initialization.
 
int32_t axi_jesd204_rx_init (struct axi_jesd204_rx **jesd204, const struct jesd204_rx_init *init)
 Device initialization, JESD FSM ON.
 
int32_t axi_jesd204_rx_remove (struct axi_jesd204_rx *jesd)
 Free resoulces allocated for JESD204 RX peripheral.
 

Detailed Description

Driver for the Analog Devices AXI-JESD204-RX peripheral.

Author
DBogdan (drago.nosp@m.s.bo.nosp@m.gdan@.nosp@m.anal.nosp@m.og.co.nosp@m.m)

Copyright 2018(c) Analog Devices, Inc.

SPDX-License-Identifier: BSD-3-Clause

Function Documentation

◆ axi_jesd204_rx_check_lane_status()

bool axi_jesd204_rx_check_lane_status ( struct axi_jesd204_rx * jesd,
uint32_t lane )

Check JESD204 RX Lane Status.

JESD204 RX Lane Status check (true if the lane is desynced)

Parameters
jesd- The device structure.
lane- Lane ID.
Returns
Returns 0 in case of success or positive value otherwise.

◆ axi_jesd204_rx_init()

int32_t axi_jesd204_rx_init ( struct axi_jesd204_rx ** jesd204,
const struct jesd204_rx_init * init )

Device initialization, JESD FSM ON.

Device initialization, JESD FSM ON

Parameters
jesd204- The device structure.
init- The structure containing the device initial parameters.
Returns
Returns 0 in case of success or negative error code otherwise.

◆ axi_jesd204_rx_init_legacy()

int32_t axi_jesd204_rx_init_legacy ( struct axi_jesd204_rx ** jesd204,
const struct jesd204_rx_init * init )

Device initialization.

Device initialization

Parameters
jesd204- The device structure.
init- The structure containing the device initial parameters.
Returns
Returns 0 in case of success or negative error code otherwise.

◆ axi_jesd204_rx_lane_clk_disable()

int32_t axi_jesd204_rx_lane_clk_disable ( struct axi_jesd204_rx * jesd)

JESD204 RX Lane Clock Disable.

JESD204 RX Lane Clock Disable

Parameters
jesd- The device structure.
Returns
Returns 0 in case of success or negative error code otherwise.

◆ axi_jesd204_rx_lane_clk_enable()

int32_t axi_jesd204_rx_lane_clk_enable ( struct axi_jesd204_rx * jesd)

JESD204 RX Lane Clock Enable.

JESD204 RX Lane Clock Enable

Parameters
jesd- The device structure.
Returns
Returns 0 in case of success or negative error code otherwise.

◆ axi_jesd204_rx_laneinfo_read()

int32_t axi_jesd204_rx_laneinfo_read ( struct axi_jesd204_rx * jesd,
uint32_t lane )

Read JESD204 RX Lane Info.

JESD204 RX Lane Info read

Parameters
jesd- The device structure.
lane- Lane ID.
Returns
Returns 0 in case of success or negative error code otherwise.

◆ axi_jesd204_rx_remove()

int32_t axi_jesd204_rx_remove ( struct axi_jesd204_rx * jesd)

Free resoulces allocated for JESD204 RX peripheral.

Resources Deallocation

Parameters
jesd- The device structure.
Returns
Returns 0 in case of success or negative error code.

◆ axi_jesd204_rx_status_read()

uint32_t axi_jesd204_rx_status_read ( struct axi_jesd204_rx * jesd)

Read status of the JESD204 Receive Peripherial. Prints the link-level status; when JESD204_DUMP_LANE_STATUS is defined it also prints the per-lane info for every lane (Linux "jesd_status" style).

JESD204 RX Status Read (link-level status; also per-lane info for every lane when JESD204_DUMP_LANE_STATUS is defined)

Parameters
jesd- The device structure.
Returns
Returns 0 in case of success or negative error code otherwise.

◆ axi_jesd204_rx_watchdog()

int32_t axi_jesd204_rx_watchdog ( struct axi_jesd204_rx * jesd)

JESD204 RX Watchdog.

JESD204 RX Watchdog

Parameters
jesd- The device structure.
Returns
Returns 0 in case of success or positive value otherwise.