no-OS
Loading...
Searching...
No Matches
ad413x_dev Struct Reference

Device structure. More...

#include <ad413x.h>

Public Attributes

struct no_os_spi_desc * spi_dev
 
struct no_os_gpio_desc * rdy_pin_desc
 
struct ad413x_preset preset [8]
 
struct ad413x_channel ch [16]
 
enum ad413x_chip_id chip_id
 
const struct ad413x_chip_info * chip_info
 
enum ad413x_mclk_sel mclk
 
enum ad413x_adc_mode op_mode
 
uint8_t bipolar
 
enum ad413x_int_ref int_ref
 
uint16_t v_bias
 
struct ad413x_standby_ctrl standby_ctrl
 
uint8_t data_stat
 
uint8_t spi_crc_en
 

Detailed Description

Device structure.

Member Data Documentation

◆ bipolar

uint8_t ad413x_dev::bipolar

◆ ch

struct ad413x_channel ad413x_dev::ch[16]

◆ chip_id

enum ad413x_chip_id ad413x_dev::chip_id

◆ chip_info

const struct ad413x_chip_info* ad413x_dev::chip_info

◆ data_stat

uint8_t ad413x_dev::data_stat

◆ int_ref

enum ad413x_int_ref ad413x_dev::int_ref

◆ mclk

enum ad413x_mclk_sel ad413x_dev::mclk

◆ op_mode

enum ad413x_adc_mode ad413x_dev::op_mode

◆ preset

struct ad413x_preset ad413x_dev::preset[8]

◆ rdy_pin_desc

struct no_os_gpio_desc* ad413x_dev::rdy_pin_desc

◆ spi_crc_en

uint8_t ad413x_dev::spi_crc_en

◆ spi_dev

struct no_os_spi_desc* ad413x_dev::spi_dev

◆ standby_ctrl

struct ad413x_standby_ctrl ad413x_dev::standby_ctrl

◆ v_bias

uint16_t ad413x_dev::v_bias

The documentation for this struct was generated from the following file: