no-OS
Loading...
Searching...
No Matches
ad413x.h File Reference

Header file of AD413X Driver. More...

#include <stdint.h>
#include "no_os_delay.h"
#include "no_os_gpio.h"
#include "no_os_spi.h"
#include "no_os_irq.h"
#include "no_os_util.h"
Include dependency graph for ad413x.h:

Classes

struct  ad413x_ref_buf
 ADC reference buffer selection. More...
 
struct  ad413x_chip_info
 Device specific parameters. More...
 
struct  ad413x_standby_ctrl
 Standby control flags. More...
 
struct  ad413x_preset
 Preset setting. More...
 
struct  ad413x_channel
 Channel setting. More...
 
struct  ad413x_dev
 Device structure. More...
 
struct  ad413x_init_param
 Initial parameter structure. More...
 
struct  ad413x_callback_ctx
 Callback structure. More...
 

Macros

#define AD413X_CMD_WR_COM_REG(x)
 
#define AD413X_CMD_RD_COM_REG(x)
 
#define AD413X_R1B   (1 << 8)
 
#define AD413X_R2B   (2 << 8)
 
#define AD413X_R3B   (3 << 8)
 
#define AD413X_TRANSF_LEN(x)
 
#define AD413X_ADDR(x)
 
#define AD413X_REG_STATUS   (AD413X_R1B | 0x0)
 
#define AD413X_REG_ADC_CTRL   (AD413X_R2B | 0x1)
 
#define AD413X_REG_DATA   (AD413X_R3B | 0x2)
 
#define AD413X_REG_IO_CTRL   (AD413X_R2B | 0x3)
 
#define AD413X_REG_VBIAS_CTRL   (AD413X_R2B | 0x4)
 
#define AD413X_REG_ID   (AD413X_R1B | 0x5)
 
#define AD413X_REG_ERROR   (AD413X_R2B | 0x6)
 
#define AD413X_REG_ERROR_EN   (AD413X_R2B | 0x7)
 
#define AD413X_REG_MCLK_CNT   (AD413X_R1B | 0x8)
 
#define AD413X_REG_CHN(x)
 
#define AD413X_REG_CONFIG(x)
 
#define AD413X_REG_FILTER(x)
 
#define AD413X_REG_OFFSET(x)
 
#define AD413X_REG_GAIN(x)
 
#define AD413X_REG_MISC   (AD413X_R2B | 0x39)
 
#define AD413X_REG_FIFO_CTRL   (AD413X_R3B | 0x3A)
 
#define AD413X_REG_FIFO_STS   (AD413X_R1B | 0x3B)
 
#define AD413X_REG_FIFO_THRSHLD   (AD413X_R3B | 0x3C)
 
#define AD413X_REG_FIFO_DATA   (AD413X_R3B | 0x3D)
 
#define AD413X_ADC_BIPOLAR   NO_OS_BIT(14)
 
#define AD413X_ADC_REF_VAL   NO_OS_BIT(13)
 
#define AD413X_ADC_DOUT_DIS_DEL   NO_OS_BIT(12)
 
#define AD413X_ADC_CONT_READ   NO_OS_BIT(11)
 
#define AD413X_ADC_DATA_STATUS   NO_OS_BIT(10)
 
#define AD413X_ADC_CSB_EN   NO_OS_BIT(9)
 
#define AD413X_ADC_REF_EN   NO_OS_BIT(8)
 
#define AD413X_ADC_DUTY_CYC_RATIO   NO_OS_BIT(6)
 
#define AD413X_ADC_MODE(x)
 
#define AD413X_ADC_CNTRL_MCLK(x)
 
#define AD413X_SYNCB_CLEAR   NO_OS_BIT(10)
 
#define AD413X_INT_PIN_SEL(x)
 
#define AD413X_GPO_DATA_P4   NO_OS_BIT(7)
 
#define AD413X_GPO_DATA_P3   NO_OS_BIT(6)
 
#define AD413X_GPO_DATA_P2   NO_OS_BIT(5)
 
#define AD413X_GPO_DATA_P1   NO_OS_BIT(4)
 
#define AD413X_GPO_CTRL_P4   NO_OS_BIT(3)
 
#define AD413X_GPO_CTRL_P3   NO_OS_BIT(2)
 
#define AD413X_GPO_CTRL_P2   NO_OS_BIT(1)
 
#define AD413X_GPO_CTRL_P1   0x01
 
#define AD413X_VBIAS_15   NO_OS_BIT(15)
 
#define AD413X_VBIAS_14   NO_OS_BIT(14)
 
#define AD413X_VBIAS_13   NO_OS_BIT(13)
 
#define AD413X_VBIAS_12   NO_OS_BIT(12)
 
#define AD413X_VBIAS_11   NO_OS_BIT(11)
 
#define AD413X_VBIAS_10   NO_OS_BIT(10)
 
#define AD413X_VBIAS_9   NO_OS_BIT(9)
 
#define AD413X_VBIAS_8   NO_OS_BIT(8)
 
#define AD413X_VBIAS_7   NO_OS_BIT(7)
 
#define AD413X_VBIAS_6   NO_OS_BIT(6)
 
#define AD413X_VBIAS_5   NO_OS_BIT(5)
 
#define AD413X_VBIAS_4   NO_OS_BIT(4)
 
#define AD413X_VBIAS_3   NO_OS_BIT(3)
 
#define AD413X_VBIAS_2   NO_OS_BIT(2)
 
#define AD413X_VBIAS_1   NO_OS_BIT(1)
 
#define AD413X_VBIAS_0   0x01
 
#define AD413X_AINP_OV_UV_ERR   NO_OS_BIT(11)
 
#define AD413X_AINM_OV_UV_ERR   NO_OS_BIT(10)
 
#define AD413X_REF_OV_UV_ERR   NO_OS_BIT(9)
 
#define AD413X_REF_DETECT_ERR   NO_OS_BIT(8)
 
#define AD413X_ADC_ERR   NO_OS_BIT(7)
 
#define AD413X_SPI_IGNORE_ERR   NO_OS_BIT(6)
 
#define AD413X_SPI_SCLK_CNT_ERR   NO_OS_BIT(5)
 
#define AD413X_SPI_READ_ERR   NO_OS_BIT(4)
 
#define AD413X_SPI_WRITE_ERR   NO_OS_BIT(3)
 
#define AD413X_SPI_CRC_ERR   NO_OS_BIT(2)
 
#define AD413X_MM_CRC_ERR   NO_OS_BIT(1)
 
#define AD413X_ROM_CRC_ERR   0x01
 
#define AD413X_MCLK_CNT_EN   NO_OS_BIT(12)
 
#define AD413X_AINP_OV_UV_ERR_EN   NO_OS_BIT(11)
 
#define AD413X_AINM_OV_UV_ERR_EN   NO_OS_BIT(10)
 
#define AD413X_REF_OV_UV_ERR_EN   NO_OS_BIT(9)
 
#define AD413X_REF_DETECT_ERR_EN   NO_OS_BIT(8)
 
#define AD413X_ADC_ERR_EN   NO_OS_BIT(7)
 
#define AD413X_SPI_IGNORE_ERR_EN   NO_OS_BIT(6)
 
#define AD413X_SPI_SCLK_CNT_ERR_EN   NO_OS_BIT(5)
 
#define AD413X_SPI_READ_ERR_EN   NO_OS_BIT(4)
 
#define AD413X_SPI_WRITE_ERR_EN   NO_OS_BIT(3)
 
#define AD413X_SPI_CRC_ERR_EN   NO_OS_BIT(2)
 
#define AD413X_MM_CRC_ERR_EN   NO_OS_BIT(1)
 
#define AD413X_ROM_CRC_ERR_EN   0x01
 
#define AD413X_ENABLE_M   NO_OS_BIT(23)
 
#define AD413X_SETUP_M(x)
 
#define AD413X_PDSW_M   NO_OS_BIT(19)
 
#define AD413X_THRES_EN_M   NO_OS_BIT(18)
 
#define AD413X_AINP_M(x)
 
#define AD413X_AINM_M(x)
 
#define AD413X_I_OUT1_CH_M(x)
 
#define AD413X_I_OUT0_CH_M(x)
 
#define AD413X_I_OUT_CH_MSK   NO_OS_GENMASK(7,0)
 
#define AD413X_I_OUT1_N(x)
 
#define AD413X_I_OUT0_N(x)
 
#define AD413X_I_OUT_MSK   NO_OS_GENMASK(15,10)
 
#define AD413X_BURNOUT_N(x)
 
#define AD413X_REF_BUF_MSK   NO_OS_GENMASK(7,6)
 
#define AD413X_REF_BUFP_N   NO_OS_BIT(7)
 
#define AD413X_REF_BUFM_N   NO_OS_BIT(6)
 
#define AD413X_REF_SEL_N(x)
 
#define AD413X_PGA_N(x)
 
#define AD413X_PGA_BYP_N   0x01
 
#define AD413X_SETTLE_N(x)
 
#define AD413X_REPEAT_N(x)
 
#define AD413X_FILTER_MODE_N(x)
 
#define AD413X_FS_N(x)
 
#define AD413X_OFFSET_N(x)
 
#define AD413X_GAIN_N(x)
 
#define AD413X_BYPASS_OSC   NO_OS_BIT(15)
 
#define AD413X_PD_ALDO   NO_OS_BIT(14)
 
#define AD413X_CAL_RANGE_X2   NO_OS_BIT(13)
 
#define AD413X_RESERVED(x)
 
#define AD413X_STBY_CTRL_MSK   NO_OS_GENMASK(8,0)
 
#define AD413X_STBY_OUT_EN   NO_OS_BIT(8)
 
#define AD413X_STBY_DIAGNOSTICS_EN   NO_OS_BIT(7)
 
#define AD413X_STBY_GPO_EN   NO_OS_BIT(6)
 
#define AD413X_STBY_PDSW_EN   NO_OS_BIT(5)
 
#define AD413X_STBY_BURNOUT_EN   NO_OS_BIT(4)
 
#define AD413X_STBY_VBIAS_EN   NO_OS_BIT(3)
 
#define AD413X_STBY_IEXC_EN   NO_OS_BIT(2)
 
#define AD413X_STBY_REFHOL_EN   NO_OS_BIT(1)
 
#define AD413X_STBY_INTREF_EN   0x01
 
#define AD413X_ADD_FIFO_STATUS   NO_OS_BIT(19)
 
#define AD413X_ADD_FIFO_HEADER   NO_OS_BIT(18)
 
#define AD413X_FIFO_MODE(x)
 
#define AD413X_FIFO_WRITE_ERR_INT_EN   NO_OS_BIT(14)
 
#define AD413X_FIFO_READ_ERR_INT_EN   NO_OS_BIT(13)
 
#define AD413X_THRES_HIGH_INT_EN   NO_OS_BIT(12)
 
#define AD413X_THRES_LOW_INT_EN   NO_OS_BIT(11)
 
#define AD413X_OVERRUN_INT_EN   NO_OS_BIT(10)
 
#define AD413X_WATERMARK_INT_EN   NO_OS_BIT(9)
 
#define AD413X_EMPTY_INT_EN   NO_OS_BIT(8)
 
#define AD413X_WATERMARK(x)
 
#define AD413X_MASTER_ERR   NO_OS_BIT(7)
 
#define AD413X_FIFO_WRITE_ERR   NO_OS_BIT(6)
 
#define AD413X_FIFO_READ_ERR   NO_OS_BIT(5)
 
#define AD413X_THRES_HIGH_FLAG   NO_OS_BIT(4)
 
#define AD413X_THRES_LOW_FLAG   NO_OS_BIT(3)
 
#define AD413X_OVERRUN_FLAG   NO_OS_BIT(2)
 
#define AD413X_WATERMARK_FLAG   NO_OS_BIT(1)
 
#define AD413X_EMPTY_FLAG   0x01
 
#define AD413X_THRES_HIGH_VAL(x)
 
#define AD413X_THRES_LOW_VAL(x)
 
#define AD413X_CRC8_POLY   0x07
 
#define ENABLE   1U
 
#define DISABLE   0U
 

Enumerations

enum  ad413x_input {
  AD413X_AIN0 ,
  AD413X_AIN1 ,
  AD413X_AIN2 ,
  AD413X_AIN3 ,
  AD413X_AIN4 ,
  AD413X_AIN5 ,
  AD413X_AIN6 ,
  AD413X_AIN7 ,
  AD413X_AIN8 ,
  AD413X_AIN9 ,
  AD413X_AIN10 ,
  AD413X_AIN11 ,
  AD413X_AIN12 ,
  AD413X_AIN13 ,
  AD413X_AIN14 ,
  AD413X_AIN15 ,
  AD413X_TEMP ,
  AD413X_AVSS ,
  AD413X_INT_REF ,
  AD413X_DGND ,
  AD413X_AVDD_AVSS_6P ,
  AD413X_AVDD_AVSS_6M ,
  AD413X_IOVDD_DGND_6P ,
  AD413X_IOVDD_DGND_6M ,
  AD413X_ALDO_AVSS_6P ,
  AD413X_ALDO_AVSS_6M ,
  AD413X_DLDO_DGND_6P ,
  AD413X_DLDO_DGND_6M ,
  AD413X_V_MV_P ,
  AD413X_V_MV_M
}
 ADC input sources for each channel. More...
 
enum  ad413x_preset_nb {
  AD413X_PRESET_0 ,
  AD413X_PRESET_1 ,
  AD413X_PRESET_2 ,
  AD413X_PRESET_3 ,
  AD413X_PRESET_4 ,
  AD413X_PRESET_5 ,
  AD413X_PRESET_6 ,
  AD413X_PRESET_7
}
 Preset number. More...
 
enum  ad413x_mclk_sel {
  AD413X_INT_76_8_KHZ_OUT_OFF ,
  AD413X_INT_76_8_KHZ_OUT_ON ,
  AD413X_EXT_76_8KHZ ,
  AD413X_EXT_153_6_KHZ_DIV_2
}
 Master clock options. More...
 
enum  ad413x_adc_mode {
  AD413X_CONTINOUS_CONV_MODE = 0 ,
  AD413X_SINGLE_CONV_MODE = 1 ,
  AD413X_STANDBY_MODE = 2 ,
  AD413X_PW_DOWN_MODE = 3 ,
  AD413X_IDLE_MODE = 4 ,
  AD413X_INT_OFFSET_CAL = 5 ,
  AD413X_INT_GAIN_CAL = 6 ,
  AD413X_SYS_OFFSET_CAL = 7 ,
  AD413X_SYS_GAIN_CAL = 8 ,
  AD413X_DUTY_CYCLING_MODE = 9 ,
  AD413X_SINGLE_CONV_SYNC_IDLE_MODE = 10 ,
  AD413X_DUTY_CYCLING_SYNC_STBY_MODE = 11
}
 ADC conversion modes. More...
 
enum  ad413x_ref_sel {
  AD413X_REFIN1 ,
  AD413X_REFIN2 ,
  AD413X_REFOUT_AVSS ,
  AD413X_AVDD_AVSS
}
 ADC reference selection. More...
 
enum  ad413x_int_ref {
  AD413X_INTREF_DISABLED ,
  AD413X_INTREF_2_5V ,
  AD413X_INTREF_1_25V
}
 Internal reference selection. More...
 
enum  ad413x_filter {
  AD413X_SYNC4_STANDALONE ,
  AD413X_SYNC4_SYNC1 ,
  AD413X_SYNC3_STANDALONE ,
  AD413X_SYNC3_REJ60 ,
  AD413X_SYNC3_SYNC1 ,
  AD413X_SYNC3_PF1 ,
  AD413X_SYNC3_PF2 ,
  AD413X_SYNC3_PF3 ,
  AD413X_SYNC3_PF4
}
 Filter types. More...
 
enum  ad413x_gain {
  AD413X_GAIN_1 ,
  AD413X_GAIN_2 ,
  AD413X_GAIN_4 ,
  AD413X_GAIN_8 ,
  AD413X_GAIN_16 ,
  AD413X_GAIN_32 ,
  AD413X_GAIN_64 ,
  AD413X_GAIN_128
}
 Gain options. More...
 
enum  ad413x_chip_id {
  AD4129_4 ,
  AD4129_8 ,
  AD4130_4 ,
  AD4130_8 ,
  AD4131_4 ,
  AD4131_8
}
 Supported devices. More...
 
enum  ad413x_settle_time {
  AD413X_32_MCLK ,
  AD413X_64_MCLK ,
  AD413X_128_MCLK ,
  AD413X_256_MCLK ,
  AD413X_512_MCLK ,
  AD413X_1024_MCLK ,
  AD413X_2048_MCLK ,
  AD413X_4096_MCLK
}
 Channel settle time. More...
 
enum  ad413x_exc_current {
  AD413X_EXC_OFF ,
  AD413X_EXC_10UA ,
  AD413X_EXC_20UA ,
  AD413X_EXC_50UA ,
  AD413X_EXC_100UA ,
  AD413X_EXC_150UA ,
  AD413X_EXC_200UA ,
  AD413X_EXC_100NA
}
 Excitation current value. More...
 

Functions

int32_t ad413x_reg_write_msk (struct ad413x_dev *dev, uint32_t reg_addr, uint32_t data, uint32_t mask)
 
int32_t ad413x_set_adc_mode (struct ad413x_dev *dev, enum ad413x_adc_mode mode)
 
int32_t ad413x_set_int_ref (struct ad413x_dev *dev, enum ad413x_int_ref int_ref)
 
int32_t ad413x_data_stat_en (struct ad413x_dev *dev, uint8_t enable)
 
int32_t ad413x_set_gain (struct ad413x_dev *dev, enum ad413x_gain gain, enum ad413x_preset_nb reg_nb)
 
int32_t ad413x_set_ref (struct ad413x_dev *dev, enum ad413x_ref_sel ref, enum ad413x_preset_nb reg_nb)
 
int32_t ad413x_set_ref_buf (struct ad413x_dev *dev, struct ad413x_ref_buf ref_buf, enum ad413x_preset_nb reg_nb)
 
int32_t ad413x_set_filter (struct ad413x_dev *dev, enum ad413x_filter filter, enum ad413x_preset_nb reg_nb)
 
int32_t ad413x_set_settle_time (struct ad413x_dev *dev, enum ad413x_settle_time s_time, enum ad413x_preset_nb reg_nb)
 
int32_t ad413x_set_exc_current (struct ad413x_dev *dev, enum ad413x_exc_current iout0_exc, enum ad413x_exc_current iout1_exc, enum ad413x_preset_nb reg_nb)
 
int32_t ad413x_ch_exc_input (struct ad413x_dev *dev, uint8_t ch_nb, enum ad413x_input iout0_exc_inp, enum ad413x_input iout1_exc_inp)
 
int32_t ad413x_set_ch_preset (struct ad413x_dev *dev, uint8_t ch_nb, enum ad413x_preset_nb preset_nb)
 
int32_t ad413x_ch_en (struct ad413x_dev *dev, uint8_t ch_nb, uint8_t enable)
 
int32_t ad413x_pdsw_en (struct ad413x_dev *dev, uint8_t ch_nb, bool pdsw_en)
 
int32_t ad413x_set_v_bias (struct ad413x_dev *dev, uint16_t v_bias_val)
 
int32_t ad413x_set_standby_ctrl (struct ad413x_dev *dev, struct ad413x_standby_ctrl standby_ctrl)
 
int32_t ad413x_set_mclk (struct ad413x_dev *dev, enum ad413x_mclk_sel clk)
 
int32_t ad413x_do_soft_reset (struct ad413x_dev *dev)
 
int32_t ad413x_reg_write (struct ad413x_dev *dev, uint32_t reg_addr, uint32_t reg_data)
 
int32_t ad413x_reg_read (struct ad413x_dev *dev, uint32_t reg_addr, uint32_t *reg_data)
 
int32_t ad413x_single_conv (struct ad413x_dev *dev, uint32_t *buffer, uint8_t ch_nb)
 
int32_t ad413x_continuous_conv (struct ad413x_dev *dev, uint32_t *buffer, uint8_t ch_nb, uint32_t sample_nb)
 
int32_t ad413x_adc_bipolar (struct ad413x_dev *dev, uint8_t enable)
 
int32_t ad413x_preset_store (struct ad413x_dev *dev, struct ad413x_preset preset, enum ad413x_preset_nb preset_nb)
 
int32_t ad413x_init (struct ad413x_dev **device, struct ad413x_init_param init_param)
 
int32_t ad413x_remove (struct ad413x_dev *dev)
 Free the resources allocated by ad413x_init().
 

Detailed Description

Header file of AD413X Driver.

Author
Andrei Porumb (andre.nosp@m.i.po.nosp@m.rumb@.nosp@m.anal.nosp@m.og.co.nosp@m.m)

Copyright 2022(c) Analog Devices, Inc.

SPDX-License-Identifier: BSD-3-Clause

Macro Definition Documentation

◆ AD413X_ADC_BIPOLAR

#define AD413X_ADC_BIPOLAR   NO_OS_BIT(14)

◆ AD413X_ADC_CNTRL_MCLK

#define AD413X_ADC_CNTRL_MCLK ( x)
Value:
((x) & 0x3)

◆ AD413X_ADC_CONT_READ

#define AD413X_ADC_CONT_READ   NO_OS_BIT(11)

◆ AD413X_ADC_CSB_EN

#define AD413X_ADC_CSB_EN   NO_OS_BIT(9)

◆ AD413X_ADC_DATA_STATUS

#define AD413X_ADC_DATA_STATUS   NO_OS_BIT(10)

◆ AD413X_ADC_DOUT_DIS_DEL

#define AD413X_ADC_DOUT_DIS_DEL   NO_OS_BIT(12)

◆ AD413X_ADC_DUTY_CYC_RATIO

#define AD413X_ADC_DUTY_CYC_RATIO   NO_OS_BIT(6)

◆ AD413X_ADC_ERR

#define AD413X_ADC_ERR   NO_OS_BIT(7)

◆ AD413X_ADC_ERR_EN

#define AD413X_ADC_ERR_EN   NO_OS_BIT(7)

◆ AD413X_ADC_MODE

#define AD413X_ADC_MODE ( x)
Value:
(((x) & 0xF) << 2)

◆ AD413X_ADC_REF_EN

#define AD413X_ADC_REF_EN   NO_OS_BIT(8)

◆ AD413X_ADC_REF_VAL

#define AD413X_ADC_REF_VAL   NO_OS_BIT(13)

◆ AD413X_ADD_FIFO_HEADER

#define AD413X_ADD_FIFO_HEADER   NO_OS_BIT(18)

◆ AD413X_ADD_FIFO_STATUS

#define AD413X_ADD_FIFO_STATUS   NO_OS_BIT(19)

◆ AD413X_ADDR

#define AD413X_ADDR ( x)
Value:
((x) & 0xFF)

◆ AD413X_AINM_M

#define AD413X_AINM_M ( x)
Value:
(((x) & 0x1F) << 8)

◆ AD413X_AINM_OV_UV_ERR

#define AD413X_AINM_OV_UV_ERR   NO_OS_BIT(10)

◆ AD413X_AINM_OV_UV_ERR_EN

#define AD413X_AINM_OV_UV_ERR_EN   NO_OS_BIT(10)

◆ AD413X_AINP_M

#define AD413X_AINP_M ( x)
Value:
(((x) & 0x1F) << 13)

◆ AD413X_AINP_OV_UV_ERR

#define AD413X_AINP_OV_UV_ERR   NO_OS_BIT(11)

◆ AD413X_AINP_OV_UV_ERR_EN

#define AD413X_AINP_OV_UV_ERR_EN   NO_OS_BIT(11)

◆ AD413X_BURNOUT_N

#define AD413X_BURNOUT_N ( x)
Value:
(((x) & 0x3) << 8)

◆ AD413X_BYPASS_OSC

#define AD413X_BYPASS_OSC   NO_OS_BIT(15)

◆ AD413X_CAL_RANGE_X2

#define AD413X_CAL_RANGE_X2   NO_OS_BIT(13)

◆ AD413X_CMD_RD_COM_REG

#define AD413X_CMD_RD_COM_REG ( x)
Value:
(0x40 | ((x) & 0x3F))

◆ AD413X_CMD_WR_COM_REG

#define AD413X_CMD_WR_COM_REG ( x)
Value:
(0x00 | ((x) & 0x3F))

◆ AD413X_CRC8_POLY

#define AD413X_CRC8_POLY   0x07

◆ AD413X_EMPTY_FLAG

#define AD413X_EMPTY_FLAG   0x01

◆ AD413X_EMPTY_INT_EN

#define AD413X_EMPTY_INT_EN   NO_OS_BIT(8)

◆ AD413X_ENABLE_M

#define AD413X_ENABLE_M   NO_OS_BIT(23)

◆ AD413X_FIFO_MODE

#define AD413X_FIFO_MODE ( x)
Value:
(((x) & 0x3) << 16)

◆ AD413X_FIFO_READ_ERR

#define AD413X_FIFO_READ_ERR   NO_OS_BIT(5)

◆ AD413X_FIFO_READ_ERR_INT_EN

#define AD413X_FIFO_READ_ERR_INT_EN   NO_OS_BIT(13)

◆ AD413X_FIFO_WRITE_ERR

#define AD413X_FIFO_WRITE_ERR   NO_OS_BIT(6)

◆ AD413X_FIFO_WRITE_ERR_INT_EN

#define AD413X_FIFO_WRITE_ERR_INT_EN   NO_OS_BIT(14)

◆ AD413X_FILTER_MODE_N

#define AD413X_FILTER_MODE_N ( x)
Value:
(((x) & 0xF) << 12)

◆ AD413X_FS_N

#define AD413X_FS_N ( x)
Value:
((x) & 0x7FF)

◆ AD413X_GAIN_N

#define AD413X_GAIN_N ( x)
Value:
((x) & 0xFFFFFF)

◆ AD413X_GPO_CTRL_P1

#define AD413X_GPO_CTRL_P1   0x01

◆ AD413X_GPO_CTRL_P2

#define AD413X_GPO_CTRL_P2   NO_OS_BIT(1)

◆ AD413X_GPO_CTRL_P3

#define AD413X_GPO_CTRL_P3   NO_OS_BIT(2)

◆ AD413X_GPO_CTRL_P4

#define AD413X_GPO_CTRL_P4   NO_OS_BIT(3)

◆ AD413X_GPO_DATA_P1

#define AD413X_GPO_DATA_P1   NO_OS_BIT(4)

◆ AD413X_GPO_DATA_P2

#define AD413X_GPO_DATA_P2   NO_OS_BIT(5)

◆ AD413X_GPO_DATA_P3

#define AD413X_GPO_DATA_P3   NO_OS_BIT(6)

◆ AD413X_GPO_DATA_P4

#define AD413X_GPO_DATA_P4   NO_OS_BIT(7)

◆ AD413X_I_OUT0_CH_M

#define AD413X_I_OUT0_CH_M ( x)
Value:
((x) & 0xF)

◆ AD413X_I_OUT0_N

#define AD413X_I_OUT0_N ( x)
Value:
(((x) & 0x7) << 10)

◆ AD413X_I_OUT1_CH_M

#define AD413X_I_OUT1_CH_M ( x)
Value:
(((x) & 0xF) << 4)

◆ AD413X_I_OUT1_N

#define AD413X_I_OUT1_N ( x)
Value:
(((x) & 0x7) << 13)

◆ AD413X_I_OUT_CH_MSK

#define AD413X_I_OUT_CH_MSK   NO_OS_GENMASK(7,0)

◆ AD413X_I_OUT_MSK

#define AD413X_I_OUT_MSK   NO_OS_GENMASK(15,10)

◆ AD413X_INT_PIN_SEL

#define AD413X_INT_PIN_SEL ( x)
Value:
(((x) & 0x3) << 8)

◆ AD413X_MASTER_ERR

#define AD413X_MASTER_ERR   NO_OS_BIT(7)

◆ AD413X_MCLK_CNT_EN

#define AD413X_MCLK_CNT_EN   NO_OS_BIT(12)

◆ AD413X_MM_CRC_ERR

#define AD413X_MM_CRC_ERR   NO_OS_BIT(1)

◆ AD413X_MM_CRC_ERR_EN

#define AD413X_MM_CRC_ERR_EN   NO_OS_BIT(1)

◆ AD413X_OFFSET_N

#define AD413X_OFFSET_N ( x)
Value:
((x) & 0xFFFFFF)

◆ AD413X_OVERRUN_FLAG

#define AD413X_OVERRUN_FLAG   NO_OS_BIT(2)

◆ AD413X_OVERRUN_INT_EN

#define AD413X_OVERRUN_INT_EN   NO_OS_BIT(10)

◆ AD413X_PD_ALDO

#define AD413X_PD_ALDO   NO_OS_BIT(14)

◆ AD413X_PDSW_M

#define AD413X_PDSW_M   NO_OS_BIT(19)

◆ AD413X_PGA_BYP_N

#define AD413X_PGA_BYP_N   0x01

◆ AD413X_PGA_N

#define AD413X_PGA_N ( x)
Value:
(((x) & 0x7) << 1)

◆ AD413X_R1B

#define AD413X_R1B   (1 << 8)

◆ AD413X_R2B

#define AD413X_R2B   (2 << 8)

◆ AD413X_R3B

#define AD413X_R3B   (3 << 8)

◆ AD413X_REF_BUF_MSK

#define AD413X_REF_BUF_MSK   NO_OS_GENMASK(7,6)

◆ AD413X_REF_BUFM_N

#define AD413X_REF_BUFM_N   NO_OS_BIT(6)

◆ AD413X_REF_BUFP_N

#define AD413X_REF_BUFP_N   NO_OS_BIT(7)

◆ AD413X_REF_DETECT_ERR

#define AD413X_REF_DETECT_ERR   NO_OS_BIT(8)

◆ AD413X_REF_DETECT_ERR_EN

#define AD413X_REF_DETECT_ERR_EN   NO_OS_BIT(8)

◆ AD413X_REF_OV_UV_ERR

#define AD413X_REF_OV_UV_ERR   NO_OS_BIT(9)

◆ AD413X_REF_OV_UV_ERR_EN

#define AD413X_REF_OV_UV_ERR_EN   NO_OS_BIT(9)

◆ AD413X_REF_SEL_N

#define AD413X_REF_SEL_N ( x)
Value:
(((x) & 0x3) << 4)

◆ AD413X_REG_ADC_CTRL

#define AD413X_REG_ADC_CTRL   (AD413X_R2B | 0x1)

◆ AD413X_REG_CHN

#define AD413X_REG_CHN ( x)
Value:
(AD413X_R3B | (0x09U + (x)))
#define AD413X_R3B
Definition ad413x.h:27

◆ AD413X_REG_CONFIG

#define AD413X_REG_CONFIG ( x)
Value:
(AD413X_R2B | (0x19U + (x)))
#define AD413X_R2B
Definition ad413x.h:26

◆ AD413X_REG_DATA

#define AD413X_REG_DATA   (AD413X_R3B | 0x2)

◆ AD413X_REG_ERROR

#define AD413X_REG_ERROR   (AD413X_R2B | 0x6)

◆ AD413X_REG_ERROR_EN

#define AD413X_REG_ERROR_EN   (AD413X_R2B | 0x7)

◆ AD413X_REG_FIFO_CTRL

#define AD413X_REG_FIFO_CTRL   (AD413X_R3B | 0x3A)

◆ AD413X_REG_FIFO_DATA

#define AD413X_REG_FIFO_DATA   (AD413X_R3B | 0x3D)

◆ AD413X_REG_FIFO_STS

#define AD413X_REG_FIFO_STS   (AD413X_R1B | 0x3B)

◆ AD413X_REG_FIFO_THRSHLD

#define AD413X_REG_FIFO_THRSHLD   (AD413X_R3B | 0x3C)

◆ AD413X_REG_FILTER

#define AD413X_REG_FILTER ( x)
Value:
(AD413X_R3B | (0x21U + (x)))

◆ AD413X_REG_GAIN

#define AD413X_REG_GAIN ( x)
Value:
(AD413X_R3B | (0x31U + (x)))

◆ AD413X_REG_ID

#define AD413X_REG_ID   (AD413X_R1B | 0x5)

◆ AD413X_REG_IO_CTRL

#define AD413X_REG_IO_CTRL   (AD413X_R2B | 0x3)

◆ AD413X_REG_MCLK_CNT

#define AD413X_REG_MCLK_CNT   (AD413X_R1B | 0x8)

◆ AD413X_REG_MISC

#define AD413X_REG_MISC   (AD413X_R2B | 0x39)

◆ AD413X_REG_OFFSET

#define AD413X_REG_OFFSET ( x)
Value:
(AD413X_R3B | (0x29U + (x)))

◆ AD413X_REG_STATUS

#define AD413X_REG_STATUS   (AD413X_R1B | 0x0)

◆ AD413X_REG_VBIAS_CTRL

#define AD413X_REG_VBIAS_CTRL   (AD413X_R2B | 0x4)

◆ AD413X_REPEAT_N

#define AD413X_REPEAT_N ( x)
Value:
(((x) & 0x1F) << 16)

◆ AD413X_RESERVED

#define AD413X_RESERVED ( x)
Value:
(((x) & 0xF) << 9)

◆ AD413X_ROM_CRC_ERR

#define AD413X_ROM_CRC_ERR   0x01

◆ AD413X_ROM_CRC_ERR_EN

#define AD413X_ROM_CRC_ERR_EN   0x01

◆ AD413X_SETTLE_N

#define AD413X_SETTLE_N ( x)
Value:
(((x) & 0x7) << 21)

◆ AD413X_SETUP_M

#define AD413X_SETUP_M ( x)
Value:
(((x) & 0x7) << 20)

◆ AD413X_SPI_CRC_ERR

#define AD413X_SPI_CRC_ERR   NO_OS_BIT(2)

◆ AD413X_SPI_CRC_ERR_EN

#define AD413X_SPI_CRC_ERR_EN   NO_OS_BIT(2)

◆ AD413X_SPI_IGNORE_ERR

#define AD413X_SPI_IGNORE_ERR   NO_OS_BIT(6)

◆ AD413X_SPI_IGNORE_ERR_EN

#define AD413X_SPI_IGNORE_ERR_EN   NO_OS_BIT(6)

◆ AD413X_SPI_READ_ERR

#define AD413X_SPI_READ_ERR   NO_OS_BIT(4)

◆ AD413X_SPI_READ_ERR_EN

#define AD413X_SPI_READ_ERR_EN   NO_OS_BIT(4)

◆ AD413X_SPI_SCLK_CNT_ERR

#define AD413X_SPI_SCLK_CNT_ERR   NO_OS_BIT(5)

◆ AD413X_SPI_SCLK_CNT_ERR_EN

#define AD413X_SPI_SCLK_CNT_ERR_EN   NO_OS_BIT(5)

◆ AD413X_SPI_WRITE_ERR

#define AD413X_SPI_WRITE_ERR   NO_OS_BIT(3)

◆ AD413X_SPI_WRITE_ERR_EN

#define AD413X_SPI_WRITE_ERR_EN   NO_OS_BIT(3)

◆ AD413X_STBY_BURNOUT_EN

#define AD413X_STBY_BURNOUT_EN   NO_OS_BIT(4)

◆ AD413X_STBY_CTRL_MSK

#define AD413X_STBY_CTRL_MSK   NO_OS_GENMASK(8,0)

◆ AD413X_STBY_DIAGNOSTICS_EN

#define AD413X_STBY_DIAGNOSTICS_EN   NO_OS_BIT(7)

◆ AD413X_STBY_GPO_EN

#define AD413X_STBY_GPO_EN   NO_OS_BIT(6)

◆ AD413X_STBY_IEXC_EN

#define AD413X_STBY_IEXC_EN   NO_OS_BIT(2)

◆ AD413X_STBY_INTREF_EN

#define AD413X_STBY_INTREF_EN   0x01

◆ AD413X_STBY_OUT_EN

#define AD413X_STBY_OUT_EN   NO_OS_BIT(8)

◆ AD413X_STBY_PDSW_EN

#define AD413X_STBY_PDSW_EN   NO_OS_BIT(5)

◆ AD413X_STBY_REFHOL_EN

#define AD413X_STBY_REFHOL_EN   NO_OS_BIT(1)

◆ AD413X_STBY_VBIAS_EN

#define AD413X_STBY_VBIAS_EN   NO_OS_BIT(3)

◆ AD413X_SYNCB_CLEAR

#define AD413X_SYNCB_CLEAR   NO_OS_BIT(10)

◆ AD413X_THRES_EN_M

#define AD413X_THRES_EN_M   NO_OS_BIT(18)

◆ AD413X_THRES_HIGH_FLAG

#define AD413X_THRES_HIGH_FLAG   NO_OS_BIT(4)

◆ AD413X_THRES_HIGH_INT_EN

#define AD413X_THRES_HIGH_INT_EN   NO_OS_BIT(12)

◆ AD413X_THRES_HIGH_VAL

#define AD413X_THRES_HIGH_VAL ( x)
Value:
(((x) & 0xFFF) << 12)

◆ AD413X_THRES_LOW_FLAG

#define AD413X_THRES_LOW_FLAG   NO_OS_BIT(3)

◆ AD413X_THRES_LOW_INT_EN

#define AD413X_THRES_LOW_INT_EN   NO_OS_BIT(11)

◆ AD413X_THRES_LOW_VAL

#define AD413X_THRES_LOW_VAL ( x)
Value:
((x) & 0xFFF)

◆ AD413X_TRANSF_LEN

#define AD413X_TRANSF_LEN ( x)
Value:
(((x) >> 8) & 0xFF)

◆ AD413X_VBIAS_0

#define AD413X_VBIAS_0   0x01

◆ AD413X_VBIAS_1

#define AD413X_VBIAS_1   NO_OS_BIT(1)

◆ AD413X_VBIAS_10

#define AD413X_VBIAS_10   NO_OS_BIT(10)

◆ AD413X_VBIAS_11

#define AD413X_VBIAS_11   NO_OS_BIT(11)

◆ AD413X_VBIAS_12

#define AD413X_VBIAS_12   NO_OS_BIT(12)

◆ AD413X_VBIAS_13

#define AD413X_VBIAS_13   NO_OS_BIT(13)

◆ AD413X_VBIAS_14

#define AD413X_VBIAS_14   NO_OS_BIT(14)

◆ AD413X_VBIAS_15

#define AD413X_VBIAS_15   NO_OS_BIT(15)

◆ AD413X_VBIAS_2

#define AD413X_VBIAS_2   NO_OS_BIT(2)

◆ AD413X_VBIAS_3

#define AD413X_VBIAS_3   NO_OS_BIT(3)

◆ AD413X_VBIAS_4

#define AD413X_VBIAS_4   NO_OS_BIT(4)

◆ AD413X_VBIAS_5

#define AD413X_VBIAS_5   NO_OS_BIT(5)

◆ AD413X_VBIAS_6

#define AD413X_VBIAS_6   NO_OS_BIT(6)

◆ AD413X_VBIAS_7

#define AD413X_VBIAS_7   NO_OS_BIT(7)

◆ AD413X_VBIAS_8

#define AD413X_VBIAS_8   NO_OS_BIT(8)

◆ AD413X_VBIAS_9

#define AD413X_VBIAS_9   NO_OS_BIT(9)

◆ AD413X_WATERMARK

#define AD413X_WATERMARK ( x)
Value:
((x) & 0xFF)

◆ AD413X_WATERMARK_FLAG

#define AD413X_WATERMARK_FLAG   NO_OS_BIT(1)

◆ AD413X_WATERMARK_INT_EN

#define AD413X_WATERMARK_INT_EN   NO_OS_BIT(9)

◆ DISABLE

#define DISABLE   0U

◆ ENABLE

#define ENABLE   1U

Enumeration Type Documentation

◆ ad413x_adc_mode

ADC conversion modes.

Enumerator
AD413X_CONTINOUS_CONV_MODE 
AD413X_SINGLE_CONV_MODE 
AD413X_STANDBY_MODE 
AD413X_PW_DOWN_MODE 
AD413X_IDLE_MODE 
AD413X_INT_OFFSET_CAL 
AD413X_INT_GAIN_CAL 
AD413X_SYS_OFFSET_CAL 
AD413X_SYS_GAIN_CAL 
AD413X_DUTY_CYCLING_MODE 
AD413X_SINGLE_CONV_SYNC_IDLE_MODE 
AD413X_DUTY_CYCLING_SYNC_STBY_MODE 

◆ ad413x_chip_id

Supported devices.

Enumerator
AD4129_4 
AD4129_8 
AD4130_4 
AD4130_8 
AD4131_4 
AD4131_8 

◆ ad413x_exc_current

Excitation current value.

Enumerator
AD413X_EXC_OFF 
AD413X_EXC_10UA 
AD413X_EXC_20UA 
AD413X_EXC_50UA 
AD413X_EXC_100UA 
AD413X_EXC_150UA 
AD413X_EXC_200UA 
AD413X_EXC_100NA 

◆ ad413x_filter

Filter types.

Enumerator
AD413X_SYNC4_STANDALONE 
AD413X_SYNC4_SYNC1 
AD413X_SYNC3_STANDALONE 
AD413X_SYNC3_REJ60 
AD413X_SYNC3_SYNC1 
AD413X_SYNC3_PF1 
AD413X_SYNC3_PF2 
AD413X_SYNC3_PF3 
AD413X_SYNC3_PF4 

◆ ad413x_gain

Gain options.

Enumerator
AD413X_GAIN_1 
AD413X_GAIN_2 
AD413X_GAIN_4 
AD413X_GAIN_8 
AD413X_GAIN_16 
AD413X_GAIN_32 
AD413X_GAIN_64 
AD413X_GAIN_128 

◆ ad413x_input

ADC input sources for each channel.

Enumerator
AD413X_AIN0 
AD413X_AIN1 
AD413X_AIN2 
AD413X_AIN3 
AD413X_AIN4 
AD413X_AIN5 
AD413X_AIN6 
AD413X_AIN7 
AD413X_AIN8 
AD413X_AIN9 
AD413X_AIN10 
AD413X_AIN11 
AD413X_AIN12 
AD413X_AIN13 
AD413X_AIN14 
AD413X_AIN15 
AD413X_TEMP 
AD413X_AVSS 
AD413X_INT_REF 
AD413X_DGND 
AD413X_AVDD_AVSS_6P 
AD413X_AVDD_AVSS_6M 
AD413X_IOVDD_DGND_6P 
AD413X_IOVDD_DGND_6M 
AD413X_ALDO_AVSS_6P 
AD413X_ALDO_AVSS_6M 
AD413X_DLDO_DGND_6P 
AD413X_DLDO_DGND_6M 
AD413X_V_MV_P 
AD413X_V_MV_M 

◆ ad413x_int_ref

Internal reference selection.

Enumerator
AD413X_INTREF_DISABLED 
AD413X_INTREF_2_5V 
AD413X_INTREF_1_25V 

◆ ad413x_mclk_sel

Master clock options.

Enumerator
AD413X_INT_76_8_KHZ_OUT_OFF 
AD413X_INT_76_8_KHZ_OUT_ON 
AD413X_EXT_76_8KHZ 
AD413X_EXT_153_6_KHZ_DIV_2 

◆ ad413x_preset_nb

Preset number.

Enumerator
AD413X_PRESET_0 
AD413X_PRESET_1 
AD413X_PRESET_2 
AD413X_PRESET_3 
AD413X_PRESET_4 
AD413X_PRESET_5 
AD413X_PRESET_6 
AD413X_PRESET_7 

◆ ad413x_ref_sel

ADC reference selection.

Enumerator
AD413X_REFIN1 
AD413X_REFIN2 
AD413X_REFOUT_AVSS 
AD413X_AVDD_AVSS 

◆ ad413x_settle_time

Channel settle time.

Enumerator
AD413X_32_MCLK 
AD413X_64_MCLK 
AD413X_128_MCLK 
AD413X_256_MCLK 
AD413X_512_MCLK 
AD413X_1024_MCLK 
AD413X_2048_MCLK 
AD413X_4096_MCLK 

Function Documentation

◆ ad413x_adc_bipolar()

int32_t ad413x_adc_bipolar ( struct ad413x_dev * dev,
uint8_t enable )

Enable/disable bipolar data coding.

Parameters
dev- The device structure.
enable- 1 - Bipolar 0 - Unipolar
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_ch_en()

int32_t ad413x_ch_en ( struct ad413x_dev * dev,
uint8_t ch_nb,
uint8_t enable )

Enable/disable channel.

Parameters
dev- The device structure.
ch_nb- The channel number.
enable- Channel status.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_ch_exc_input()

int32_t ad413x_ch_exc_input ( struct ad413x_dev * dev,
uint8_t ch_nb,
enum ad413x_input iout0_exc_inp,
enum ad413x_input iout1_exc_inp )

Select the excitation source pins.

Parameters
dev- The device structure.
ch_nb- The channel number.
iout0_exc_inp- IOUT0 excitation input pin.
iout1_exc_inp- IOUT1 excitation input pin.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_continuous_conv()

int32_t ad413x_continuous_conv ( struct ad413x_dev * dev,
uint32_t * buffer,
uint8_t ch_nb,
uint32_t sample_nb )

Continuous conversion of each adc active channel.

Parameters
dev- The device structure.
buffer- Buffer to store read data. Buffer size needs to be at least equal to the number of active channels * samples number. Results will be stored in consecutive order of the active channels.
ch_nb- Number of active channels.
sample_nb- Samples number.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_data_stat_en()

int32_t ad413x_data_stat_en ( struct ad413x_dev * dev,
uint8_t enable )

Enable/disable DATA_STAT field.

Parameters
dev- The device structure.
enable- 0 DISABLE 1 ENABLE
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_do_soft_reset()

int32_t ad413x_do_soft_reset ( struct ad413x_dev * dev)

Do a SPI software reset.

Parameters
dev- The device structure.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_init()

int32_t ad413x_init ( struct ad413x_dev ** device,
struct ad413x_init_param init_param )

Initialize the device.

Parameters
device- The device structure.
init_param- The structure that contains the device initial parameters.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_pdsw_en()

int32_t ad413x_pdsw_en ( struct ad413x_dev * dev,
uint8_t ch_nb,
bool pdsw_en )

Enable/disable Power-Down Switch (PDSW).

Parameters
dev- The device structure.
ch_nb- The channel number.
pdsw_en- PDSW status.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_preset_store()

int32_t ad413x_preset_store ( struct ad413x_dev * dev,
struct ad413x_preset preset,
enum ad413x_preset_nb preset_nb )

Store adc channel presets.

Parameters
dev- The device structure.
preset- The structure to be saved as preset.
preset_nb- Preset's number.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_reg_read()

int32_t ad413x_reg_read ( struct ad413x_dev * dev,
uint32_t reg_addr,
uint32_t * reg_data )

SPI internal register read from device.

Parameters
dev- The device structure.
reg_addr- The register address.
reg_data- The register data.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_reg_write()

int32_t ad413x_reg_write ( struct ad413x_dev * dev,
uint32_t reg_addr,
uint32_t reg_data )

SPI internal register write to device.

Parameters
dev- The device structure.
reg_addr- The register address.
reg_data- The register data.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_reg_write_msk()

int32_t ad413x_reg_write_msk ( struct ad413x_dev * dev,
uint32_t reg_addr,
uint32_t data,
uint32_t mask )

SPI internal register write to device using a mask.

Parameters
dev- The device structure.
reg_addr- The register address.
data- The register data.
mask- The mask.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_remove()

int32_t ad413x_remove ( struct ad413x_dev * dev)

Free the resources allocated by ad413x_init().

Parameters
dev- The device structure.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_adc_mode()

int32_t ad413x_set_adc_mode ( struct ad413x_dev * dev,
enum ad413x_adc_mode mode )

Set the mode of the ADC.

Parameters
dev- The device structure.
mode- The ADC mode Accepted values: AD4110_CONTINOUS_CONV_MODE AD4110_SINGLE_CONV_MODE AD4110_STANDBY_MODE AD4110_PW_DOWN_MODE AD4110_SYS_OFFSET_CAL AD4110_SYS_GAIN_CAL
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_ch_preset()

int32_t ad413x_set_ch_preset ( struct ad413x_dev * dev,
uint8_t ch_nb,
enum ad413x_preset_nb preset_nb )

Select preset for adc channel.

Parameters
dev- The device structure.
ch_nb- The channel number.
preset_nb- The preset number.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_exc_current()

int32_t ad413x_set_exc_current ( struct ad413x_dev * dev,
enum ad413x_exc_current iout0_exc,
enum ad413x_exc_current iout1_exc,
enum ad413x_preset_nb reg_nb )

Select excitation current value from config register.

Parameters
dev- The device structure.
iout0_exc- The Iout0 excitation current value.
iout1_exc- The Iout1 excitation current value. Accepted values: AD413X_EXC_OFF AD413X_EXC_10UA AD413X_EXC_20UA AD413X_EXC_50UA AD413X_EXC_100UA AD413X_EXC_150UA AD413X_EXC_200UA AD413X_EXC_100NA
reg_nb- Number of Configuration Register
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_filter()

int32_t ad413x_set_filter ( struct ad413x_dev * dev,
enum ad413x_filter filter,
enum ad413x_preset_nb reg_nb )

Select filter from filter register.

Parameters
dev- The device structure.
filter- The filter type. Accepted values: AD413X_SYNC4_STANDALONE AD413X_SYNC4_SYNC1 AD413X_SYNC3_STANDALONE AD413X_SYNC3_REJ60 AD413X_SYNC3_SYNC1 AD413X_SYNC3_PF1 AD413X_SYNC3_PF2 AD413X_SYNC3_PF3 AD413X_SYNC3_PF4
reg_nb- Number of Configuration Register
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_gain()

int32_t ad413x_set_gain ( struct ad413x_dev * dev,
enum ad413x_gain gain,
enum ad413x_preset_nb reg_nb )

Set the gain from configuration register.

Parameters
dev- The device structure.
gain- The gain value. Accepted values: AD413X_GAIN_1 AD413X_GAIN_2 AD413X_GAIN_4 AD413X_GAIN_8 AD413X_GAIN_16 AD413X_GAIN_32 AD413X_GAIN_64 AD413X_GAIN_128
reg_nb- Number of Configuration Register
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_int_ref()

int32_t ad413x_set_int_ref ( struct ad413x_dev * dev,
enum ad413x_int_ref int_ref )

Set the internal reference.

Parameters
dev- The device structure.
int_ref- The internal reference option. Accepted values: AD413X_INTREF_DISABLED AD413X_INTREF_2_5V, AD413X_INTREF_1_25V
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_mclk()

int32_t ad413x_set_mclk ( struct ad413x_dev * dev,
enum ad413x_mclk_sel clk )

Set ADC master clock mode.

Parameters
dev- The device structure.
clk- The clock mode. Accepted values: AD413X_INT_76_8_KHZ_OUT_OFF AD413X_INT_76_8_KHZ_OUT_ON AD413X_EXT_76_8KHZ AD413X_EXT_153_6_KHZ_DIV_2
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_ref()

int32_t ad413x_set_ref ( struct ad413x_dev * dev,
enum ad413x_ref_sel ref,
enum ad413x_preset_nb reg_nb )

Select reference from configuration register.

Parameters
dev- The device structure.
ref- The reference value. Accepted values: AD413X_REFIN1 AD413X_REFIN2 AD413X_REFOUT_AVSS AD413X_AVDD_AVSS
reg_nb- Number of Configuration Register
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_ref_buf()

int32_t ad413x_set_ref_buf ( struct ad413x_dev * dev,
struct ad413x_ref_buf ref_buf,
enum ad413x_preset_nb reg_nb )

Select the reference buffers.

Parameters
dev- The device structure.
ref_buf- The reference buffer status.
reg_nb- Number of Configuration Register
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_settle_time()

int32_t ad413x_set_settle_time ( struct ad413x_dev * dev,
enum ad413x_settle_time s_time,
enum ad413x_preset_nb reg_nb )

Select settle time from filter register.

Parameters
dev- The device structure.
s_time- The settle time value. Accepted values: AD413X_32_MCLK AD413X_64_MCLK AD413X_128_MCLK AD413X_256_MCLK AD413X_512_MCLK AD413X_1024_MCLK AD413X_2048_MCLK AD413X_4096_MCLK
reg_nb- Number of Configuration Register
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_standby_ctrl()

int32_t ad413x_set_standby_ctrl ( struct ad413x_dev * dev,
struct ad413x_standby_ctrl standby_ctrl )

Set standby control flags.

Parameters
dev- The device structure.
standby_ctrl- Standby control value
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_set_v_bias()

int32_t ad413x_set_v_bias ( struct ad413x_dev * dev,
uint16_t v_bias_val )

Set output VBIAS on analog inputs.

Parameters
dev- The device structure.
v_bias_val- Bitmask of the VBIAS pins to enable, bit n corresponding to VBIAS_n of the device.
Returns
0 in case of success, negative error code otherwise.

◆ ad413x_single_conv()

int32_t ad413x_single_conv ( struct ad413x_dev * dev,
uint32_t * buffer,
uint8_t ch_nb )

Single conversion of each adc active channel.

Parameters
dev- The device structure.
buffer- Buffer to store read data. Buffer size needs to be at least equal to the number of active channels. Results will be stored in consecutive order of the active channels.
ch_nb- Number of active channels.
Returns
0 in case of success, negative error code otherwise.