![]() |
no-OS
|
Device specific parameters. More...
#include <ad413x.h>
Public Attributes | |
| const char * | name |
| uint8_t | id |
| uint8_t | resolution |
| uint8_t | max_analog_pins |
| bool | has_fifo |
| const uint8_t * | pin_map |
Device specific parameters.
| bool ad413x_chip_info::has_fifo |
| uint8_t ad413x_chip_info::id |
| uint8_t ad413x_chip_info::max_analog_pins |
| const char* ad413x_chip_info::name |
| const uint8_t* ad413x_chip_info::pin_map |
| uint8_t ad413x_chip_info::resolution |