![]() |
no-OS
|
MAX78000 RISC-V (CPU1) initialization. More...
Functions | |
| void | SystemCoreClockUpdate (void) |
| Update SystemCoreClock from the system clock configuration. | |
| __weak int | no_os_init (void) |
| Initialize CPU1 services; system clocks are configured by CPU0. | |
| int | Board_Init (void) |
| SDK board initialization hook, called by the CPU1 startup code. | |
MAX78000 RISC-V (CPU1) initialization.
Copyright 2026(c) Analog Devices, Inc.
SPDX-License-Identifier: BSD-3-Clause
| int Board_Init | ( | void | ) |
SDK board initialization hook, called by the CPU1 startup code.
| __weak int no_os_init | ( | void | ) |
Initialize CPU1 services; system clocks are configured by CPU0.
Initialize the risc-v rx and run in machine mode.
| void SystemCoreClockUpdate | ( | void | ) |
Update SystemCoreClock from the system clock configuration.
PeripheralClock is derived from the system clock, independently of CPU1's ISO clock. CPU0 may put its SDK clock variable in a different SRAM region.