no-OS
Loading...
Searching...
No Matches
maxim_time.h File Reference

MAX78000 RISC-V (CPU1) time base interface. More...

Functions

int maxim_time_init (void)
 Reserve the configured timer for CPU1 elapsed time.
 

Detailed Description

MAX78000 RISC-V (CPU1) time base interface.

Author
Victor Pascu (victo.nosp@m.r.pa.nosp@m.scu@a.nosp@m.nalo.nosp@m.g.com)

Copyright 2026(c) Analog Devices, Inc.

SPDX-License-Identifier: BSD-3-Clause

Function Documentation

◆ maxim_time_init()

int maxim_time_init ( void )

Reserve the configured timer for CPU1 elapsed time.

Reserve the configured timer for CPU1 elapsed time.

Returns
0 in case of success, -EIO if the timer could not be initialized.