Scopy Preferences
Scopy Preferences can be accessed using the bottom left side preferences button. On the right side of the page, preferences for each plugin are available.
The Open button will try to open the specific OS explorer in order to find the preference storage file.
Clicking the Reset Scopy button will reset the application to a default configuration.
Changing some of the listed preferences will require an application restart. More details on each preference, as well as their ID - used to identify them in the .ini files, can be found in the table below.
ID |
Title |
Description |
|---|---|---|
general_save_session |
Save/Load Scopy session |
Allow Scopy to automatically save/load the session using .ini files into a predefined location. |
general_save_attached |
Save/Load tool attached state |
Allow Scopy to save the state of all instruments, whether they were detached/attached when the application was closed, and load this state accordingly when the application restarts. |
general_doubleclick_attach |
Doubleclick to attach/detach tool |
Indicates whether double-clicking attaches instruments in the application. Enabling this option allows the user to quickly attach instruments by double-clicking on them. |
general_doubleclick_ctrl_opens_menu |
Doubleclick control buttons to open menu |
Enable the double click action for menu opening. |
general_use_opengl |
Enable OpenGL plotting |
Use OpenGL accelerated plotting in order to speed-up the process and avoid blocking the application while large numbers of samples are displayed. This feature may not be supported on all systems. |
general_use_animations |
Enable menu animations |
Enable a smooth sliding transition effect for menus when they are opened or closed. |
general_check_online_version |
Enable automatic online check for updates. |
Indicates whether the application should check for online version updates. Enabling this option allows the application to automatically check for and notify the user of available updates at startup. |
general_show_status_bar |
Enable the status bar for displaying important messages. |
Indicates whether the status bar should be displayed in the application. This setting allows the user to enable or disable the status bar, which provides information about the current state of the application. Important messages such as connection done or alerts are displayed here. |
show_grid |
Show Grid |
Indicates whether the plot grid is visible across the application. The user can enable or disable this in order to configure the |
show_graticule |
Show Graticule |
This setting allows the user to enable or disable the display of the graticule on all the plots in the application for better signal visualization. |
iiowidgets_use_lazy_loading |
Use Lazy Loading |
Indicates whether lazy loading should be used for IIO widgets. Enabling this option allows the application to load IIO widgets only when they are needed, improving startup performance. |
general_use_native_dialogs |
Use native dialogs |
Indicates whether native dialogs should be used in the application. This setting allows the user to enable or disable the use of native file dialogs and other system dialogs within the application. |
general_connect_to_multiple_devices |
Connect to multiple devices |
Allows the application to connect to multiple devices simultaneously, providing a mechanism to handle them separately using different sections in the left side menu. |
general_scan_for_devices |
Regularly scan for new devices |
Select whether Scopy should be able to search for new devices periodically, allowing the application to automatically populate the device list with connected devices. Otherwise, all devices need to be added manually from the Add page. |
general_show_warning_on_connection_lost |
Show warning before disconnecting on connection lost |
When enabled, shows a warning in the status bar with a disconnect button when connection to a device is lost. When disabled, the device will be automatically disconnected. |
device_menu_item |
Show detailed device header in tool menu |
Toggle the display of a detailed device header in the tool menu. This header includes the device name, URI, icon, and status indicators. Clicking the device icon navigates to the device configuration page, if available. Note: Enabling this option requires removing and re-adding all devices in the tool menu. |
general_use_docking_if_available |
Use docking elements if available |
If the application was built with the docking feature, enable it. This will make some plots and elements detachable, thus enabling the user to configure the position of these elements in the application. |
general_scripting_enabled |
Enable the use of Scripting Tool |
When disabled, the Scripting Tool will not be accessible. |
general_mcp_server_enabled |
Enable the MCP server |
When enabled, Scopy exposes a local MCP control socket for AI agents. |
dc_cmd_execution_parallel |
Enable parallel command execution |
When enabled, Scopy’s plugins execute backend commands in parallel using an optimal number of threads. Otherwise, a single thread is used. If the device has already been added to the Device Browser, changing this preference will have no effect. The preference is applied when a new device is added. |
autoconnect_previous |
Auto-connect to previous session |
Automatically use the saved URI to connect to previous devices, if available, when the application starts. This speeds up the connection process and reduces the number of necessary steps. |
general_show_plot_fps |
Show plot FPS |
Indicates whether the frames per second should be displayed in plots across the entire application. |
general_theme |
Theme |
Theme setting for the application interface. The user can choose between Harmonic style (light or dark |
general_language |
Language |
Language setting for the application interface. Multiple options available, check out the documentation if a new language is needed. |
general_plot_target_fps |
Plot target FPS |
Select the Frames per second value for rendering plots in the entire application. |
plugins_use_debugger_v2 |
Use Debugger V2 plugin |
Switch between the old style debugger instrument, having just basic controls over attributes or the new instrument type, IIO Explorer, having a tree-like structure. |
debugger_v2_include_debugfs |
Include debug attributes in IIO Explorer |
Enable/disable the use of advanced debug attributes in the instrument. |
regmap_color_by_value |
Use color to reflect value |
Select from various configurations available which elements in the Register Map are color coded for better visual interpretation. |
adc_plot_labels |
Default state for plot labels |
Sets plot labels to be visible/hidden by default. Plot labels may be enabled/disabled within the ADC plot settings, overwriting this setting |
adc_add_remove_plot |
Add/Remove plot feature |
Allows the user to create multiple time or frequency plots within the ADC instrument. Any channel can be moved between plots to provide visual clarity and separation. |
adc_add_remove_instrument |
Add/Remove instrument feature |
Allows the user to create multiple time or frequency instruments, providing an easy way to switch between different run scenarios without affecting previous settings. |
adc_enable_iio_context_ping |
Enable automatic IIO context ping |
When enabled, a ping may be called before some ADC operations to verify if the context is working as expected. |
adc_plot_xaxis_label_position |
Plot X-Axis scale position |
Select whether the X-Axis labels are displayed on the top or bottom of the plot. Only applied after restart. |
adc_plot_yaxis_label_position |
Plot Y-Axis scale position |
Select whether the Y-Axis labels are displayed on the left or right side of the plot. Only applied after restart. |
adc_plot_yaxis_handle_position |
Plot channel Y-handle position |
Select whether the Y-Axis handle is located on the left or right side of the plot. Only applied after restart. |
adc_plot_xcursor_position |
Plot X-Cursor position |
Select whether the X-Axis cursor handles are located on the top or bottom of the plot. Only applied after restart. |
adc_plot_ycursor_position |
Plot Y-Cursor position |
Select whether the Y-Axis cursor handles are located on the left or right side of the plot. Only applied after restart. |
adc_default_y_mode |
ADC Default Y-Mode |
Select the Y-Axis default mode, can be either ADC Counts or %Full Scale. This is also controllable while running, from the instrument settings. Only applied after restart. |
dac_reset_dds_on_connect |
Reset DDS on connect |
Reset all DDS settings when connecting to the device. Disable if another application is actively using the DDS. |
dac_reset_dds_on_disconnect |
Reset DDS on disconnect |
Reset all DDS settings when disconnecting from the device. Disable if another application needs the DDS to keep running. |
dataloggerplugin_data_storage_size |
Maximum data stored for each monitor |
Select the maximum data storage size for each monitor in the datalogger. |
m2k_instrument_notes_active |
Instrument Notes |
Enable or disable a text section at the bottom of each ADALM2000 instrument, allowing the user to take notes. Disabled by default. |
m2k_debugger_plugin_included |
Include debugger plugin |
Include the Debugger in the current instrument list when connected to an ADALM2000 device. Disabled by default. |
m2k_show_adc_filters |
Show ADC digital filter config |
Enable/disable the configuration panel for ADC digital filters. This allows manual control over the parameters of the filters. |
m2k_show_graticule |
Enable graticule |
Select whether the plot backbone (graticule |
m2k_mini_histogram |
Enable mini histogram |
Select whether the Oscilloscope plot displays a histogram on the right side. |
m2k_osc_filtering |
Enable sample rate filters |
Enable or disable the ADALM2000 ADC filters for all samplerates less than 100 MHz. |
m2k_osc_label |
Enable labels on the plot |
Enable or disable the plot labels in the Oscilloscope instrument. |
m2k_spectrum_visible_peak_search |
Only search marker peaks in visible domain |
Enabled by default, this control allows the Spectrum Analyzer to search for marker peaks outside the visible frequency range. |
m2k_na_show_zero |
Always display 0db value on the graph |
Select whether the 0dB value is displayed as a reference point on the Network Analyzer plot. This control is disabled by default. |
m2k_logic_separate_annotations |
Separate decoder annotations when exporting |
Select whether to export decoder annotations and data separately from the Logic Analyzer instrument. Disabled by default. |
m2k_logic_display_sampling_points |
Display sampling points when zoomed |
Select whether to display each sampling point when zoomed in on the Logic Analyzer. Disabled by default. |
m2k_logic_display_sample_time |
Show sample and time info in decoder table |
Select whether the sample and time detailed information is shown in the decoder table of the Logic Analyzer. Enabled by default. |