CN0511

Description

The CN0511 plugin works with Scopy to control the CN0511 wideband synthesizer board. It communicates with the AD9166 DAC and the AD9166-AMP amplifier via the IIO subsystem.

On connection, the plugin initializes the AD9166 with the FIR85 interpolation filter enabled and a 6 GHz DAC sampling frequency. All output settings (frequency, amplitude, and IOFS calibration coefficients) are written to the device together when the Enter button is clicked.

Use the Refresh button in the top-right corner to read the current NCO frequency back from the hardware and update the displayed value.

The CN0511 view is divided into two sections:

  • Single Tone Mode

  • DAC Amplifier

Single Tone Mode

DAC Amplifier