JIF Tools Quick Start Guide
Get started with the JIF Tools Explorer in minutes!
Installation and Launch
Install pyadi-jif:
pip install 'pyadi-jif[cplex,tools,draw]'
Launch the tools:
jiftools
Access the web interface: The application will open automatically in your browser at
http://localhost:8501
Quick Example 1: Find JESD Modes for AD9680
Goal: Find a 4-lane JESD204B mode for the AD9680 running at 1 GSPS
Steps:
Select Tool: Click “JESD204 Mode Selector” in the sidebar
Select Part: Choose “ad9680” from the dropdown
Configure Datapath:
Decimation: 1
Units: GHz
Converter Rate: 1.0
Filter Modes:
In Configuration section, select L → [4]
In Configuration section, select jesd_class → [“jesd204b”]
View Results:
Check the JESD204 Modes table
Note the lane rate (e.g., 10 Gbps)
Export to CSV if needed
Result: You’ll see valid modes with 4 lanes operating at 1 GSPS, showing parameters like M=2, L=4, F=1, S=1, K=32.
Quick Example 2: Configure HMC7044 for AD9680
Goal: Generate clocks for AD9680 and FPGA reference
Steps:
Select Tool: Click “Clock Configurator” in the sidebar
Select Part: Choose “hmc7044” from the dropdown
Set Reference Clock:
Reference Clock: 125000000 (125 MHz)
Configure Outputs:
Number of Clock Outputs: 2
Output Clock 1: 1000000000 (1 GHz for ADC)
Output Clock 1 Name: “ADC_CLK”
Output Clock 2: 250000000 (250 MHz for FPGA)
Output Clock 2 Name: “FPGA_REF”
View Results:
Configuration appears if valid solution found
Clock tree diagram shows signal routing
Device tree fragment available for Linux
Result: Valid HMC7044 configuration with VCO and divider settings.
Quick Example 3: Complete System Configuration
Goal: Configure complete AD9680 + HMC7044 + Xilinx ZCU102 system
Steps:
Select Tool: Click “System Configurator” in the sidebar
The tool will automatically:
Set up AD9680 converter
Configure HMC7044 clock chip
Set Xilinx FPGA parameters
Use 125 MHz VCXO reference
Configure Settings:
Converter sample clock: 1e9 (1 GSPS)
Decimation: 1
Quick config mode: “0x88”
K: 32
FPGA Setup:
Dev kit: “zc706”
Force QPLL: 1
Solve:
Click solve button
View complete system configuration
Check system block diagram
Result: Complete validated configuration for converter, clock chip, and FPGA transceivers.
Common Tasks
Export JESD Mode Table
Configure filters in JESD Mode Selector
View results table
Click data editor
Use browser to copy/export data
Save Clock Configuration
Generate configuration in Clock Configurator
Copy device tree fragment from output
Save to file for use with Linux drivers
Compare Different Parts
Select first part and note results
Use browser back button or refresh
Select different part
Compare specifications
Tips for Success
Start Simple
Begin with default settings
Add one filter/constraint at a time
Verify each step works before proceeding
Understand Your Requirements
Know your sample rate target
Understand FPGA lane rate limits
Consider available reference clocks
Use Visual Feedback
Check derived settings after each change
Review diagrams to understand signal flow
Toggle valid/invalid modes to see constraints
Iterate
Start with broad filters, then narrow down
Try multiple configurations
Compare trade-offs (lanes vs rate)
Troubleshooting Quick Fixes
“No modes found”
Check: Sample rate within device limits?
Try: Remove some filters
Verify: Decimation/interpolation correct?
“No valid configuration found” (Clock)
Check: Are output frequencies achievable from reference?
Try: Different reference frequency
Verify: Internal VCO ranges compatible?
System solve fails
Check: All components compatible?
Try: Different JESD mode or lane count
Verify: FPGA supports required lane rate?
Application won’t start
Check: Python version (3.9+)
Try: Reinstall with
pip install --force-reinstall 'pyadi-jif[cplex]'Verify: No other Streamlit apps on port 8501
Next Steps
After completing the quick start:
Read Full Documentation: JIF Tools Explorer Guide
Explore Python API: Converter API
Learn About JESD204: Flow Documentation
Advanced Features: Drawing Tools
Getting Help
Documentation: https://developer.analog.com/docs/pyadi-jif/
GitHub Issues: https://github.com/analogdevicesinc/pyadi-jif/issues
ADI Support: https://ez.analog.com/
Examples: Check
examples/directory in repository
Quick Reference
Supported Converters
ADCs: AD9680, AD9625, AD9208, etc.
DACs: AD9144, AD9136, AD9172, etc.
MxFEs: AD9081, AD9082, AD9084, etc.
Transceivers: ADRV9009, ADRV9002, etc.
Supported Clock Chips
HMC7044 - High-performance jitter attenuator
AD9545 - Multi-input clock generator
AD9523-1 - Low jitter clock distribution
Supported FPGAs
Xilinx: 7-series, UltraScale, UltraScale+
Intel (Altera): Arria, Stratix
Common Development Kits
ZC706, ZCU102 (Xilinx)
Various ADI evaluation boards
Ready to get started? Launch the tools with jiftools and try Example 1!