JIF Tools Explorer

The JIF Tools Explorer is an interactive web-based application built with Streamlit that provides a graphical interface for configuring and exploring JESD204 based systems with Analog Devices converters and clock chips.

New to JIF Tools?

Check out the Quick Start Guide for step-by-step examples to get up and running in minutes!

Installation

The JIF Tools Explorer is included with the pyadi-jif package. Install it with:

pip install 'pyadi-jif[cplex]'

For development or to include Streamlit dependencies:

pip install 'pyadi-jif[cplex,tools,draw]'

Launching the Application

Once installed, you can launch the JIF Tools Explorer from the command line:

jiftools

This will start a local web server and automatically open the application in your default web browser. The application typically runs at http://localhost:8501.

Application Overview

The JIF Tools Explorer provides five tools accessible from the sidebar:

  1. JESD204 Mode Selector - Explore and filter JESD204 modes for ADI converters

  2. Clock Configurator - Configure clock distribution chips for your system

  3. System Configurator - Complete end-to-end system configuration (FPGA + Converter + Clock)

  4. ADF4030 System Designer - Plan an Aion (ADF4030) clock-distribution system: pick the cascade / tree / hybrid / hybrid2 architecture and the per-Unit-Board sizing, then view the partition summary and a topology diagram. See Clocking → ADF4030 Architectures for the underlying Python API.

  5. Basic JESD204 Calculator - Calculate lane rate, sample rate, and core clock directly from a small set of JESD204 link parameters


JESD204 Mode Selector

The JESD204 Mode Selector helps you find suitable JESD204 modes for your ADI converter based on your application requirements.

Features

  • Part Selection: Choose from a wide range of ADI converters (ADCs, DACs, MxFEs, Transceivers)

  • Datapath Configuration: Configure decimation/interpolation settings

  • Sample Rate Control: Set converter sample rates with flexible units (Hz, kHz, MHz, GHz)

  • Mode Filtering: Filter JESD204 modes by parameters (M, L, N, Np, F, S, K, HD, CS)

  • Validation: Automatically validates modes against device constraints

  • Visual Diagrams: View clock tree diagrams for ADC converters

  • Export: Export mode tables to CSV

JESD204 Mode Selector showing the AD9680 datapath diagram and configuration controls

The Mode Selector pairs the selected converter’s datapath diagram with the controls that determine its sample rate and JESD204 operating mode.

Usage

1. Select a Converter

From the “Select a part” dropdown, choose your converter. The list includes:

  • ADCs: AD9680, AD9625, etc.

  • DACs: AD9144, AD9136, etc.

  • MxFEs: AD9081, AD9082, etc.

  • Transceivers: adrv9009, etc.

2. Configure Datapath

In the “Datapath Configuration” section:

For ADCs:

  • Set decimation values (CDDC, FDDC if available)

  • Configure converter sample rate

For DACs:

  • Set interpolation values (CDUC, FDUC if available)

  • Configure converter sample rate

3. Set Converter Rate

  1. Select units (Hz, kHz, MHz, or GHz)

  2. Enter the desired converter rate

  3. The derived sample rate will be calculated automatically

4. Filter JESD Modes

Use the multiselect controls in the “Configuration” section to filter modes by JESD204 parameters:

  • M: Number of converters

  • L: Number of lanes

  • N: Converter resolution

  • Np: Number of bits per sample

  • F: Octets per frame

  • S: Samples per converter per frame cycle

  • K: Frames per multiframe

  • HD: High density mode

  • CS: Control bits per sample

5. View Results

The “JESD204 Modes” section displays:

  • Valid modes matching your criteria

  • Lane rates and sample rates for each mode

  • Toggle to show/hide invalid modes

JESD204 Mode Selector filters and valid mode table shown side by side

Filters and matching modes stay side by side, making it easy to compare lane counts, rates, and framing parameters while narrowing the result set.

Example Workflow

# Example: Configure AD9680 for 1 GSPS operation

1. Select part: "AD9680"
2. Set decimation: 1 (no decimation)
3. Set units: GHz
4. Set converter rate: 1.0 GHz
5. Filter by L=4 (4 lanes)
6. Review valid modes in the table
7. Note lane rates for FPGA configuration

Clock Configurator

The Clock Configurator helps you configure ADI clock distribution chips (e.g., HMC7044, AD9545) to generate the required clocks for your system.

Features

  • Multi-Clock Output: Configure multiple output clocks with different frequencies

  • Reference Clock: Set input reference clock frequency

  • Internal Configuration: Control internal clock chip parameters (VCO, dividers, etc.)

  • Visual Diagrams: View generated clock tree diagrams

  • Device Tree Export: Export configuration as device tree fragments (for supported chips)

Clock Configurator showing HMC7044 reference and output clock inputs

The Clock Configurator collects the reference, requested outputs, and optional internal-divider constraints on one page.

Usage

1. Select a Clock Chip

Choose from supported clock chips:

  • HMC7044 - High-performance clock distribution

  • AD9545 - Quad/Octal Clock Generator & Synchronizer

  • And more…

2. Configure Clocks

Reference Clock:

  • Set the input reference clock frequency

Output Clocks:

  1. Specify number of clock outputs needed

  2. For each output:

    • Set the desired frequency

    • Assign a descriptive name (e.g., “ADC_CLK”, “FPGA_REF”)

3. Internal Configuration

Adjust internal parameters if needed:

  • VCO frequency ranges

  • Divider values

  • Distribution settings

The tool will automatically calculate valid configurations.

4. View Results

If a valid configuration is found:

  • Configuration parameters are displayed

  • Clock tree diagram shows the signal flow

  • Device tree fragment (if supported) for Linux driver integration

Solved HMC7044 clock configuration and generated clock tree diagram

The solved divider values are followed by a generated clock tree, so the numeric configuration and signal path can be reviewed together.

Example Workflow

# Example: HMC7044 configuration for AD9680 + FPGA

1. Select part: "hmc7044"
2. Set reference clock: 125 MHz
3. Configure outputs:
   - Output 1: 1000 MHz (name: "ADC_SAMPLE_CLK")
   - Output 2: 250 MHz (name: "FPGA_REF_CLK")
4. Review generated configuration
5. View clock tree diagram
6. Export device tree fragment

System Configurator

The System Configurator provides end-to-end configuration of a complete JESD204 system including FPGA, converter, and clock chip.

Features

  • Complete System: Configure all components together

  • FPGA Integration: Set up FPGA transceiver parameters (Xilinx, Intel)

  • Development Kit Presets: Quick setup for common evaluation boards

  • Automatic Solving: Automatically finds valid configurations across all components

  • System Diagram: Visualize the complete system architecture

System Configurator showing AD9680, HMC7044, ZCU102, converter, and FPGA controls

System-level choices appear first, followed by converter and FPGA controls in parallel columns for an at-a-glance view of the complete setup.

Usage

1. Select Components

Choose:

  • Converter: Your ADI converter (ADC/DAC/MxFE)

  • Clock Chip: Clock distribution chip

  • FPGA: Target FPGA vendor (Xilinx, Intel)

2. Configure Converter

Set converter parameters:

  • Sample clock frequency

  • Decimation/interpolation

  • JESD204 mode

3. Configure FPGA

Select FPGA settings:

  • Development kit (optional)

  • Transceiver type (QPLL/CPLL for Xilinx)

  • Reference clock frequency

4. Set VCXO/Reference

Specify the system reference clock (VCXO) frequency.

5. Solve and View

Click solve to:

  • Calculate complete system configuration

  • Validate all constraints are met

  • Generate system diagram

  • Show configuration for all components

Solved AD9680 HMC7044 ZCU102 system configuration and complete system diagram

The solved JESD204 parameters sit directly above the complete converter, clock, and FPGA signal-flow diagram. This example uses AD9680 quick mode 136 (0x88) with four lanes at 10 Gbps.

Example Workflow

# Example: AD9680 + HMC7044 + Xilinx ZCU102

1. Create system:
   - Converter: "AD9680"
   - Clock: "hmc7044"
   - FPGA: "xilinx"
   - VCXO: 125 MHz

2. Configure converter:
   - Sample rate: 1 GSPS
   - Decimation: 1
   - Mode: 0x88
   - K: 32

3. Configure FPGA:
   - Dev kit: "zcu102"
   - Force QPLL: Yes

4. Solve system

5. View results:
   - Clock configuration
   - Converter settings
   - FPGA transceiver config
   - JESD204 link parameters
   - System block diagram

ADF4030 System Designer

The ADF4030 System Designer helps you plan how Aion (ADF4030) chips chain together to produce SYSREF for large multi-converter systems. Pick an architecture, set the per-Unit-Board sizing, and the page renders the partition summary plus a topology diagram of one Unit Board (or the full system).

Features

  • Four architectures: cascade, tree, hybrid (cascade-of-trees), hybrid2 (tree-of-cascades)

  • Partition summary: per-FPGA / per-Aion / per-Apollo counts, plus the number of Unit Boards required for the total Apollo count

  • Topology diagram: rendered SVG of the Aion / Apollo / FPGA hierarchy with the architecture-appropriate intra-FPGA connections

  • Scope selector: per-Unit-Board (fast) or full system (slower at large N)

ADF4030 System Designer inputs and partition summary

Architecture and board-sizing controls update the partition summary and topology in the same view.

Usage

1. Sizing inputs

  • Total Apollo devices (N): how many Apollo data converters in the system.

  • Apollos per Unit Board: how many Apollos a single board hosts.

  • FPGAs per Unit Board: how many FPGAs partition the Aions on a board.

2. Architecture and branch count

Pick an architecture. For tree, hybrid, and hybrid2, a Branches (N_branch) input appears — that is how many sub-branches the tree fans into.

3. Diagram scope

Toggle between ub (one Unit Board) and system (the full multi-board layout).

4. Review the partition

The “Partition summary” block lists the same fields that the Python Adf4030Architecture.summary property emits, plus the calculated N_UB. The topology diagram below it visualises the selected scope.

ADF4030 Unit Board topology with FPGA, Aion, and Apollo hierarchy

The focused topology view makes the Unit Board, FPGA, Aion, and Apollo hierarchy—and the clock-distribution connections between them—visible without leaving the sizing workflow.

Example Workflow

# Example: 32 Apollo devices, 8 per board, 1 FPGA per board, tree topology
#
# Inputs in the page:
#   N = 32
#   N_Apollo = 8
#   N_FPGA = 1
#   Architecture = tree
#   N_branch = 2
#   Diagram scope = ub
#
# Result:
#   N_Aion_UB = 2 (each board needs 2 Aions: 1 root + 1 leaf)
#   N_UB = 4 (4 boards needed for 32 Apollos)
#   ...plus the topology SVG below the summary.

Basic JESD204 Calculator

The Basic JESD204 Calculator provides a quick link-budget check without loading a converter model or running the constraint solver. Enter the lane count (L), converter count (M), bits per sample (Np), and JESD204 class, then calculate from either a sample rate or a lane rate.

Features

  • Bidirectional rate calculation: derive lane rate from sample rate, or sample rate from lane rate

  • JESD204B/C overhead: applies the appropriate 8b/10b or 64b/66b encoding factor

  • Core clock estimate: reports the link-layer core clock alongside the derived rate

  • No solver required: useful for fast feasibility checks and transceiver budgeting

Basic JESD204 Calculator showing link inputs and derived lane and core clock rates

Inputs and derived parameters share one compact view, making the calculator a quick companion to the Mode Selector and System Configurator.

Example Workflow

  1. Set L=4, M=4, and Np=16.

  2. Select JESD204B and Sample Rate as the reference source.

  3. Enter the converter sample rate.

  4. Read the resulting lane rate and core clock from Derived parameters.


Tips and Best Practices

Performance Optimization

  1. Start Simple: Begin with basic configurations before adding complexity

  2. Use Filters: Narrow down modes early to reduce computation

  3. Valid Modes Toggle: Hide invalid modes to focus on viable options

Common Workflows

Finding Compatible Modes

  1. Set your sample rate requirement

  2. Filter by available lane count

  3. Review lane rates against FPGA capabilities

  4. Select mode with margin for PVT variation

Clock System Design

  1. Identify all required clocks (ADC, FPGA ref, SYSREF, etc.)

  2. Start with reference clock you have available

  3. Configure outputs in priority order

  4. Verify clock quality (jitter, phase noise)

System Integration

  1. Use System Configurator for initial feasibility

  2. Switch to individual tools for fine-tuning

  3. Validate with hardware using exported configurations

Troubleshooting

No valid modes found:

  • Relax filter constraints

  • Check sample rate is within device limits

  • Verify decimation/interpolation settings

Clock configuration fails:

  • Check if output frequencies are achievable with selected reference

  • Verify VCO frequency ranges

  • Try different internal divider settings

System solve fails:

  • Ensure all components are compatible

  • Check FPGA transceiver supports required lane rates

  • Verify reference clock is appropriate for FPGA


API Access

While the JIF Tools Explorer provides a graphical interface, all functionality is also available through the pyadi-jif Python API for scripting and automation:

import adijif

# Example: Programmatic JESD mode search
converter = adijif.AD9680()
converter.sample_clock = 1e9
converter.decimation = 1

# Get valid modes
modes = converter.quick_configuration_modes

# Or use the mode selector
from adijif.utils import get_jesd_mode_from_params
found_modes = get_jesd_mode_from_params(
    converter,
    L=4,
    M=2,
    jesd_class="jesd204b"
)

For more details on the Python API, see the API Documentation.

Technical Details

Architecture

The JIF Tools Explorer is built using:

  • Streamlit: Web application framework

  • pyadi-jif: Core JESD204 configuration library

  • docplex: Constraint solver (CPLEX)

  • D2: Diagram generation

State Management

The application uses Streamlit’s session state to maintain:

  • Part selections across tool switches

  • Configuration values

  • Generated diagrams (cached for performance)

Performance Considerations

  • Diagram generation is cached per part

  • Mode searching is optimized with early filtering

  • Solver constraints are pre-validated


Contributing

To contribute to JIF Tools Explorer:

  1. See Developer Documentation

  2. Test changes with: streamlit run adijif/tools/explorer/main.py

  3. Add tests in tests/tools/

  4. Update documentation as needed

Support

For issues or questions:

  • GitHub Issues: https://github.com/analogdevicesinc/pyadi-jif/issues

  • Documentation: https://developer.analog.com/docs/pyadi-jif/

  • ADI Support: https://ez.analog.com/


See Also