no-OS
Loading...
Searching...
No Matches
oa_tc6_init_param Struct Reference

Holds the initialization parameters for the OA TC6 driver. More...

#include <oa_tc6.h>

Public Attributes

struct no_os_spi_desc * comm_desc
 
enum oa_tc6_bufst_polling bufst_polling
 
bool prote_spi
 

Detailed Description

Holds the initialization parameters for the OA TC6 driver.

Member Data Documentation

◆ bufst_polling

enum oa_tc6_bufst_polling oa_tc6_init_param::bufst_polling

◆ comm_desc

struct no_os_spi_desc* oa_tc6_init_param::comm_desc

◆ prote_spi

bool oa_tc6_init_param::prote_spi

The documentation for this struct was generated from the following file: