no-OS
Loading...
Searching...
No Matches
oa_tc6_desc Struct Reference

Holds the frame buffers and the communication descriptor for the OA TC6 driver. More...

#include <oa_tc6.h>

Public Attributes

struct no_os_spi_desc * comm_desc
 
uint8_t ctrl_chunks [OA_SPI_CTRL_LEN]
 
uint8_t data_chunks [OA_SPI_BUFF_LEN]
 
void * ctrl_lock
 
void * data_lock
 
struct oa_tc6_frame_buffer user_rx_frame_buffer [OA_RX_FRAME_BUFF_NUM]
 
struct oa_tc6_frame_buffer user_tx_frame_buffer [OA_TX_FRAME_BUFF_NUM]
 
uint32_t data_tx_credit
 
uint32_t data_rx_credit
 
uint32_t ctrl_tx_credit
 
uint32_t ctrl_rx_credit
 
enum oa_tc6_bufst_polling bufst_polling
 
struct oa_tc6_flags xfer_flags
 
bool prote_spi
 
struct oa_tc6_stats stats
 
void(* callback )(struct oa_tc6_desc *, uint32_t, void *)
 
void * callback_arg
 
uint32_t pending_events
 

Detailed Description

Holds the frame buffers and the communication descriptor for the OA TC6 driver.

Member Data Documentation

◆ bufst_polling

enum oa_tc6_bufst_polling oa_tc6_desc::bufst_polling

◆ callback

void(* oa_tc6_desc::callback) (struct oa_tc6_desc *, uint32_t, void *)

◆ callback_arg

void* oa_tc6_desc::callback_arg

◆ comm_desc

struct no_os_spi_desc* oa_tc6_desc::comm_desc

◆ ctrl_chunks

uint8_t oa_tc6_desc::ctrl_chunks[OA_SPI_CTRL_LEN]

◆ ctrl_lock

void* oa_tc6_desc::ctrl_lock

◆ ctrl_rx_credit

uint32_t oa_tc6_desc::ctrl_rx_credit

◆ ctrl_tx_credit

uint32_t oa_tc6_desc::ctrl_tx_credit

◆ data_chunks

uint8_t oa_tc6_desc::data_chunks[OA_SPI_BUFF_LEN]

◆ data_lock

void* oa_tc6_desc::data_lock

◆ data_rx_credit

uint32_t oa_tc6_desc::data_rx_credit

◆ data_tx_credit

uint32_t oa_tc6_desc::data_tx_credit

◆ pending_events

uint32_t oa_tc6_desc::pending_events

◆ prote_spi

bool oa_tc6_desc::prote_spi

◆ stats

struct oa_tc6_stats oa_tc6_desc::stats

◆ user_rx_frame_buffer

struct oa_tc6_frame_buffer oa_tc6_desc::user_rx_frame_buffer[OA_RX_FRAME_BUFF_NUM]

◆ user_tx_frame_buffer

struct oa_tc6_frame_buffer oa_tc6_desc::user_tx_frame_buffer[OA_TX_FRAME_BUFF_NUM]

◆ xfer_flags

struct oa_tc6_flags oa_tc6_desc::xfer_flags

The documentation for this struct was generated from the following file: