no-OS
Loading...
Searching...
No Matches
max_gpio_spi_state Struct Reference

Resolved, per-descriptor register view cached at init so the bit loop does no lookups. Stored in no_os_spi_desc.extra. More...

Public Attributes

mxc_gpio_regs_t * gpio
 
uint32_t sclk
 
uint32_t mosi
 
uint32_t miso
 
uint32_t cs
 
uint32_t bus
 
uint32_t all
 
uint32_t half_period_nops
 
uint32_t saved_vssel
 
uint32_t saved_en0
 
uint32_t saved_en1
 
uint32_t saved_en2
 

Detailed Description

Resolved, per-descriptor register view cached at init so the bit loop does no lookups. Stored in no_os_spi_desc.extra.

Member Data Documentation

◆ all

uint32_t max_gpio_spi_state::all

◆ bus

uint32_t max_gpio_spi_state::bus

◆ cs

uint32_t max_gpio_spi_state::cs

◆ gpio

mxc_gpio_regs_t* max_gpio_spi_state::gpio

◆ half_period_nops

uint32_t max_gpio_spi_state::half_period_nops

◆ miso

uint32_t max_gpio_spi_state::miso

◆ mosi

uint32_t max_gpio_spi_state::mosi

◆ saved_en0

uint32_t max_gpio_spi_state::saved_en0

◆ saved_en1

uint32_t max_gpio_spi_state::saved_en1

◆ saved_en2

uint32_t max_gpio_spi_state::saved_en2

◆ saved_vssel

uint32_t max_gpio_spi_state::saved_vssel

◆ sclk

uint32_t max_gpio_spi_state::sclk

The documentation for this struct was generated from the following file: