no-OS
Loading...
Searching...
No Matches
ltc4284_init_param Struct Reference

LTC4284 initialization parameters. More...

#include <ltc4284.h>

Public Attributes

struct no_os_i2c_init_param * i2c_init
 
uint32_t rsense_uohm
 
uint16_t vpwr_divider
 
uint16_t drain_divider
 
uint8_t vsense_mv
 
struct no_os_gpio_init_param * alert_gpio
 

Detailed Description

LTC4284 initialization parameters.

Member Data Documentation

◆ alert_gpio

struct no_os_gpio_init_param* ltc4284_init_param::alert_gpio

◆ drain_divider

uint16_t ltc4284_init_param::drain_divider

◆ i2c_init

struct no_os_i2c_init_param* ltc4284_init_param::i2c_init

◆ rsense_uohm

uint32_t ltc4284_init_param::rsense_uohm

◆ vpwr_divider

uint16_t ltc4284_init_param::vpwr_divider

◆ vsense_mv

uint8_t ltc4284_init_param::vsense_mv

The documentation for this struct was generated from the following file: