![]() |
no-OS
|
ADF4382 Device Descriptor. More...
#include <adf4382.h>
Public Attributes | |
| struct no_os_spi_desc * | spi_desc |
| bool | spi_3wire_en |
| bool | cmos_3v3 |
| uint64_t | ref_freq_hz |
| uint64_t | freq |
| bool | ref_doubler_en |
| uint8_t | ref_div |
| uint8_t | cp_i |
| uint16_t | bleed_word |
| uint8_t | ld_count |
| uint32_t | phase_adj |
| bool | auto_align_en |
| uint8_t | en_lut_gen |
| uint8_t | en_lut_cal |
| uint64_t | vco_max |
| uint64_t | vco_min |
| uint64_t | freq_max |
| uint64_t | freq_min |
| uint8_t | clkout_div_reg_val_max |
| uint8_t | max_lpf_cap_value_uf |
| uint32_t | cal_vtune_to |
| uint16_t | n_int |
ADF4382 Device Descriptor.
| bool adf4382_dev::auto_align_en |
| uint16_t adf4382_dev::bleed_word |
| uint32_t adf4382_dev::cal_vtune_to |
| uint8_t adf4382_dev::clkout_div_reg_val_max |
| bool adf4382_dev::cmos_3v3 |
| uint8_t adf4382_dev::cp_i |
| uint8_t adf4382_dev::en_lut_cal |
| uint8_t adf4382_dev::en_lut_gen |
| uint64_t adf4382_dev::freq |
| uint64_t adf4382_dev::freq_max |
| uint64_t adf4382_dev::freq_min |
| uint8_t adf4382_dev::ld_count |
| uint8_t adf4382_dev::max_lpf_cap_value_uf |
| uint16_t adf4382_dev::n_int |
| uint32_t adf4382_dev::phase_adj |
| uint8_t adf4382_dev::ref_div |
| bool adf4382_dev::ref_doubler_en |
| uint64_t adf4382_dev::ref_freq_hz |
| bool adf4382_dev::spi_3wire_en |
| struct no_os_spi_desc* adf4382_dev::spi_desc |
SPI Descriptor
| uint64_t adf4382_dev::vco_max |
| uint64_t adf4382_dev::vco_min |