no-OS
Loading...
Searching...
No Matches
ad9088_clk_ops Struct Reference

Accessors for the board's device-clock PLL, used by MCS tracking calibration to correct clock drift. More...

#include <ad9088.h>

Public Attributes

void * ctx
 
int(* auto_align_set )(void *ctx, bool en)
 
int(* phase_set_fs )(void *ctx, int32_t phase_fs)
 

Detailed Description

Accessors for the board's device-clock PLL, used by MCS tracking calibration to correct clock drift.

Member Data Documentation

◆ auto_align_set

int(* ad9088_clk_ops::auto_align_set) (void *ctx, bool en)

Re-apply the phase adjustment on every resync rather than once.

◆ ctx

void* ad9088_clk_ops::ctx

Opaque handle passed back to every callback.

◆ phase_set_fs

int(* ad9088_clk_ops::phase_set_fs) (void *ctx, int32_t phase_fs)

Set the signed clock phase adjustment, in fs.


The documentation for this struct was generated from the following file: