no-OS
Loading...
Searching...
No Matches
ad4170_iio_dev_init_param Struct Reference

AD4170 IIO device initialization parameters. More...

#include <iio_ad4170.h>

Public Attributes

struct ad4170_init_param * ad4170_init_param
 
uint32_t vref_mv
 
uint32_t mclk_hz
 

Detailed Description

AD4170 IIO device initialization parameters.

Member Data Documentation

◆ ad4170_init_param

struct ad4170_init_param* ad4170_iio_dev_init_param::ad4170_init_param

AD4170 device initialization parameters.

◆ mclk_hz

uint32_t ad4170_iio_dev_init_param::mclk_hz

Frequency in Hz of the clock wired to XTAL1/XTAL2, ignored when the internal oscillator is selected.

◆ vref_mv

uint32_t ad4170_iio_dev_init_param::vref_mv

Reference voltage in mV, ignored when REFOUT is selected.


The documentation for this struct was generated from the following file: