![]() |
no-OS
|
AD4170 IIO device descriptor. More...
#include <iio_ad4170.h>
Public Attributes | |
| struct ad4170_dev * | ad4170_dev |
| struct iio_device * | iio_dev |
| struct scan_type * | scan_types |
| uint32_t | vref_mv |
| uint32_t | mclk_hz |
| uint32_t | active_channels |
| uint8_t | num_active_channels |
| uint16_t | prev_channel_en |
| enum ad4170_mode | prev_mode |
| bool | prev_multi_data_reg_sel |
AD4170 IIO device descriptor.
| uint32_t ad4170_iio_dev::active_channels |
Mask of the channels enabled by the current buffer.
| struct ad4170_dev* ad4170_iio_dev::ad4170_dev |
AD4170 device descriptor.
| struct iio_device* ad4170_iio_dev::iio_dev |
IIO device descriptor.
| uint32_t ad4170_iio_dev::mclk_hz |
Master clock frequency in Hz the digital filter runs from.
| uint8_t ad4170_iio_dev::num_active_channels |
Number of channels the mask above enables.
| uint16_t ad4170_iio_dev::prev_channel_en |
Channel_En to restore once the buffered read is done.
| enum ad4170_mode ad4170_iio_dev::prev_mode |
Operating mode to restore once the buffered read is done.
| bool ad4170_iio_dev::prev_multi_data_reg_sel |
Data register selection to restore once the buffered read is done.
| struct scan_type* ad4170_iio_dev::scan_types |
Scan type of every IIO channel.
| uint32_t ad4170_iio_dev::vref_mv |
Reference voltage in mV, ignored when REFOUT is selected.