no-OS
Loading...
Searching...
No Matches
powrms_max77986.c File Reference

MAX77985/MAX77986 charger setup for EVAL-POWRMS project. More...

#include "powrms_max77986.h"
#include "no_os_error.h"
#include "no_os_delay.h"
#include "no_os_print_log.h"
Include dependency graph for powrms_max77986.c:

Macros

#define MAX77986_WRITE_DELAY_MS   50
 

Functions

int max77986_init (struct no_os_i2c_desc **desc, const struct no_os_i2c_init_param *param)
 Initialize the MAX77986 over I2C in MODE 6 with maximum current.
 
int max77986_remove (struct no_os_i2c_desc *desc)
 Free the resources allocated by max77986_init().
 

Detailed Description

MAX77985/MAX77986 charger setup for EVAL-POWRMS project.

Author
Robert Budai (rober.nosp@m.t.bu.nosp@m.dai@a.nosp@m.nalo.nosp@m.g.com)

Copyright 2025(c) Analog Devices, Inc.

SPDX-License-Identifier: BSD-3-Clause

Macro Definition Documentation

◆ MAX77986_WRITE_DELAY_MS

#define MAX77986_WRITE_DELAY_MS   50

Function Documentation

◆ max77986_init()

int max77986_init ( struct no_os_i2c_desc ** desc,
const struct no_os_i2c_init_param * param )

Initialize the MAX77986 over I2C in MODE 6 with maximum current.

Brings up the adapter->SYS synchronous buck (no battery) regulated to a fixed 5.0 V with the adapter input current limit set to its maximum (5.5 A). The charger config registers are unlocked first, the voltage and current limits configured, the BATT-to-SYS FET forced off, and MODE = 0x6 enabled last.

Parameters
desc- Will be set to the allocated I2C descriptor on success. The caller owns it and must release it with max77986_remove().
param- I2C bus initialization parameters (slave address 0x6B).
Returns
0 on success, negative error code on failure.

◆ max77986_remove()

int max77986_remove ( struct no_os_i2c_desc * desc)

Free the resources allocated by max77986_init().

Parameters
desc- I2C descriptor returned by max77986_init().
Returns
0 on success, negative error code on failure.