no-OS
Loading...
Searching...
No Matches
powrms_gpios.c File Reference

Button handling implementation for eval-powrms project. More...

#include <stdbool.h>
#include <stdint.h>
#include "powrms_gpios.h"
#include "parameters.h"
#include "no_os_gpio.h"
#include "no_os_error.h"
#include "no_os_delay.h"
#include "no_os_irq.h"
#include "maxim_gpio_irq.h"
#include "example.h"
#include "no_os_print_log.h"
Include dependency graph for powrms_gpios.c:

Macros

#define BTN_ON_OFF_HOLD_MS   250
 
#define BTN_NEXT_FLAG   (1 << 0)
 
#define BTN_BACK_FLAG   (1 << 1)
 
#define BTN_ENTER_FLAG   (1 << 2)
 
#define BTN_ON_OFF_PIN   14
 
#define BTN_BACK_PIN   17
 
#define BTN_NEXT_PIN   16
 
#define BTN_ENTER_PIN   18
 
#define BTN_GPIO_PORT   0
 

Functions

int buttons_init (void)
 Initialize button GPIO pins.
 
int buttons_read (void)
 Read button states with debouncing.
 
void configure_gpios_upon_startup ()
 Configure GPIOs upon system startup.
 
int configure_gpios_upon_shutdown ()
 Configure GPIOs upon system shutdown.
 

Detailed Description

Button handling implementation for eval-powrms project.

Author
Robert Budai (rober.nosp@m.t.bu.nosp@m.dai@a.nosp@m.nalo.nosp@m.g.com)

Copyright 2025(c) Analog Devices, Inc.

SPDX-License-Identifier: BSD-3-Clause

Macro Definition Documentation

◆ BTN_BACK_FLAG

#define BTN_BACK_FLAG   (1 << 1)

◆ BTN_BACK_PIN

#define BTN_BACK_PIN   17

◆ BTN_ENTER_FLAG

#define BTN_ENTER_FLAG   (1 << 2)

◆ BTN_ENTER_PIN

#define BTN_ENTER_PIN   18

◆ BTN_GPIO_PORT

#define BTN_GPIO_PORT   0

◆ BTN_NEXT_FLAG

#define BTN_NEXT_FLAG   (1 << 0)

◆ BTN_NEXT_PIN

#define BTN_NEXT_PIN   16

◆ BTN_ON_OFF_HOLD_MS

#define BTN_ON_OFF_HOLD_MS   250

◆ BTN_ON_OFF_PIN

#define BTN_ON_OFF_PIN   14

Function Documentation

◆ buttons_init()

int buttons_init ( void )

Initialize button GPIO pins.

Initialize interrupt-based button handling.

Configures GPIO pins 0.16, 0.17, and 0.18 as input pins with pull-up resistors for button functionality (NEXT, BACK, ENTER).

Returns
0 on success, negative error code on failure

◆ buttons_read()

int buttons_read ( void )

Read button states with debouncing.

Read button states using interrupt flags.

Reads the current state of all buttons and applies debouncing logic to prevent false triggers from mechanical switch bounce.

Returns
Button press code:
  • 0: No button pressed
  • 1: NEXT button pressed (GPIO 0.17)
  • 2: BACK button pressed (GPIO 0.16)
  • 3: ENTER button pressed (GPIO 0.18)
  • 4: ON_OFF latch held LOW for > 250 ms (GPIO 0.14)

◆ configure_gpios_upon_shutdown()

int configure_gpios_upon_shutdown ( )

Configure GPIOs upon system shutdown.

Safely powers down the system by disabling power rails and setting control signals to their safe states. Finally, triggers a system reset.

Returns
0 on success, negative error code on failure

◆ configure_gpios_upon_startup()

void configure_gpios_upon_startup ( void )

Configure GPIOs upon system startup.

Sets up necessary GPIO pins for system operation, including enabling power rails and setting initial states for control signals.