no-OS
Loading...
Searching...
No Matches
iio_example.h File Reference

IIO example header for LTC4284 project. More...

Functions

int iio_example_main (void)
 IIO example main execution.
 

Detailed Description

IIO example header for LTC4284 project.

Author
Carlos Jones Jr carlo.nosp@m.sjr..nosp@m.jones.nosp@m.@ana.nosp@m.log.c.nosp@m.om
Christopher de Guzman chris.nosp@m.toph.nosp@m.er.de.nosp@m.guzm.nosp@m.an@an.nosp@m.alog.nosp@m..com

Copyright 2026(c) Analog Devices, Inc.

SPDX-License-Identifier: BSD-3-Clause

Function Documentation

◆ iio_example_main()

int iio_example_main ( )

IIO example main execution.

Returns
ret - Result of the example execution. If working correctly, will execute continuously the while(1) loop and will not return.
ret - Result of the example execution. If working correctly, will execute continuously function iio_app_run and will not return.
ret - Result of the example execution. If working correctly, will execute continuously the while(1) loop and will not return.
ret - Result of the example execution. If working correctly, will execute continuously function iio_app_run and will not return.
0 in case of success, negative error code otherwise