![]() |
no-OS
|
Header file of LTC4284 IIO Driver. More...
Classes | |
| struct | ltc4284_iio_desc |
| LTC4284 IIO descriptor. More... | |
| struct | ltc4284_iio_init_param |
| LTC4284 IIO initialization parameters. More... | |
Enumerations | |
| enum | ltc4284_iio_channels { LTC4284_IIO_VIN_CHAN , LTC4284_IIO_IIN_CHAN , LTC4284_IIO_VOUT_CHAN , LTC4284_IIO_POWER_CHAN , LTC4284_IIO_ENERGY_CHAN , LTC4284_IIO_NUM_CHANNELS } |
| LTC4284 IIO channel enumeration. More... | |
Functions | |
| int | ltc4284_iio_init (struct ltc4284_iio_desc **iio_desc, const struct ltc4284_iio_init_param *init_param) |
| Initialize LTC4284 IIO interface. | |
| int | ltc4284_iio_remove (struct ltc4284_iio_desc *desc) |
| Remove LTC4284 IIO interface. | |
Header file of LTC4284 IIO Driver.
Copyright 2026(c) Analog Devices, Inc.
SPDX-License-Identifier: BSD-3-Clause
| enum ltc4284_iio_channels |
| int ltc4284_iio_init | ( | struct ltc4284_iio_desc ** | iio_desc, |
| const struct ltc4284_iio_init_param * | init_param ) |
Initialize LTC4284 IIO interface.
| iio_desc | - Pointer to IIO descriptor pointer |
| init_param | - Initialization parameters |
| int ltc4284_iio_remove | ( | struct ltc4284_iio_desc * | desc | ) |
Remove LTC4284 IIO interface.
| desc | - IIO descriptor |