no-OS
Loading...
Searching...
No Matches
iio_trigger_example.c File Reference

Implementation of IIO trigger example for eval-adis16607 project. More...

#include "iio_adis16607.h"
#include "iio_trigger.h"
#include "iio_app.h"
#include "no_os_pwm.h"
#include "no_os_print_log.h"
#include "common_data.h"
#include "maxim_pwm.h"
Include dependency graph for iio_trigger_example.c:

Macros

#define DATA_BUFFER_SIZE   400
 

Functions

int example_main ()
 IIO trigger example main execution.
 

Variables

uint8_t iio_data_buffer [DATA_BUFFER_SIZE *13 *sizeof(int)]
 

Detailed Description

Implementation of IIO trigger example for eval-adis16607 project.

Author
Radu Sabau (radu..nosp@m.saba.nosp@m.u@ana.nosp@m.log..nosp@m.com)

Copyright 2026(c) Analog Devices, Inc.

SPDX-License-Identifier: BSD-3-Clause

Macro Definition Documentation

◆ DATA_BUFFER_SIZE

#define DATA_BUFFER_SIZE   400

Function Documentation

◆ example_main()

int example_main ( void )

IIO trigger example main execution.

Basic example main execution.

Basic example main executiont.

Returns
ret - Result of the example execution. If working correctly, will execute continuously function iio_app_run_with_trigs and will not return.

IIO descriptor and initialization parameter.

IIO app.

Declaring iio_devices structure

Initializing IIO app init param.

Initializing IIO app.

Running the IIO app (use iio_info or osc in terminal).

Set the threshold voltage to 5V

The comparator output will be available on the GPO_A pin

Set the DAC output on channel C to 5V

Measure input current on channel D

GPIO Pin Interrupt Controller

UART init params

IIO application descriptor

IIO application initialization parameters

iio axi adc configurations.

iio axi dac configurations.

iio instance descriptor.

iio instance descriptor.

iio device instance descriptor.

UART init params

IIO application descriptor

IIO application initialization parameters

iio axi adc configurations.

iio axi dac configurations.

iio instance descriptor.

iio instance descriptor.

iio device instance descriptor.

Negative temperature

Positive temperature

Negative temperature

Positive temperature

Switch to APG mode

Switch to AWG mode

Variable Documentation

◆ iio_data_buffer

uint8_t iio_data_buffer[DATA_BUFFER_SIZE *13 *sizeof(int)]