no-OS
Loading...
Searching...
No Matches
basic_example.c File Reference

BASIC example header for eval-adis16607 project. More...

#include "common_data.h"
#include "adis16607.h"
#include "no_os_delay.h"
#include "no_os_print_log.h"
#include "no_os_units.h"
#include "no_os_util.h"
Include dependency graph for basic_example.c:

Functions

int example_main ()
 Dummy example main execution.
 

Detailed Description

BASIC example header for eval-adis16607 project.

Author
Radu Sabau (radu..nosp@m.saba.nosp@m.u@ana.nosp@m.log..nosp@m.com)

Copyright 2026(c) Analog Devices, Inc.

SPDX-License-Identifier: BSD-3-Clause

Function Documentation

◆ example_main()

int example_main ( void )

Dummy example main execution.

Basic example main execution.

Basic example main executiont.

Returns
ret - Result of the example execution. If working correctly, will execute continuously the while(1) loop and will not return.

IIO descriptor and initialization parameter.

IIO app.

Declaring iio_devices structure

Initializing IIO app init param.

Initializing IIO app.

Running the IIO app (use iio_info or osc in terminal).

Set the threshold voltage to 5V

The comparator output will be available on the GPO_A pin

Set the DAC output on channel C to 5V

Measure input current on channel D

GPIO Pin Interrupt Controller

UART init params

IIO application descriptor

IIO application initialization parameters

iio axi adc configurations.

iio axi dac configurations.

iio instance descriptor.

iio instance descriptor.

iio device instance descriptor.

UART init params

IIO application descriptor

IIO application initialization parameters

iio axi adc configurations.

iio axi dac configurations.

iio instance descriptor.

iio instance descriptor.

iio device instance descriptor.

Negative temperature

Positive temperature

Negative temperature

Positive temperature

Switch to APG mode

Switch to AWG mode