Header for the basic example.
More...
Header for the basic example.
- Author
- Ciprian Regus (cipri.nosp@m.an.r.nosp@m.egus@.nosp@m.anal.nosp@m.og.co.nosp@m.m)
Copyright 2023(c) Analog Devices, Inc.
SPDX-License-Identifier: BSD-3-Clause
◆ basic_example_main()
| int basic_example_main |
( |
| ) |
|
basic example main execution.
- Returns
- ret - Result of the example execution. If working correctly, will execute print the sample data.
basic example main execution.
- Returns
- ret - Result of the example execution. If working correctly, will execute continuously function basic_app_run and will not return.
-
ret - Result of the example execution. If working correctly, will execute print the sample data.
basic example main execution.
- Returns
- ret - Result of the example execution. If working correctly, will execute continuously function basic_app_run and will not return.
basic example main execution.
Demonstrates a full IO-Link communication cycle without an IO-Link stack:
- STARTUP - establish communication, read device identity from DPP
- PREOPERATE - read ISDU parameters (vendor name, serial number, etc.)
- OPERATE - exchange cyclic process data
- Returns
- 0 on success, negative error code otherwise.
basic example main execution.
- Returns
- ret - Result of the example execution.
basic example main execution.
Initialises the UART peripheral, prints a banner, then loops forever printing a counter message once per second.
- Returns
- 0 on success, negative error code on failure.