no-OS
Loading...
Searching...
No Matches
ad9434.h File Reference

Header file of AD9434 Driver. More...

#include <stdint.h>
#include "no_os_delay.h"
#include "no_os_spi.h"
Include dependency graph for ad9434.h:

Classes

struct  ad9434_dev
 
struct  ad9434_init_param
 

Macros

#define AD9434_REG_CHIP_PORT_CONF   0x00
 
#define AD9434_REG_CHIP_ID   0x01
 
#define AD9434_REG_CHIP_GRADE   0x02
 
#define AD9434_REG_CHAN_INDEX   0x05
 
#define AD9434_REG_TRANSFER   0xFF
 
#define AD9434_REG_MODES   0x08
 
#define AD9434_REG_TEST_IO   0x0D
 
#define AD9434_REG_ADC_INPUT   0x0F
 
#define AD9434_REG_OFFSET   0x10
 
#define AD9434_REG_OUTPUT_MODE   0x14
 
#define AD9434_REG_OUTPUT_ADJUST   0x15
 
#define AD9434_REG_OUTPUT_PHASE   0x16
 
#define AD9434_REG_OUTPUT_DELAY   0x17
 
#define AD9434_REG_VREF   0x18
 
#define AD9434_REG_ANALOG_INPUT   0x2C
 
#define TRANSFER_SYNC   0x1
 
#define TESTMODE_OFF   0x0
 
#define TESTMODE_MIDSCALE_SHORT   0x1
 
#define TESTMODE_POS_FULLSCALE   0x2
 
#define TESTMODE_NEG_FULLSCALE   0x3
 
#define TESTMODE_ALT_CHECKERBOARD   0x4
 
#define TESTMODE_PN23_SEQ   0x5
 
#define TESTMODE_PN9_SEQ   0x6
 
#define TESTMODE_ONE_ZERO_TOGGLE   0x7
 
#define TESTMODE_USER_DEFINED   0x8
 
#define OUTPUT_MODE_OFFSET_BINARY   0x0
 
#define OUTPUT_MODE_TWOS_COMPLEMENT   0x1
 
#define OUTPUT_MODE_GRAY_CODE   0x2
 
#define OUTPUT_EVEN_ODD_MODE_EN   0x20
 
#define INVERT_DCO_CLK   0x80
 
#define AD9434_CHIP_ID   0x6A
 
#define AD9434_DEF_OUTPUT_MODE   0x00
 

Functions

int32_t ad9434_spi_read (struct ad9434_dev *dev, uint16_t reg_addr, uint8_t *reg_data)
 ad9434_spi_read
 
int32_t ad9434_spi_write (struct ad9434_dev *dev, uint16_t reg_addr, uint8_t reg_data)
 ad9434_spi_write
 
int32_t ad9434_testmode_set (struct ad9434_dev *dev, uint8_t mode)
 ad9434_testmode_set
 
int32_t ad9434_data_delay (struct ad9434_dev *dev, int16_t delay)
 ad9434_data_delay
 
int32_t ad9434_setup (struct ad9434_dev **device, struct ad9434_init_param init_param)
 ad9434_setup
 
int32_t ad9434_outputmode_set (struct ad9434_dev *dev, uint8_t mode)
 ad9434_setup
 
int32_t ad9434_remove (struct ad9434_dev *dev)
 ad9434_remove
 

Detailed Description

Header file of AD9434 Driver.

Author
DBogdan (drago.nosp@m.s.bo.nosp@m.gdan@.nosp@m.anal.nosp@m.og.co.nosp@m.m)

Copyright 2015(c) Analog Devices, Inc.

SPDX-License-Identifier: BSD-3-Clause

Macro Definition Documentation

◆ AD9434_CHIP_ID

#define AD9434_CHIP_ID   0x6A

◆ AD9434_DEF_OUTPUT_MODE

#define AD9434_DEF_OUTPUT_MODE   0x00

◆ AD9434_REG_ADC_INPUT

#define AD9434_REG_ADC_INPUT   0x0F

◆ AD9434_REG_ANALOG_INPUT

#define AD9434_REG_ANALOG_INPUT   0x2C

◆ AD9434_REG_CHAN_INDEX

#define AD9434_REG_CHAN_INDEX   0x05

◆ AD9434_REG_CHIP_GRADE

#define AD9434_REG_CHIP_GRADE   0x02

◆ AD9434_REG_CHIP_ID

#define AD9434_REG_CHIP_ID   0x01

◆ AD9434_REG_CHIP_PORT_CONF

#define AD9434_REG_CHIP_PORT_CONF   0x00

◆ AD9434_REG_MODES

#define AD9434_REG_MODES   0x08

◆ AD9434_REG_OFFSET

#define AD9434_REG_OFFSET   0x10

◆ AD9434_REG_OUTPUT_ADJUST

#define AD9434_REG_OUTPUT_ADJUST   0x15

◆ AD9434_REG_OUTPUT_DELAY

#define AD9434_REG_OUTPUT_DELAY   0x17

◆ AD9434_REG_OUTPUT_MODE

#define AD9434_REG_OUTPUT_MODE   0x14

◆ AD9434_REG_OUTPUT_PHASE

#define AD9434_REG_OUTPUT_PHASE   0x16

◆ AD9434_REG_TEST_IO

#define AD9434_REG_TEST_IO   0x0D

◆ AD9434_REG_TRANSFER

#define AD9434_REG_TRANSFER   0xFF

◆ AD9434_REG_VREF

#define AD9434_REG_VREF   0x18

◆ INVERT_DCO_CLK

#define INVERT_DCO_CLK   0x80

◆ OUTPUT_EVEN_ODD_MODE_EN

#define OUTPUT_EVEN_ODD_MODE_EN   0x20

◆ OUTPUT_MODE_GRAY_CODE

#define OUTPUT_MODE_GRAY_CODE   0x2

◆ OUTPUT_MODE_OFFSET_BINARY

#define OUTPUT_MODE_OFFSET_BINARY   0x0

◆ OUTPUT_MODE_TWOS_COMPLEMENT

#define OUTPUT_MODE_TWOS_COMPLEMENT   0x1

◆ TESTMODE_ALT_CHECKERBOARD

#define TESTMODE_ALT_CHECKERBOARD   0x4

◆ TESTMODE_MIDSCALE_SHORT

#define TESTMODE_MIDSCALE_SHORT   0x1

◆ TESTMODE_NEG_FULLSCALE

#define TESTMODE_NEG_FULLSCALE   0x3

◆ TESTMODE_OFF

#define TESTMODE_OFF   0x0

◆ TESTMODE_ONE_ZERO_TOGGLE

#define TESTMODE_ONE_ZERO_TOGGLE   0x7

◆ TESTMODE_PN23_SEQ

#define TESTMODE_PN23_SEQ   0x5

◆ TESTMODE_PN9_SEQ

#define TESTMODE_PN9_SEQ   0x6

◆ TESTMODE_POS_FULLSCALE

#define TESTMODE_POS_FULLSCALE   0x2

◆ TESTMODE_USER_DEFINED

#define TESTMODE_USER_DEFINED   0x8

◆ TRANSFER_SYNC

#define TRANSFER_SYNC   0x1

Function Documentation

◆ ad9434_data_delay()

int32_t ad9434_data_delay ( struct ad9434_dev * dev,
int16_t delay )

ad9434_data_delay

◆ ad9434_outputmode_set()

int32_t ad9434_outputmode_set ( struct ad9434_dev * dev,
uint8_t mode )

ad9434_setup

◆ ad9434_remove()

int32_t ad9434_remove ( struct ad9434_dev * dev)

ad9434_remove

◆ ad9434_setup()

int32_t ad9434_setup ( struct ad9434_dev ** device,
struct ad9434_init_param init_param )

ad9434_setup

◆ ad9434_spi_read()

int32_t ad9434_spi_read ( struct ad9434_dev * dev,
uint16_t reg_addr,
uint8_t * reg_data )

ad9434_spi_read

◆ ad9434_spi_write()

int32_t ad9434_spi_write ( struct ad9434_dev * dev,
uint16_t reg_addr,
uint8_t reg_data )

ad9434_spi_write

◆ ad9434_testmode_set()

int32_t ad9434_testmode_set ( struct ad9434_dev * dev,
uint8_t mode )

ad9434_testmode_set