![]() |
no-OS
|
Implementation of AD9361 Driver. More...
#include <limits.h>#include <stdint.h>#include <stdio.h>#include <stdlib.h>#include <string.h>#include <inttypes.h>#include "ad9361.h"#include "ad9361_ext_band_ctrl.h"#include "no_os_spi.h"#include "no_os_gpio.h"#include "no_os_delay.h"#include "ad9361_util.h"#include "no_os_util.h"#include "no_os_alloc.h"#include "app_config.h"Macros | |
| #define | diff_abs(x, y) |
| #define | NO_GAIN_TABLE ((uint32_t)-1) |
| #define | SYNTH_LUT_SIZE 53 |
| #define | SIZE_FULL_TABLE 77 |
| #define | SIZE_SPLIT_TABLE 41 |
| #define | ad9361_spi_readf(spi, reg, mask) |
| #define | ad9361_spi_writef(spi, reg, mask, val) |
Functions | |
| int32_t | ad9361_spi_readm (struct no_os_spi_desc *spi, uint32_t reg, uint8_t *rbuf, uint32_t num) |
| int32_t | ad9361_spi_read (struct no_os_spi_desc *spi, uint32_t reg) |
| int32_t | ad9361_reg_read (struct ad9361_rf_phy *phy, uint32_t reg, uint32_t *val) |
| int32_t | ad9361_spi_write (struct no_os_spi_desc *spi, uint32_t reg, uint32_t val) |
| int32_t | ad9361_reg_write (struct ad9361_rf_phy *phy, uint32_t reg, uint32_t val) |
| uint32_t | ad9361_validate_rf_bw (struct ad9361_rf_phy *phy, uint32_t bw) |
| int32_t | ad9361_validate_rfpll (struct ad9361_rf_phy *phy, bool is_tx, uint64_t freq) |
| int32_t | ad9361_find_opt (uint8_t *field, uint32_t size, uint32_t *ret_start) |
| int32_t | ad9361_1rx1tx_channel_map (struct ad9361_rf_phy *phy, bool tx, int32_t channel) |
| int32_t | ad9361_reset (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_en_dis_tx (struct ad9361_rf_phy *phy, uint32_t tx_if, uint32_t enable) |
| int32_t | ad9361_en_dis_rx (struct ad9361_rf_phy *phy, uint32_t rx_if, uint32_t enable) |
| int32_t | ad9361_bist_loopback (struct ad9361_rf_phy *phy, int32_t mode) |
| void | ad9361_get_bist_loopback (struct ad9361_rf_phy *phy, int32_t *mode) |
| int32_t | ad9361_bist_prbs (struct ad9361_rf_phy *phy, enum ad9361_bist_mode mode) |
| void | ad9361_get_bist_prbs (struct ad9361_rf_phy *phy, enum ad9361_bist_mode *mode) |
| int32_t | ad9361_bist_tone (struct ad9361_rf_phy *phy, enum ad9361_bist_mode mode, uint32_t freq_Hz, uint32_t level_dB, uint32_t mask) |
| void | ad9361_get_bist_tone (struct ad9361_rf_phy *phy, enum ad9361_bist_mode *mode, uint32_t *freq_Hz, uint32_t *level_dB, uint32_t *mask) |
| uint32_t | ad9361_gt (struct ad9361_rf_phy *phy) |
| uint32_t | ad9361_to_clk (uint64_t freq) |
| uint64_t | ad9361_from_clk (uint32_t freq) |
| int32_t | ad9361_set_tx_atten (struct ad9361_rf_phy *phy, uint32_t atten_mdb, bool tx1, bool tx2, bool immed) |
| int32_t | ad9361_get_tx_atten (struct ad9361_rf_phy *phy, uint32_t tx_num) |
| int32_t | ad9361_tx_mute (struct ad9361_rf_phy *phy, uint32_t state) |
| int32_t | ad9361_get_rx_gain (struct ad9361_rf_phy *phy, uint32_t rx_id, struct rf_rx_gain *rx_gain) |
| uint8_t | ad9361_ensm_get_state (struct ad9361_rf_phy *phy) |
| void | ad9361_ensm_force_state (struct ad9361_rf_phy *phy, uint8_t ensm_state) |
| void | ad9361_ensm_restore_state (struct ad9361_rf_phy *phy, uint8_t ensm_state) |
| void | ad9361_ensm_restore_prev_state (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_set_rx_gain (struct ad9361_rf_phy *phy, uint32_t rx_id, struct rf_rx_gain *rx_gain) |
| int32_t | ad9361_set_gain_ctrl_mode (struct ad9361_rf_phy *phy, struct rf_gain_ctrl *gain_ctrl) |
| int32_t | ad9361_read_rssi (struct ad9361_rf_phy *phy, struct rf_rssi *rssi) |
| int32_t | ad9361_tracking_control (struct ad9361_rf_phy *phy, bool bbdc_track, bool rfdc_track, bool rxquad_track) |
| int | ad9361_synth_lo_powerdown (struct ad9361_rf_phy *phy, enum synth_pd_ctrl rx, enum synth_pd_ctrl tx) |
| int32_t | ad9361_set_dcxo_tune (struct ad9361_rf_phy *phy, uint32_t coarse, uint32_t fine) |
| int32_t | ad9361_rf_port_setup (struct ad9361_rf_phy *phy, bool is_out, uint32_t rx_inputs, uint32_t txb) |
| int32_t | ad9361_auxdac_get (struct ad9361_rf_phy *phy, int32_t dac) |
| int32_t | ad9361_get_auxadc (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_ensm_set_state (struct ad9361_rf_phy *phy, uint8_t ensm_state, bool pinctrl) |
| int32_t | ad9361_set_trx_clock_chain (struct ad9361_rf_phy *phy, uint32_t *rx_path_clks, uint32_t *tx_path_clks) |
| int32_t | ad9361_get_trx_clock_chain (struct ad9361_rf_phy *phy, uint32_t *rx_path_clks, uint32_t *tx_path_clks) |
| int32_t | ad9361_calculate_rf_clock_chain (struct ad9361_rf_phy *phy, uint32_t tx_sample_rate, uint32_t rate_gov, uint32_t *rx_path_clks, uint32_t *tx_path_clks) |
| int32_t | ad9361_set_trx_clock_chain_freq (struct ad9361_rf_phy *phy, uint32_t freq) |
| int32_t | ad9361_set_ensm_mode (struct ad9361_rf_phy *phy, bool fdd, bool pinctrl) |
| int32_t | ad9361_fastlock_load (struct ad9361_rf_phy *phy, bool tx, uint32_t profile, uint8_t *values) |
| int32_t | ad9361_fastlock_store (struct ad9361_rf_phy *phy, bool tx, uint32_t profile) |
| int32_t | ad9361_fastlock_exit_foreign (struct ad9361_rf_phy *phy, bool tx) |
| int32_t | ad9361_fastlock_recall (struct ad9361_rf_phy *phy, bool tx, uint32_t profile) |
| int32_t | ad9361_fastlock_save (struct ad9361_rf_phy *phy, bool tx, uint32_t profile, uint8_t *values) |
| int32_t | ad9361_mcs (struct ad9361_rf_phy *phy, int32_t step) |
| void | ad9361_clear_state (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_setup (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_do_calib_run (struct ad9361_rf_phy *phy, uint32_t cal, int32_t arg) |
| int32_t | ad9361_update_rf_bandwidth (struct ad9361_rf_phy *phy, uint32_t rf_rx_bw, uint32_t rf_tx_bw) |
| int32_t | ad9361_load_fir_filter_coef (struct ad9361_rf_phy *phy, enum fir_dest dest, int32_t gain_dB, uint32_t ntaps, int16_t *coef) |
| int32_t | ad9361_parse_fir (struct ad9361_rf_phy *phy, char *data, uint32_t size) |
| int32_t | ad9361_validate_enable_fir (struct ad9361_rf_phy *phy) |
| uint32_t | ad9361_clk_factor_recalc_rate (struct refclk_scale *clk_priv, uint32_t parent_rate) |
| int32_t | ad9361_clk_factor_round_rate (struct refclk_scale *clk_priv, uint32_t rate, uint32_t *prate) |
| int32_t | ad9361_clk_factor_set_rate (struct refclk_scale *clk_priv, uint32_t rate, uint32_t parent_rate) |
| uint32_t | ad9361_bbpll_recalc_rate (struct refclk_scale *clk_priv, uint32_t parent_rate) |
| int32_t | ad9361_bbpll_round_rate (struct refclk_scale *clk_priv, uint32_t rate, uint32_t *prate) |
| int32_t | ad9361_bbpll_set_rate (struct refclk_scale *clk_priv, uint32_t rate, uint32_t parent_rate) |
| uint32_t | ad9361_rfpll_int_recalc_rate (struct refclk_scale *clk_priv, uint32_t parent_rate) |
| int32_t | ad9361_rfpll_int_round_rate (struct refclk_scale *clk_priv, uint32_t rate, uint32_t *prate) |
| int32_t | ad9361_rfpll_int_set_rate (struct refclk_scale *clk_priv, uint32_t rate, uint32_t parent_rate) |
| uint32_t | ad9361_rfpll_dummy_recalc_rate (struct refclk_scale *clk_priv) |
| int32_t | ad9361_rfpll_dummy_set_rate (struct refclk_scale *clk_priv, uint32_t rate) |
| uint32_t | ad9361_rfpll_recalc_rate (struct refclk_scale *clk_priv) |
| int32_t | ad9361_rfpll_round_rate (struct refclk_scale *clk_priv, uint32_t rate) |
| int32_t | ad9361_rfpll_set_rate (struct refclk_scale *clk_priv, uint32_t rate) |
| int32_t | ad9361_clk_mux_set_parent (struct refclk_scale *clk_priv, uint8_t index) |
| int32_t | ad9361_register_clocks (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_unregister_clocks (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_rssi_gain_step_calib (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_rssi_program_lna_gain (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_rssi_write_err_tbl (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_read_clock_data_delays (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_write_clock_data_delays (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_get_dig_tune_data (struct ad9361_rf_phy *phy, struct ad9361_dig_tune_data *data) |
| int32_t | ad9361_write_bist_reg (struct ad9361_rf_phy *phy, uint32_t val) |
| int32_t | ad9361_ensm_mode_disable_pinctrl (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_ensm_mode_restore_pinctrl (struct ad9361_rf_phy *phy) |
| int32_t | ad9361_set_cal_sw (struct ad9361_rf_phy *phy, uint32_t val) |
Variables | |
| const bool | has_split_gt = HAVE_SPLIT_GAIN_TABLE |
| struct gain_table_info | ad9361_adi_gt_info [] |
| const char * | ad9361_ensm_states [] |
Implementation of AD9361 Driver.
Copyright 2014-2015(c) Analog Devices, Inc.
SPDX-License-Identifier: BSD-3-Clause
| #define ad9361_spi_readf | ( | spi, | |
| reg, | |||
| mask ) |
SPI register bits read.
| spi | |
| reg | The register address. |
| mask | The bits mask. |
| #define ad9361_spi_writef | ( | spi, | |
| reg, | |||
| mask, | |||
| val ) |
SPI register bits write.
| spi | |
| reg | The register address. |
| mask | The bits mask. |
| val | The bits value. |
| #define diff_abs | ( | x, | |
| y ) |
| #define NO_GAIN_TABLE ((uint32_t)-1) |
| #define SIZE_FULL_TABLE 77 |
| #define SIZE_SPLIT_TABLE 41 |
| #define SYNTH_LUT_SIZE 53 |
| int32_t ad9361_1rx1tx_channel_map | ( | struct ad9361_rf_phy * | phy, |
| bool | tx, | ||
| int32_t | channel ) |
Select the channel mapping in 1rx1tx mode.
| phy | The AD9361 state structure. |
| tx | TX |
| channel | Channel |
| int32_t ad9361_auxdac_get | ( | struct ad9361_rf_phy * | phy, |
| int32_t | dac ) |
Get the Aux DAC value.
| phy | The AD9361 state structure. |
| dac | The DAC. |
| uint32_t ad9361_bbpll_recalc_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | parent_rate ) |
Recalculate the clock rate.
| clk_priv | The refclk_scale structure. |
| parent_rate | The parent clock rate. |
| int32_t ad9361_bbpll_round_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | rate, | ||
| uint32_t * | prate ) |
Calculate the closest possible clock rate that can be set.
| clk_priv | The refclk_scale structure. |
| rate | The clock rate. |
| prate | The parent clock rate. |
| int32_t ad9361_bbpll_set_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | rate, | ||
| uint32_t | parent_rate ) |
Set the clock rate.
| clk_priv | The refclk_scale structure. |
| rate | The clock rate. |
| parent_rate | The parent clock rate. |
| int32_t ad9361_bist_loopback | ( | struct ad9361_rf_phy * | phy, |
| int32_t | mode ) |
BIST loopback mode.
| phy | The AD9361 state structure. |
| mode | BIST loopback mode. |
| int32_t ad9361_bist_prbs | ( | struct ad9361_rf_phy * | phy, |
| enum ad9361_bist_mode | mode ) |
BIST mode.
| phy | The AD9361 state structure. |
| mode | Bist mode. |
| int32_t ad9361_bist_tone | ( | struct ad9361_rf_phy * | phy, |
| enum ad9361_bist_mode | mode, | ||
| uint32_t | freq_Hz, | ||
| uint32_t | level_dB, | ||
| uint32_t | mask ) |
BIST tone.
| phy | The AD9361 state structure. |
| mode | Bist tone mode. |
| freq_Hz | Bist tone frequency. |
| level_dB | Bist tone level. |
| mask | Bist reg mask. |
| int32_t ad9361_calculate_rf_clock_chain | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | tx_sample_rate, | ||
| uint32_t | rate_gov, | ||
| uint32_t * | rx_path_clks, | ||
| uint32_t * | tx_path_clks ) |
Calculate the RX and TX path rates to obtain the desired sample rate.
| phy | The AD9361 state structure. |
| tx_sample_rate | The desired sample rate. |
| rate_gov | The rate governor option. |
| rx_path_clks | RX path rates buffer. |
| tx_path_clks | TX path rates buffer. |
| void ad9361_clear_state | ( | struct ad9361_rf_phy * | phy | ) |
Clear state.
| phy | The AD9361 state structure. |
| uint32_t ad9361_clk_factor_recalc_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | parent_rate ) |
Recalculate the clock rate.
| clk_priv | The refclk_scale structure. |
| parent_rate | The parent clock rate. |
| int32_t ad9361_clk_factor_round_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | rate, | ||
| uint32_t * | prate ) |
Calculate the closest possible clock rate that can be set.
| clk_priv | The refclk_scale structure. |
| rate | The clock rate. |
| prate | The parent clock rate. |
| int32_t ad9361_clk_factor_set_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | rate, | ||
| uint32_t | parent_rate ) |
Set the clock rate.
| clk_priv | The refclk_scale structure. |
| rate | The clock rate. |
| parent_rate | The parent clock rate. |
| int32_t ad9361_clk_mux_set_parent | ( | struct refclk_scale * | clk_priv, |
| uint8_t | index ) |
Set clock mux parent.
| clk_priv | The refclk_scale structure. |
| index | Index - Enable (1) external LO, disable (0) = use internal PLL. |
| int32_t ad9361_do_calib_run | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | cal, | ||
| int32_t | arg ) |
Perform the selected calibration
| phy | The AD9361 state structure. |
| cal | The selected calibration. |
| arg | The argument of the calibration. |
| int32_t ad9361_en_dis_rx | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | rx_if, | ||
| uint32_t | enable ) |
Enable/disable the desired RX channel.
| phy | The AD9361 state structure. |
| rx_if | The desired channel number [1, 2]. |
| enable | Enable/disable option. |
| int32_t ad9361_en_dis_tx | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | tx_if, | ||
| uint32_t | enable ) |
Enable/disable the desired TX channel.
| phy | The AD9361 state structure. |
| tx_if | The desired channel number [1, 2]. |
| enable | Enable/disable option. |
| void ad9361_ensm_force_state | ( | struct ad9361_rf_phy * | phy, |
| uint8_t | ensm_state ) |
Force Enable State Machine (ENSM) to the desired state (internally used only).
| phy | The AD9361 state structure. |
| ensm_state | The ENSM state [ENSM_STATE_SLEEP_WAIT, ENSM_STATE_ALERT, ENSM_STATE_TX, ENSM_STATE_TX_FLUSH, ENSM_STATE_RX, ENSM_STATE_RX_FLUSH, ENSM_STATE_FDD, ENSM_STATE_FDD_FLUSH]. |
| uint8_t ad9361_ensm_get_state | ( | struct ad9361_rf_phy * | phy | ) |
Get Enable State Machine (ENSM) state.
| phy | The AD9361 state structure. |
| int32_t ad9361_ensm_mode_disable_pinctrl | ( | struct ad9361_rf_phy * | phy | ) |
Temporarily disable ENSM pin control by forcing TDD SPI mode. Useful before calibration sequences that must use SPI-driven state.
| phy | The AD9361 state structure. |
| int32_t ad9361_ensm_mode_restore_pinctrl | ( | struct ad9361_rf_phy * | phy | ) |
Restore ENSM pin control to the state configured in pdata.
| phy | The AD9361 state structure. |
| void ad9361_ensm_restore_prev_state | ( | struct ad9361_rf_phy * | phy | ) |
Restore the previous Enable State Machine (ENSM) state.
| phy | The AD9361 state structure. |
| void ad9361_ensm_restore_state | ( | struct ad9361_rf_phy * | phy, |
| uint8_t | ensm_state ) |
Restore an Enable State Machine (ENSM) state.
| phy | The AD9361 state structure. |
| ensm_state | The state. |
| int32_t ad9361_ensm_set_state | ( | struct ad9361_rf_phy * | phy, |
| uint8_t | ensm_state, | ||
| bool | pinctrl ) |
Set the desired Enable State Machine (ENSM) state.
| phy | The AD9361 state structure. |
| ensm_state | The ENSM state [ENSM_STATE_SLEEP_WAIT, ENSM_STATE_ALERT, ENSM_STATE_TX, ENSM_STATE_TX_FLUSH, ENSM_STATE_RX, ENSM_STATE_RX_FLUSH, ENSM_STATE_FDD, ENSM_STATE_FDD_FLUSH]. |
| pinctrl | Set true, will enable the ENSM pin control. |
| int32_t ad9361_fastlock_exit_foreign | ( | struct ad9361_rf_phy * | phy, |
| bool | tx ) |
Leave fastlock mode when it was entered outside this driver.
A fast lock profile can be recalled by an agent this driver does not see (on a bladeRF 2.0 micro, the FPGA's Nios core). current_profile stays zero, so ad9361_fastlock_prepare() never runs its exit sequence and later tuning programs the RFPLL with FORCE_ALC_ENABLE still asserted, which shows up as a lock failure with the charge pump saturated.
Writes nothing when the part is not in fastlock, so it may be called unconditionally; every path that programs the synthesiser should, since a foreign recall is asynchronous and the leak surfaces on the next tune.
| phy | The AD9361 state structure. |
| tx | True for TX, false for RX. |
| int32_t ad9361_fastlock_load | ( | struct ad9361_rf_phy * | phy, |
| bool | tx, | ||
| uint32_t | profile, | ||
| uint8_t * | values ) |
Fastlock load values.
| phy | The AD9361 state structure. |
| tx | |
| profile | |
| values |
| int32_t ad9361_fastlock_recall | ( | struct ad9361_rf_phy * | phy, |
| bool | tx, | ||
| uint32_t | profile ) |
Fastlock recall.
| phy | The AD9361 state structure. |
| tx | |
| profile |
| int32_t ad9361_fastlock_save | ( | struct ad9361_rf_phy * | phy, |
| bool | tx, | ||
| uint32_t | profile, | ||
| uint8_t * | values ) |
Fastlock save.
| phy | The AD9361 state structure. |
| tx | |
| profile | |
| values |
| int32_t ad9361_fastlock_store | ( | struct ad9361_rf_phy * | phy, |
| bool | tx, | ||
| uint32_t | profile ) |
Fastlock store.
| phy | The AD9361 state structure. |
| tx | |
| profile |
| int32_t ad9361_find_opt | ( | uint8_t * | field, |
| uint32_t | size, | ||
| uint32_t * | ret_start ) |
Find optimal value.
| field | |
| size | |
| ret_start |
| uint64_t ad9361_from_clk | ( | uint32_t | freq | ) |
Shift back the frequency value, so it reflects the real value. Note: PLL operates between 47 .. 6000 MHz which is > 2^32.
| freq | The frequency value [Hz]. |
| int32_t ad9361_get_auxadc | ( | struct ad9361_rf_phy * | phy | ) |
Get the Aux ADC value.
| phy | The AD9361 state structure. |
| void ad9361_get_bist_loopback | ( | struct ad9361_rf_phy * | phy, |
| int32_t * | mode ) |
Get BIST loopback mode.
| phy | The AD9361 state structure. |
| mode | BIST loopback mode. |
| void ad9361_get_bist_prbs | ( | struct ad9361_rf_phy * | phy, |
| enum ad9361_bist_mode * | mode ) |
Get BIST mode settings.
| phy | The AD9361 state structure. |
| mode | Bist mode. |
| void ad9361_get_bist_tone | ( | struct ad9361_rf_phy * | phy, |
| enum ad9361_bist_mode * | mode, | ||
| uint32_t * | freq_Hz, | ||
| uint32_t * | level_dB, | ||
| uint32_t * | mask ) |
Get BIST tone settings.
| phy | The AD9361 state structure. |
| mode | Bist tone mode. |
| freq_Hz | Bist tone frequency. |
| level_dB | Bist tone level. |
| mask | Bist reg mask. |
| int32_t ad9361_get_dig_tune_data | ( | struct ad9361_rf_phy * | phy, |
| struct ad9361_dig_tune_data * | data ) |
Return the current digital interface tuning state.
| phy | The AD9361 state structure. |
| data | Output: populated with skip_mode and current delay register values. |
| int32_t ad9361_get_rx_gain | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | rx_id, | ||
| struct rf_rx_gain * | rx_gain ) |
Get current RX gain for the selected channel.
| phy | The AD9361 state structure. |
| rx_id | The desired channel number (0, 1). |
| rx_gain | A rf_rx_gain struct to store the RF gain. |
| int32_t ad9361_get_trx_clock_chain | ( | struct ad9361_rf_phy * | phy, |
| uint32_t * | rx_path_clks, | ||
| uint32_t * | tx_path_clks ) |
Get the RX and TX path rates.
| phy | The AD9361 state structure. |
| rx_path_clks | RX path rates buffer. |
| tx_path_clks | TX path rates buffer. |
| int32_t ad9361_get_tx_atten | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | tx_num ) |
Get the attenuation for the selected TX channel.
| phy | The AD9361 state structure. |
| tx_num | The selected channel [1, 2]. |
| uint32_t ad9361_gt | ( | struct ad9361_rf_phy * | phy | ) |
Return the current gain table index.
| phy | The AD9361 state structure. |
| int32_t ad9361_load_fir_filter_coef | ( | struct ad9361_rf_phy * | phy, |
| enum fir_dest | dest, | ||
| int32_t | gain_dB, | ||
| uint32_t | ntaps, | ||
| int16_t * | coef ) |
Load the FIR filter coefficients.
| phy | The AD9361 state structure. |
| dest | Destination identifier (RX1,2 / TX1,2). |
| gain_dB | Gain option. |
| ntaps | Number of filter Taps. |
| coef | Pointer to filter coefficients. |
| int32_t ad9361_mcs | ( | struct ad9361_rf_phy * | phy, |
| int32_t | step ) |
Multi Chip Sync (MCS) config.
| phy | The AD9361 state structure. |
| step | MCS step. |
| int32_t ad9361_parse_fir | ( | struct ad9361_rf_phy * | phy, |
| char * | data, | ||
| uint32_t | size ) |
Parse the FIR filter file/buffer.
| phy | The AD9361 state structure. |
| data | Pointer to buffer. |
| size | Buffer size. |
| int32_t ad9361_read_clock_data_delays | ( | struct ad9361_rf_phy * | phy | ) |
Read the current RX and TX clock/data delay register values back into pdata. Call this after ad9361_dig_tune() to persist the tuned values.
| phy | The AD9361 state structure. |
| int32_t ad9361_read_rssi | ( | struct ad9361_rf_phy * | phy, |
| struct rf_rssi * | rssi ) |
Get the RSSI.
| phy | The AD9361 state structure. |
| rssi | A rf_rssi struct to store the RSSI. |
| int32_t ad9361_reg_read | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | reg, | ||
| uint32_t * | val ) |
IIO SPI register read.
| phy | The AD9361 state structure. |
| reg | The register address. |
| val | The value read from register address. |
| int32_t ad9361_reg_write | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | reg, | ||
| uint32_t | val ) |
IIO SPI register write.
| phy | The AD9361 state structure. |
| reg | The register address. |
| val | The value of the register. |
| int32_t ad9361_register_clocks | ( | struct ad9361_rf_phy * | phy | ) |
Register and initialize all the system clocks.
| phy | The AD9361 state structure. |
| int32_t ad9361_reset | ( | struct ad9361_rf_phy * | phy | ) |
AD9361 Device Reset
| phy | The AD9361 state structure. |
| int32_t ad9361_rf_port_setup | ( | struct ad9361_rf_phy * | phy, |
| bool | is_out, | ||
| uint32_t | rx_inputs, | ||
| uint32_t | txb ) |
Setup the RF port. Note: val 0 (RX1A_N & RX1A_P) and (RX2A_N & RX2A_P) enabled; balanced 1 (RX1B_N & RX1B_P) and (RX2B_N & RX2B_P) enabled; balanced 2 (RX1C_N & RX1C_P) and (RX2C_N & RX2C_P) enabled; balanced
3 RX1A_N and RX2A_N enabled; unbalanced 4 RX1A_P and RX2A_P enabled; unbalanced 5 RX1B_N and RX2B_N enabled; unbalanced 6 RX1B_P and RX2B_P enabled; unbalanced 7 RX1C_N and RX2C_N enabled; unbalanced 8 RX1C_P and RX2C_P enabled; unbalanced 9 TX_MON1 10 TX_MON2 11 TX_MON1 & TX_MON2
| phy | The AD9361 state structure. |
| is_out | TX RF output port enabled. |
| rx_inputs | RX input option identifier |
| txb | TX output option identifier |
| uint32_t ad9361_rfpll_dummy_recalc_rate | ( | struct refclk_scale * | clk_priv | ) |
| int32_t ad9361_rfpll_dummy_set_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | rate ) |
Set the clock rate.
| clk_priv | The refclk_scale structure. |
| rate | The clock rate. |
| uint32_t ad9361_rfpll_int_recalc_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | parent_rate ) |
Recalculate the clock rate.
| clk_priv | The refclk_scale structure. |
| parent_rate | The parent clock rate. |
| int32_t ad9361_rfpll_int_round_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | rate, | ||
| uint32_t * | prate ) |
Calculate the closest possible clock rate that can be set.
| clk_priv | The refclk_scale structure. |
| rate | The clock rate. |
| prate | The parent clock rate. |
| int32_t ad9361_rfpll_int_set_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | rate, | ||
| uint32_t | parent_rate ) |
Set the clock rate.
| clk_priv | The refclk_scale structure. |
| rate | The clock rate. |
| parent_rate | The parent clock rate. |
| uint32_t ad9361_rfpll_recalc_rate | ( | struct refclk_scale * | clk_priv | ) |
| int32_t ad9361_rfpll_round_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | rate ) |
Calculate the closest possible clock rate that can be set.
| clk_priv | The refclk_scale structure. |
| rate | The clock rate. |
| int32_t ad9361_rfpll_set_rate | ( | struct refclk_scale * | clk_priv, |
| uint32_t | rate ) |
Set the clock rate.
| clk_priv | The refclk_scale structure. |
| rate | The clock rate. |
| int32_t ad9361_rssi_gain_step_calib | ( | struct ad9361_rf_phy * | phy | ) |
Perform an RSSI gain step calibration. Note: Before running the function, provide a single tone within the channel bandwidth and monitor the received data. Adjust the tone amplitude until the received data is within a few dB of full scale but not overloading.
| phy | The AD9361 state structure. |
| int32_t ad9361_rssi_program_lna_gain | ( | struct ad9361_rf_phy * | phy | ) |
Program the LNA gain step values from pdata->rssi_gain_step_calib_reg_val into the AD9361 gain-step calibration table.
| phy | The AD9361 state structure. |
| int32_t ad9361_rssi_write_err_tbl | ( | struct ad9361_rf_phy * | phy | ) |
Write the pre-loaded LNA and mixer error tables from pdata into hardware.
| phy | The AD9361 state structure. |
| int32_t ad9361_set_cal_sw | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | val ) |
Drive the external calibration switch GPIOs (cal-sw1, cal-sw2). Bit 0 of val controls cal-sw1, bit 1 controls cal-sw2. These GPIOs route signals for TX quad / LO calibration on boards that have external calibration switch hardware.
| phy | The AD9361 state structure. |
| val | 2-bit value: bit0 = cal_sw1, bit1 = cal_sw2. |
| int32_t ad9361_set_dcxo_tune | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | coarse, | ||
| uint32_t | fine ) |
Setup the DCXO tune.
| phy | The AD9361 state structure. |
| coarse | The DCXO tune coarse. |
| fine | The DCXO tune fine. |
| int32_t ad9361_set_ensm_mode | ( | struct ad9361_rf_phy * | phy, |
| bool | fdd, | ||
| bool | pinctrl ) |
Internal ENSM mode options helper function.
| phy | The AD9361 state structure. |
| fdd | |
| pinctrl |
| int32_t ad9361_set_gain_ctrl_mode | ( | struct ad9361_rf_phy * | phy, |
| struct rf_gain_ctrl * | gain_ctrl ) |
Set the gain control mode.
| phy | The AD9361 state structure. |
| gain_ctrl | A rf_gain_ctrl struct that contains the the desired channel information and the gain control mode. |
| int32_t ad9361_set_rx_gain | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | rx_id, | ||
| struct rf_rx_gain * | rx_gain ) |
Set the RX gain for the selected channel.
| phy | The AD9361 state structure. |
| rx_id | The desired channel number (0, 1). |
| rx_gain | The rf_rx_gain struct containing the RF gain. |
| int32_t ad9361_set_trx_clock_chain | ( | struct ad9361_rf_phy * | phy, |
| uint32_t * | rx_path_clks, | ||
| uint32_t * | tx_path_clks ) |
Set the RX and TX path rates.
| phy | The AD9361 state structure. |
| rx_path_clks | RX path rates buffer. |
| tx_path_clks | TX path rates buffer. |
| int32_t ad9361_set_trx_clock_chain_freq | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | freq ) |
Set the desired sample rate.
| phy | The AD9361 state structure. |
| freq | The desired sample rate. |
| int32_t ad9361_set_tx_atten | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | atten_mdb, | ||
| bool | tx1, | ||
| bool | tx2, | ||
| bool | immed ) |
Set the attenuation for the selected TX channels.
| phy | The AD9361 state structure. |
| atten_mdb | Attenuation value [mdB]. |
| tx1 | Set true, the attenuation of the TX1 will be affected. |
| tx2 | Set true, the attenuation of the TX2 will be affected. |
| immed | Set true, an immediate update will take place. |
| int32_t ad9361_setup | ( | struct ad9361_rf_phy * | phy | ) |
Setup the AD9361 device.
| phy | The AD9361 state structure. |
| int32_t ad9361_spi_read | ( | struct no_os_spi_desc * | spi, |
| uint32_t | reg ) |
SPI register read.
| spi | |
| reg | The register address. |
| int32_t ad9361_spi_readm | ( | struct no_os_spi_desc * | spi, |
| uint32_t | reg, | ||
| uint8_t * | rbuf, | ||
| uint32_t | num ) |
SPI multiple bytes register read.
| spi | |
| reg | The register address. |
| rbuf | The data buffer. |
| num | The number of bytes to read. |
| int32_t ad9361_spi_write | ( | struct no_os_spi_desc * | spi, |
| uint32_t | reg, | ||
| uint32_t | val ) |
SPI register write.
| spi | |
| reg | The register address. |
| val | The value of the register. |
| int ad9361_synth_lo_powerdown | ( | struct ad9361_rf_phy * | phy, |
| enum synth_pd_ctrl | rx, | ||
| enum synth_pd_ctrl | tx ) |
Power down the TX and/or RX Local Oscillators.
| phy | The AD9361 state structure. |
| rx | The RX LO setting. |
| tx | The TX LO setting. |
| uint32_t ad9361_to_clk | ( | uint64_t | freq | ) |
Shift the real frequency value, so it fits type unsigned long Note: PLL operates between 47 .. 6000 MHz which is > 2^32.
| freq | The frequency value [Hz]. |
| int32_t ad9361_tracking_control | ( | struct ad9361_rf_phy * | phy, |
| bool | bbdc_track, | ||
| bool | rfdc_track, | ||
| bool | rxquad_track ) |
Setup RX tracking calibrations.
| phy | The AD9361 state structure. |
| bbdc_track | Set true, will enable the BBDC tracking. |
| rfdc_track | Set true, will enable the RFDC tracking. |
| rxquad_track | Set true, will enable the RXQUAD tracking. |
| int32_t ad9361_tx_mute | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | state ) |
Mute TX.
| phy | The AD9361 state structure. |
| state | The state - 0 mute; 1 - unmute. |
| int32_t ad9361_unregister_clocks | ( | struct ad9361_rf_phy * | phy | ) |
Unregister all the system clocks.
| phy | The AD9361 state structure. |
| int32_t ad9361_update_rf_bandwidth | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | rf_rx_bw, | ||
| uint32_t | rf_tx_bw ) |
Set the RF bandwidth.
| phy | The AD9361 state structure. |
| rf_rx_bw | The desired RX bandwidth [Hz]. |
| rf_tx_bw | The desired TX bandwidth [Hz]. |
| int32_t ad9361_validate_enable_fir | ( | struct ad9361_rf_phy * | phy | ) |
Validate FIR filter configuration - on pass enable.
| phy | The AD9361 state structure. |
| uint32_t ad9361_validate_rf_bw | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | bw ) |
Validate RF BW frequency.
| phy | The AD9361 state structure. |
| bw | The RF BW frequency. |
| int32_t ad9361_validate_rfpll | ( | struct ad9361_rf_phy * | phy, |
| bool | is_tx, | ||
| uint64_t | freq ) |
Validate RF PLL frequency.
| phy | The AD9361 state structure. |
| is_tx | TX enabled. |
| freq | The RF PLL frequency. |
| int32_t ad9361_write_bist_reg | ( | struct ad9361_rf_phy * | phy, |
| uint32_t | val ) |
Write directly to the AD9361 BIST configuration register.
| phy | The AD9361 state structure. |
| val | Value to write. |
| int32_t ad9361_write_clock_data_delays | ( | struct ad9361_rf_phy * | phy | ) |
Write the saved RX and TX clock/data delay values from pdata to hardware. Call this at startup to restore previously tuned values and skip dig_tune.
| phy | The AD9361 state structure. |
| struct gain_table_info ad9361_adi_gt_info[] |
| const char* ad9361_ensm_states[] |
State machine modes.
| const bool has_split_gt = HAVE_SPLIT_GAIN_TABLE |