no-OS
Loading...
Searching...
No Matches
parameters.h File Reference

Definition of STM32 platform data used by the AD4170 project. More...

#include "stm32_hal.h"
#include "stm32_spi.h"
#include "stm32_uart.h"
Include dependency graph for parameters.h:

Macros

#define INTC_DEVICE_ID   0
 
#define UART_INSTANCE   &huart5
 
#define UART_DEVICE_ID   5U /* UART5 */
 
#define UART_IRQ_ID   UART5_IRQn
 
#define UART_BAUDRATE   230400
 
#define uart_platform_ops   stm32_uart_ops
 
#define UART_EXTRA   &ad4170_uart_extra_ip
 
#define SPI_DEVICE_ID   1 /* SPI1 */
 
#define GPIO_CS_PIN   15 /* PA15 */
 
#define GPIO_CS_PORT   0 /* GPIOA */
 
#define SPI_MAX_SPEED_HZ   11250000
 
#define spi_platform_ops   stm32_spi_ops
 
#define SPI_EXTRA   &ad4170_spi_extra_ip
 

Variables

UART_HandleTypeDef huart5
 
struct stm32_uart_init_param ad4170_uart_extra_ip
 
struct stm32_spi_init_param ad4170_spi_extra_ip
 

Detailed Description

Definition of STM32 platform data used by the AD4170 project.

Author
Janani Sunil (janan.nosp@m.i.su.nosp@m.nil@a.nosp@m.nalo.nosp@m.g.com)

Copyright 2026(c) Analog Devices, Inc.

Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:

  1. Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
  2. Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
  3. Neither the name of Analog Devices, Inc. nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.

THIS SOFTWARE IS PROVIDED BY ANALOG DEVICES, INC. “AS IS” AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL ANALOG DEVICES, INC. BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

Macro Definition Documentation

◆ GPIO_CS_PIN

#define GPIO_CS_PIN   15 /* PA15 */

◆ GPIO_CS_PORT

#define GPIO_CS_PORT   0 /* GPIOA */

◆ INTC_DEVICE_ID

#define INTC_DEVICE_ID   0

◆ SPI_DEVICE_ID

#define SPI_DEVICE_ID   1 /* SPI1 */

◆ SPI_EXTRA

#define SPI_EXTRA   &ad4170_spi_extra_ip

◆ SPI_MAX_SPEED_HZ

#define SPI_MAX_SPEED_HZ   11250000

◆ spi_platform_ops

#define spi_platform_ops   stm32_spi_ops

◆ UART_BAUDRATE

#define UART_BAUDRATE   230400

◆ UART_DEVICE_ID

#define UART_DEVICE_ID   5U /* UART5 */

◆ UART_EXTRA

#define UART_EXTRA   &ad4170_uart_extra_ip

◆ UART_INSTANCE

#define UART_INSTANCE   &huart5

◆ UART_IRQ_ID

#define UART_IRQ_ID   UART5_IRQn

◆ uart_platform_ops

#define uart_platform_ops   stm32_uart_ops

Variable Documentation

◆ ad4170_spi_extra_ip

struct stm32_spi_init_param ad4170_spi_extra_ip
extern

◆ ad4170_uart_extra_ip

struct stm32_uart_init_param ad4170_uart_extra_ip
extern

◆ huart5

UART_HandleTypeDef huart5
extern