Skip to content

ELF File Explorer

The ELF File Explorer enables users to quickly parse and analyze compiled binaries, reducing time spent on debugging and profiling and providing deeper insights into the application structure.

Supported formats

The CodeFusion Studio ELF File Explorer can open and display the contents of any file with a valid ELF header. The file extensions supported by the ELF File Explorer are: AXF, DOJ, DXE, ELF, EXE, KO, MOD, O, OUT, PRX, PUFF, and SO.

Open a file

Open from Activity bar

  1. Select the CodeFusion Studio icon from the activity bar.
  2. Select Open ELF File under ELF File Explorer.
  3. Navigate to the ELF file you want to open.

Open from Explorer

Click on any ELF file in the explorer to view the contents of that file.

Navigation icons are on the left of the page for: Statistics, Metadata, Symbols and Memory Layout. Help is available via the help icon in the top right corner.

Statistics

The statistics page provides high level information about the ELF file and it's contents. Information is displayed in five sections.

ELF Statistics ELF Statistics

File overview

The file overview is a summary of the metadata for the ELF file:

  • Format: ELF 32-bit or 64-bit.
  • Data Encoding: Indicates the endianness (little or big endian).
  • File Type: Executable, relocatable, shared object, or core file.
  • Architecture: Target architecture (for example Arm, x86).
  • ABI Version: Application Binary Interface version.
  • Debug Info: Indicates if the file contains debugging information.
  • Stripping: Indicates if the file has been stripped of symbol information.

Main section sizes

The main section sizes shows the total memory used in the ELF, with a breakdown of the main data types.

  • Text: Executable code.
  • Data: Initialized global and static variables.
  • Bss: Zero-initialized data, both explicitly zero and uninitialized data.

Symbol types

Symbol types shows a count of functions and variables by binding: global, local, and weak. Filters are provided above the table for all, text, data and bss.

Sections

The Sections table provides details on all the sections contained within the ELF.

Largest symbols

The Largest symbols table provides details on the 10 largest symbols in the ELF. Filters are provided above the table for all, text, data and bss.

Metadata

The metadata page displays a summary of the sizes of each data type used (text, data and bss), and all of the information contained within the ELF header. This includes information about the architecture, data layout, ELF version, contents, and flags.

ELF Metadata ELF Metadata

Header Info

The ELF file header contains metadata about the ELF file, including its type, architecture, entry point, program headers, and section headers. This information is essential for the operating system to correctly load and execute the file.

AEABI Attributes

The AEABI (Arm Embedded Application Binary Interface) attributes in an ELF file provide important metadata about the binary, such as the target architecture, floating-point configuration, and optimization level. These attributes ensure compatibility and optimize performance by conveying specific details about how the binary was built, allowing tools and runtime environments to correctly interpret and execute the code.

Heuristic Information

Indicates the presence of any heuristic information detected in the ELF file related to the Zephyr and MSDK firmware platforms. It can provide information regarding Flash and RAM sizes, among other available data.

Symbols Explorer

The Symbol explorer provides a table of all of the symbols within the ELF file. This table can be sorted by clicking the title of any column and can be filtered using SQL queries for flexible data access.

Note

The Symbol Explorer query engine is based on AlaSQL. As a result, supported syntax and functions are limited to what AlaSQL provides. See the AlaSQL documentation for the full set of supported features and limitations.

ELF Symbol Explorer ELF Symbol Explorer

The default view SELECT * includes the following fields. You can change which fields are shown and in what order by replacing the * with a list of field names separated by a comma. For example SELECT size,name will show the size column followed by name.

Column Type Description
id integer The unique identifier for the symbol
name string The name of the symbol
type string The type of the symbol, indicating what kind of entity it represents
address integer The memory address where the symbol is located
section string The section of the program in which the symbol is defined
size integer The size of the symbol in bytes
localstack integer The worst stack usage size for a function (only local stack, not considering functions called)
stack integer The worst stack usage size for a function (considering functions called)
bind string The linkage type of the symbol (e.g., local, global)
visibility string The visibility of the symbol, indicating its accessibility from other modules (e.g., default, hidden)
path string The source file location where the symbol is defined

Note

The localstack, stack and path columns are only present when the relevant data is present in the ELF. For localstack and stack, the following GCC switches are required during build: -fdump-rtl-expand -fstack-usage -fdump-rtl-dfinish -fdump-ipa-cgraph -gdwarf-4. These switches are defined by default with CodeFusion Studio projects.

Generating additional compiler data

To generate SU and CGRAPH files with GCC (required for worst-case stack usage calculations, and call graph navigation), compile your code with the following flags: -fstack-usage -fdump-ipa-cgraph -gdwarf-4.

These flags will force the compiler to generate debug information using the DWARF-4 standard, which is the version currently supported by the built-in DWARF parser.

Zephyr

For Zephyr projects, add the following flags to CMakeLists.txt:

  zephyr_cc_option(-fstack-usage)  
  zephyr_cc_option(-fdump-ipa-cgraph)  
  zephyr_cc_option(-gdwarf-4)  

MSDK

For MSDK projects, add the following flags to the Makefile:

  PROJ_CFLAGS += -fstack-usage  
  PROJ_CFLAGS += -fdump-ipa-cgraph  
  PROJ_CFLAGS += -gdwarf-4  

Note

Stack usage and call graph data can only be parsed when generated by GCC.

Filters

The table can be filtered using SQL commands, where the table is named symbols and the fields are as above.

Tip

A quick lookup field is present above the table to search by name or address. Enter a text or numerical value and press Enter to generate a query.

Queries

Queries can be saved using the save icon to the right of the query field.
Click on the Saved queries button to the right of the query field to see a list of saved queries including some pre-populated queries. Queries can be edited or deleted from here by clicking on the pencil or trash can icons.

Note

Saved queries are stored in the user settings so they are available on any workspace.

Any valid SQL construct is supported here, including WHERE, ORDER, LIMIT, LIKE and REGEXP. Some examples of queries are as follows.

Filter Query
Specific colums SELECT name,address FROM symbols
Symbols larger than 100 bytes SELECT * FROM symbols WHERE size > 100
Largest symbols SELECT * FROM symbols ORDER BY size DESC LIMIT 10
Symbols between addresses SELECT * from symbols WHERE address BETWEEN 0x10000000 AND 0x20000000
Symbols from a specific file SELECT * from symbols WHERE path LIKE %main.c%
Symbols starting with string SELECT * FROM symbols WHERE name REGEXP '^init\*'

Memory Layout

The Memory Layout page provides a visual representation of the memory map on the left, with a table of memory segments on the right. The memory map is shared to denote the usage of the memory:

  • Stripes: Unused memory.
  • Blank: Read/write memory.
  • Filled: Read only memory.

Note

Overlapping segments are rendered as smaller rectangles to the right of the main segments. Small segments may be displayed taller than their actual relative size to enhance readability. Refer to the size value for an accurate size value.

Hovering over a segment in the memory map provides a summary of the memory segment and highlights the appropriate table entry.

Hovering over a segment in the table highlights the approprate entry in the memory map.

Segments

The segments table shows a high-level summary of each distinct secment of memory. ELF Memory Segments ELF Memory Segments

The table includes the following fields:

Field Description
Id The unique identifier for the segment
Type The type of the segment, indicating its purpose (e.g., loadable, dynamic)
Address The memory address where the segment begins
Size The size of the segment in bytes
Flags Permissions and attributes for the segment (R: read, W: write, X: executable)
Align The alignment requirement of the segment in memory in bytes

Clicking on a segment will show you a table with the sections in that segment.

Sections in a Segment

The Sections in a segment table shows a high-level summary of all the sections in that memory segment. ELF Memory Sections ELF Memory Sections

The Sections in a Segment table includes the following fields:

Field Description
Id The unique identifier for the section
Name The name of the section
Address The memory address where the section begins
Size The size of the section in bytes
Flags Permissions and attributes for the section described in the flags table
Type The type of the section, indicating its contents and purpose
Flag Description
W write
A alloc
X execute
M merge
S strings
I info
L link order
O extra OS processing required
G group
T TLS
C compressed
x unknown
o OS specific
E exclude
D mbind
y purecode
p processor specific

Clicking on a section will show you a table containing the symbols in that section. To return to the Segments, click on the Segments link in the breadcrumb at the top left of the page.

Symbols in a Section

The Symbols in a section table shows details for the symbols within that section.
ELF Memory Symbols ELF Memory Symbols

The Symbols in a section table includes the following fields:

Field Description
Id The unique identifier for the symbol
Name The name of the symbol
Address The memory address where the symbol is located
Size The size of the symbol in bytes
Bind The linkage type of the symbol (for example: local, global)
Visibility The visibility of the symbol, indicating its accessibility from other modules (for example: default, hidden)

To return to the Sections Segments, click on the appropriate link in the breadcrumb at the top left of the page.