Tools
The following tools are available in CodeFusion Studio:
The System Planner Configuration Tools dashboard includes the following tools:
- Peripheral Allocation – Assigns peripherals and signals to specific cores.
- Pin Config – Configures pin multiplexing.
- Clock Config – Controls clocks and related signals.
- Memory Allocation – Manages memory partitions and assigns RAM or Flash to cores.
- Registers – Displays register values used by the configuration code and allows filtering based on modified or default values.
- Embedded AI Tools – Import supported AI model files, assign them to cores, and configure engine-specific options for code generation.
- Profiling – Captures runtime and inference-level performance data, and prepares captured traces for visualization using the Zephelin Profiler for supported Zephyr projects.
- Generate Code – Generates the necessary source files for application configuration.
In addition to the System Planner Configuration Tools dashboard, CodeFusion Studio provides other utilities to support system development. These include:
- The CFS Command Line Utility – Provides command-line control over configuration tools and enables ELF file parsing.
- The ELF File Explorer – Enables graphical analysis of ELF files.
- The Device Tree View – Allows reviewing of hardware components in Zephyr.