blog
March 27, 2026
📚 The AI @ ADI Reading Digest: Recommended paper and research about AI at the edge.
At ADI, AI means developing world-class models that overcome latency, power, and cost constraints to deliver insights. March is behind us, and the team is recovering from very busy and memorable Embedded World and NVIDIA GTC conferences. Better yet, the sun is peeking through the clouds, and we can even dare think of spring. There may be even opportunity to sit outside and review the latest thought-provoking AI research recommended by our team:
📄 AtomicVAD: A tiny voice activity detection model for efficient inference in intelligent IoT systems
👍🏼 Recommended by: Shanza Iftikar
💡 Why it’s worth reading: The paper highlights an ultra-lightweight voice activity detection model designed for resource-constrained microcontrollers, with only 0.3K parameters and a low latency of 26 milliseconds. The model's small size was achieved using a generalized gated cosine unit activation and neural architecture search with Bayesian optimization and hyperband pruning. The Atomic VAD achieved an area under the curve of 0.903 and an F2 score of 0.891 on the challenging Ava speech benchmark.
📄 Do Foundation Models Know Geometry? Probing Frozen Features for Continuous Physical Measurements
👍🏼 Recommended by: Solomon Garber
💡 Why it’s worth reading: The paper shows how the text output machinery in vision foundation models acts as a bottleneck for task-specific features. The paper demonstrates how a simple linear probe of only 6000 parameters can be trained to extract hand joint angles from internal representations of an image generated by these models. LoRA fine-tuning is similarly effective to the linear probing, and both are significantly more accurate than the default text output channel. Deeper layers were more correlated with the target variable than the earlier, shallower layers. That remains the case until the text decoder portion of the model, at which point the information begins to drop.
This approach shows that pre-trained vision models capture more information than they can convey through the predefined text output channel. This information, however, can be extracted with simple, well-known techniques. This approach demonstrates a path forward for using pre-trained foundation models for physical intelligence tasks for which the models have not been trained for, nor show out-of-the box proficiency in.
Opinions expressed in the content posted here are the personal opinions of the original authors, and do not necessarily reflect those of Analog Devices, Inc (ADI) or its subsidiaries. The content is provided for informational purposes only and is not meant to be an endorsement or representation by ADI or any other party. This site may also provide links or references to non-ADI sites and resources. ADI makes no representations, warranties, or other commitments whatsoever about any non-ADI sites or third-party resources that may be referenced, accessible from, or linked to this site.
👍🏼 Recommended by: Muhammad Aneeq uz Zaman
💡 Why it’s worth reading: ChipMind proposes a method to enable LLMs to reason over long, complex chip specifications documents. The method converts documents into a structured knowledge graph (ChipKG) that captures circuit semantics (signals, conditions, dependencies). It then uses an iterative retrieval + reasoning loop with adaptive evidence selection to answer multi-hop questions more accurately than standard RAG. The key insight is that structure-aware retrieval and step-by-step reasoning outperform naive long-context or vector-based approaches for technical documents.
👍🏼 Recommended by: Debanjan Ghosh
💡 Why it’s worth reading: This paper tackles a practical bottleneck in aligning large language models: constrained decoding with lookahead heuristics delivers strong constraint satisfaction but is far too slow for real-world use. The authors introduce Constrained Decoding with Speculative Lookaheads (CDSL), borrowing ideas from speculative decoding to offload expensive lookahead generation to a smaller draft model while verifying with the target model and task-specific rewards. The result is a compelling 2×–12× speedup with minimal quality loss, making high-quality constrained decoding far more deployable in production settings.
👍🏼 Recommended by: Marlon Ares Milian
💡 Why it’s worth reading:
This 2025 preprint presents a modular, practical, and sample-efficient methodology to improve the performance of diffusion-based policies, particularly for the application of robotic behavioural cloning (BC). The authors introduce Diffusion Steering via Reinforcement Learning (DSRL), which develops a reinforcement learning (RL) policy to modify the latent noise space of a pretrained diffusion policy. Instead of finetuning weights, DSRL learns how to bias the initial noise distribution of the diffusion policy to indirectly modify the action space; this results in strong sample efficiency and black-box compatibility. The authors show performance improvements from 20% (diffusion policy before steering) to around 90% (RL-steered diffusion policy) success rate for a variety of tasks including: offline, online, and offline-to-online single task learning, as well as steering of generalist (multi-task) diffusion policies, both in simulation and real-world benchmarks. This work provides precise practical guidelines to adjust the methodology to different scenarios, as well as a modular, readily available, codebase. Overall, this paper bridges BC and RL elegantly, and provides a practical, readily available, methodology for developing diffusion-based policies for robot manipulation.
Like what you read here? Join us to help build the next generation of ultra-efficient AI for devices and robotics! Visit our careers page now!